Automation Rules: Workflow
Reliability Analytics: Automation Rule Workflow
This workflow describes the process for creating multiple distribution or growth analyses at a single time based on the execution of a query or an asset/event relationship.
In the following workflow diagram, the blue text in a shape indicates that the corresponding description has been provided in the sections that follow the diagram. For more information, refer to the Interpreting the Workflow Diagrams topic in the APM Product Workflows documentation.
Note: For information on the personas associated with a APM module, refer to the APM Product Workflows documentation.

View Existing Rule
Persona: Analyst
Open an existing automation rule that has been saved on the database and is accessible via hyperlinks from the Automation Rules section in Reliability Analytics
Create Rule
Persona: Analyst
Create a new automation rule using the wizard provided.
Merge Possible Analyses
Persona: Analyst
Merge sections of insufficient data to create enough data to support an analysis.
Execute Rule
Persona: Analyst
Queue the service that runs the rule that provides progress feedback and shows the details of the analyses.
Other Workflows
Persona: Analyst
Other workflows provide production data from: SAP, EAM, Recommendations.