Spares Analyses

About Spares Analysis

Spares Analysis is a tool that helps you maintain the optimal number of spare parts. Spares Analysis uses delivery time and cost, downtime, lost production costs, and failure and repair data to calculate how many spare parts should be kept on hand at any given time.

APM Reliability Analytics offers various tools that help you analyze the reliability of your equipment and locations so that you can make decisions about when to repair and replace those pieces of equipment and locations. For example, a Reliability Distribution Analysis lets you analyze historical failure data to help predict future failures. Based on those predictions, you can make plans for replacing equipment and making repairs to prevent future failures. As part of making plans to replace equipment in the future, you will want to make sure that you have an adequate number of spare parts available. Having spare parts on hand will help reduce the amount of downtime associated with unplanned failures.

The key to a successful spares program is maintaining a balance between:

  • Optimizing the spares level so that you have enough spare parts to handle unplanned failures.
  • Not having a surplus of parts that are not actually needed.

You can modify the input data for a Spares Analysis to evaluate the potential savings or losses associated with changing the spares level. For example, if you currently keep three spare seals for a pump, you could use a Spares Analysis to determine whether it would benefit your company financially to store either more or fewer spare seals instead.

Access a Spares Analysis

Procedure

  1. Access the RA Overview page.
  2. Select Spares Analyses.

    A list of Spares Analyses available in the database appears.

  3. Select the Spares Analysis whose details you want to view.

    The Analysis Summary workspace for the selected analysis appears.

    The workspace contains the following tabs:

    • Definition: Displays the details of the selected Spares Analysis.

      Note: As needed, in the Definition section, you can select to modify the values in the available fields, and then select to save your changes.
    • Summary: The Summary tab is selected by default and displays the Spare Level plot for all the Spares within the selected Spares Analysis. You can also view the following plots for all the Spares within the selected Spares Analysis:
      • Downtime plot
      • Spare Usage plot
      • Sensitivity plot
      • Optimal Holding plot

    The left pane contains a list of Spares available for the selected Spares Analysis.



Create a Spares Analysis

Procedure

  1. Access the RA Overview page.
  2. In the upper-right corner, select New Analysis, and then select Spares Analysis.

    The Spares Analysis page appears, displaying a blank datasheet in the Analysis Summary workspace.

  3. As needed, enter the values in the available fields, and then select .

    The Spares Analysis is saved.

What To Do Next

Example of a Spares Analysis

This example of a Spares Analysis demonstrates how you can use Spares Analyses to evaluate spare parts. We will refer to this example throughout the Spares Analysis documentation as needed.

Assume that you want to create a Spares Analysis for a group of pumps, which contain seals, bearings, and impellers, each of which can fail. Because you may need to replace seals, bearings, and impellers on the pumps when they fail, you can use a Spares Analysis to determine the optimal level for each spare part. Currently, two spare seals, two spare bearings, and no spare impellers are stored in the warehouse. By conducting a Spares Analysis, you can determine if this number of spare parts is adequate.

In the Spares Analysis, you will include failure data for each part of the pump, run the Monte Carlo simulation, and then view the plots to see the optimal level of each spare part. By implementing the recommended spare level, you will be able to limit the amount of downtime and reduce failure costs.

The following records will be defined for the Spares Analysis example. Data that exists within each record in the Spares Analysis example can be found in the example data tables.

  • Spares Analysis Example (Spares Analysis record)
    • Seals (Spare record)
      • Inboard Application (Spare Application record)
        • Inboard Population 1 (Spare Application Population record)
        • Inboard Population 2 (Spare Application Population record)
      • Outboard Application (Spare Application record)
        • Outboard Population 1 (Spare Application Population record)
        • Outboard Population 2 (Spare Application Population record)
        • Outboard Population 3 (Spare Application Population record)
    • Bearings (Spare record)
      • Inboard Application (Spare Application record)
        • Inboard Population 1 (Spare Application Population record)
        • Inboard Population 2 (Spare Application Population record)
      • Outboard Application (Spare Application record)
        • Outboard Population 1 (Spare Application Population record)
        • Outboard Population 2 (Spare Application Population record)
        • Outboard Population 3 (Spare Application Population record)
    • Impellers (Spare record)
      • All Applications (Spare Application record)
        • Pump Population 1 (Spare Application Population record)
        • Pump Population 2 (Spare Application Population record)
        • Pump Population 3 (Spare Application Population record)
        • Pump Population 4 (Spare Application Population record)

When viewing this list of records, you can see that each Spare record is linked to the Spares Analysis record, each Spare Application record is linked to a Spare record, and each Spare Application Population record is linked to a Spare Application record.

This example represents only one approach to creating a Spares Analysis. There are many alternate workflows that can be used for developing a Spares Analysis. For example, instead of creating a Spares Analysis at the pump level (e.g., the equipment level), you can create a Spares Analysis for each of the individual spare parts. After you are familiar with the functionality of a Spares Analysis, you can implement any workflow that works best for your organization.

Example Spare Analysis Record Data

The following table shows the data stored in the Spares Analysis record for the Spares Analysis example.

Record Section Values Specified

Spares Analysis Example

Analysis

Name: Spares Analysis Example

Description: This is a sample Spares Analysis example.

Simulation Start Date: 1/1/2015

Simulation End Date: 1/1/2025

Currency: $

Spares Analysis Example

 

Simulation Options

Number of Iterations: 100

Random Seed: No

Example Spare Record Data

The following table shows the data stored in the Spare records that are included in the Spares Analysis example.

RecordSectionValues Specified

Seals

Spare

Name: Seals

On-site Delivery Time: 4 Hours

Normal Order Time: 25 Days

Normal Cost: 100

Expedited Order Time: 3 Days

Expedited Cost: 300

Holding Cost Rate: 20 per Year

Minimum Holding Level: 0

Maximum Holding Level: 10

Current Holding Level: 1

Bearings

Spare

Name: Bearings

On-site Delivery Time: 4 Hours

Normal Order Time: 25 Days

Normal Cost: 100

Expedited Order Time : 3 Days

Expedited Cost: 300

Holding Cost Rate: 20 per Year

Minimum Holding Level: 0

Maximum Holding Level: 10

Current Holding Level: 1

Impellers

Spare

Name: Impellers

On-site Delivery Time: 4 Hours

Normal Order Time: 25 Days

Normal Cost: 100

Expedited Order Time: 3 Days

Expedited Cost: 300

Holding Cost Rate: 20 per Year

Minimum Holding Level: 0

Maximum Holding Level: 10

Current Holding Level: 0

Example Spare Application Record Data

The following table shows the data stored in the Spare Application record that are included in the Spares Analysis example.

Section Values Specified
Seals - Indoor Application

Application

Name: Indoor Application

Failure Distribution

Distribution Name: Failure Distribution

Distribution Description: Manually entered based on manufacturer data.

Units: Months

Distribution Type: Exponential

MTBF: 60

Failure Consequence

Preparation Time: 4 Hours

Repair Time: 8 Hours

Total Correction Time: 12 Hours

Labor Cost: 1000

Fixed Lost Production Cost: 0

Variable: Lost Production Cost Rate: 100000 per Day

# of Required Spares: 1

Preventive Maintenance

Enable Preventive Maintenance: No

Time-based Replacement Interval: No

Labor Cost: No

Downtime: No

Seals - Outdoor Application

Application

Name: Outdoor Application

Failure Distribution

Distribution Name: Failure Distribution

Distribution Description: Manually entered based on manufacturer data.

Units: Months

Distribution Type: Exponential

MTBF: 48

Failure Consequence

Preparation Time: 4 Hours

Repair Time: 8 Hours

Total Correction Time: 12 Hours

Labor Cost: 1000

Fixed Lost Production Cost: 0

Variable: Lost Production Cost Rate: 100000 per Day

# of Required Spares: 1

Preventive Maintenance

Enable Preventive Maintenance: No

Time-based Replacement Interval: No

Labor Costt: No

Downtime: No

Bearings - Indoor Application

Application

Name: Indoor Application

Failure Distribution

Distribution Name: Failure Distribution

Distribution Description: Manually entered based on manufacturer data.

Units: Months

Distribution Type: Exponential

MTBF: 60

Failure Consequence

Preparation Time: 4 Hours

Repair Time: 4 Hours

Total Correction Time: 8 Hours

Labor Cost: 500

Fixed Lost Production Cost: 0

Variable: Lost Production Cost Rate: 100000 per Day

# of Required Spares: 1

Preventive Maintenance

Enable Preventive Maintenance: No

Time-based Replacement Interval: No

Labor Cost: No

Downtime: No

Bearings - Outdoor Application

Application

Name: Outdoor Application

Failure Distribution

Distribution Name: Failure Distribution

Distribution Description: Manually entered based on manufacturer data.

Units: Months

Distribution Type: Exponential

MTBF: 48

Failure Consequence

Preparation Time: 4 Hours

Repair Time: 4 Hours

Total Correction Time: 8 Hours

Labor Cost: 500

Fixed Lost Production Cost: 0

Variable: Lost Production Cost Rate: 100000 per Day

# of Required Spares: 1

Preventive Maintenance

Enable Preventive Maintenance: No

Time-based Replacement Interval: No

Labor Cost: No

Downtime: No

Impellers - All Applications

Application

Name: All Applications

Failure Distribution

Distribution Name: Failure Distribution

Distribution Description: Manually entered based on manufacturer data.

Units: Months

Distribution Type: Exponential

MTBF: 72

Failure Consequence

Preparation Time: 4 Hours

Repair Time: 4 Hours

Total Correction Time: 8 Hours

Labor Cost: 500

Fixed Lost Production Cost: 0

Variable: Lost Production Cost Rate: 100000 per Day

# of Required Spares: 1

Preventive Maintenance

Enable Preventive Maintenance: No

Time-based Replacement Interval: No

Labor Cost: No

Downtime: No

Spare Application Population Record Data

The following table shows the data stored in the Spare Application Population records that are included in the Spares Analysis example.

Population Name Values Specified

Seals - Inboard Application

Inboard Population 1

Population Size: 2

Age Value: 2 Years

Inboard Population 2

Population Size: 1

Age Value: 4 Years

Seals - Outboard Application

Outboard Population 1

Population Size: 4

Age Value: 2 Years

Outboard Population 2

Population Size: 2

Age Value: 3 Years

Outboard Population 3

Population Size: 1

Age Value: 5 Years

Bearings - Inboard Application

Inboard Population 1

Population Size: 2

Age Value: 2 Years

Inboard Population 2

Population Size: 1

Age Value: 4 Years

Bearings - Outboard Application

Outboard Population 1

Population Size: 4

Age Value: 2 Years

Outboard Population 2

Population Size: 2

Age Value: 3 Years

Outboard Population 3

Population Size: 1

Age Value: 5 Years

Impellers - All Applications

Pump Population 1

Population Size: 6

Age Value: 2 Years

Pump Population 2

Population Size: 1

Age Value: 4 Years

Pump Population 3

Population Size: 2

Age Value: 3 Years

Pump Population 4

Population Size: 1

Age Value: 5 Years

Copy a Spares Analysis

Procedure

  1. Access the RA Overview page.
  2. Select Spares Analysis.
    A list of Spares Analyses appears.
  3. In the row containing the Spares Analysis that you want to copy, select .
    A message appears, asking you to confirm that you want to copy the Spares Analysis.
  4. Select Yes.
    The Copy Analysis window appears.
  5. As needed, change the name of the Spares Analysis, and then select Save.
    The Spares Analysis is copied.

Delete a Spares Analysis

Procedure

  1. Access the RA Overview page.
  2. Select Spares Analyses.

    A list of Spares Analyses available in the database appears.

  3. Select the row containing the Spares Analysis that you want to delete, and then select .

    The Delete Spares Analysis dialog box appears, asking you to confirm that you want to delete the selected Spares Analysis.

  4. Select Yes.

    The selected Spares Analysis is deleted.

Results

  • Any associated Spares are deleted.
  • Any associated Spare Applications are deleted.
  • Any associated Spare Application Populations are deleted.

Access Spares Analysis Report

Procedure

  1. Access the Spares Analysis whose report you want to access.
  2. In the upper-right corner of any workspace within the selected Spares Analysis, select Report.

    The Spares Analysis report appears in a new browser tab.

    By default, the report contains the following sections:

    • Analysis Plots
    • Analysis Properties
    • Spare Properties
    • Application Properties

About Spares Analysis Report

The baseline APM database includes the Spares Analysis Report, which you can use to view a summary of Spares Analysis results.

The Spares Analysis Report is built from the following Catalog items:

  • The main report, Spares Analysis, which is stored in the Catalog folder \\Public\Meridium\Modules\Reliability Manager\Reports.
  • The subreport, Spares, which is stored in the Catalog folder \\Public\Meridium\Modules\Reliability Manager\Reports.
  • The subreport, SparesApplication, which is stored in the Catalog folder \\Public\Meridium\Modules\Reliability Manager\Reports.
  • The subreport, SparesChart, which is stored in the Catalog folder \\Public\Meridium\Modules\Reliability Manager\Reports.
  • The supporting queries that supply data in the main report and subreports, which are stored in the Catalog folder \\Public\Meridium\Modules\Reliability Manager\Reports. The following supporting queries are available:
    • Spares Analysis - Applications
    • Spares Analysis - Charts
    • Spares Analysis - ChartsMain
    • Spares Analysis - Main
    • Spares Analysis - Spares
    • Spares Analysis - SparesMain

Throughout this documentation, we refer to the main report, the subreports, and the supporting queries collectively as the Spares Analysis Report.

Analysis Properties Section

The Analysis Properties section of the Spares Analysis Report displays information that is stored in the Spares Analysis record. The name of the analysis, which is stored in the Analysis ID field of the Spares Analysis record, is displayed in blue at the top of the Analysis Properties section.

The following table lists each item in the Analysis Properties section and the corresponding Spares Analysis record field whose data is displayed in the report.

Report ItemRecord Field(s)
Analysis Properties
Description Short Description
Start Date Analysis Start Date
End Date Analysis End Date
Currency Number
Simulation Options
Iteration Iteration Number
Random Seed Random Seed
Events Logged Enable Event Log

Spares Properties Section

Each Spare Analysis record can be linked to multiple Spare records. In the Spares Analysis report, a Spare Properties section will appear for each Spare record that is linked to the Spare Analysis record. The name of the spare, which is stored in the Spare ID field of the Spare record, is displayed in blue at the top of each Spare Properties section.

The following table lists each item in theSpare Properties section and the corresponding Spares Analysis record field whose data is displayed in the report.

Report ItemRecord Field(s)
On-site Delivery Time

Onsite Delivery Time Value

On-site Delivery Time Unit

Normal Order Time

Normal Order Time Value

Normal Order Time Unit

Expedited Order Time

Expedited Order Time Value

Expedited Order Time Unit

Normal Cost Normal Cost
Expedited Cost Expedited Cost
Holding Cost Rate

Holding Cost Rate

Holding Cost Unit

Inventory level range

Min Inventory Level

Max Inventory Level

Current Holding Level Current Holding Level

Application Properties Section

Spare records can be linked to multiple Spare Application records. For each Spare record in the Spares Analysis report, there can be multiple Application Properties sections. The name of the corresponding Application, which is stored in the Application ID field of each Spare Application record, is displayed at the beginning of each Application Properties section.

Each Application Properties section contains the following grids:

The Populations grid displays information stored in Spare Application Population records. There can be multiple Spare Application Population records linked to each Spare Application record. For each Spare Application Population record, one row exists in the Populations grid.

The following table lists each item in the Populations grid and the corresponding Spare Application Population record field whose data is displayed in the report.

Report ItemRecord Field(s)
Population Name

Name

Population Size

Population Size

Population Age

Age

Age Time Unit

The Failure Distribution grid displays information that is stored in Distribution records that are linked to the Spare Application record. There can be multiple Distribution records linked to each Spare Application record. For each Distribution record, one row exists in the Failure Distribution grid.

The following table lists each item in the Failure Distribution grid and the corresponding Distribution record field whose data is displayed in the report. The values in the Parameter 1, Parameter 2, and Parameter 3 columns will be different depending on whether the Distribution record is an Exponential, Lognormal, Normal, or Weibull distribution.

Report ItemFamilyRecord Field(s)
Name Distribution

Onsite Delivery Time Value

On-site Delivery Time Unit

Distribution Type Distribution

Normal Order Time Value

Normal Order Time Unit

Time Unit Distribution

Expedited Order Time Value

Expedited Order Time Unit

Parameter 1

Exponential

Lognormal

Normal

Weibull

MTBF

Mu

Fix Mean

Beta

Parameter 2

Lognormal

Normal

Weibull

Sigma

Fix Standard Deviation

Eta

Note: If the Distribution Type is Exponential, no value is displayed.
Parameter 3

Lognormal

Weibull

Gamma

Gamma

Note: If the Distribution Type is Exponential or Normal, no value is displayed.

The Failure Consequence grid displays information stored in the Spare Application record.

The following table lists each item in the Failure Consequence grid and the corresponding Spare Application record field whose data is displayed in the report.

Report ItemRecord Field(s)
Preparation Time

Preparation Time Value

Preparation Time Unit

Repair Time

Repair Time Value

Repair Time Unit

Labor Cost

Repair Labor Cost

Fixed Lost Production Cost Fixed Lost Production Cost
Variable Lost Production Cost Rate

Variable Lost Production Cost

Variable Lost Production Unit

# of Required Spaces

Required Spares

The Preventive Maintenance grid displays information stored in the Spare Application record.

The following table lists each item in the Preventive Maintenance grid and the corresponding Spare Application record field whose data is displayed in the report.

Report ItemRecord Field(s)
Time-based Replacement Interval

PM Interval Value

PM Interval Unit

Labor Cost

PM Labor Cost

Downtime

PM Downtime Value

PM Downtime Unit

Plots Section

If you have run a Monte Carlo simulation, the Spares Analysis graphs will appear in the Spares Analysis report with the results from the last simulation that was run.