Exceptions
About Exceptions
Exceptions are action items that must be completed by the team before delivering a change. In the Application Settings for MOC, you can create Exception records to identify the type of Exception that must be created for an Answer Option. When you respond to Questions in a Checklist in the Change Project, Exceptions are automatically created by copying the Exceptions that you created.
Default Exceptions in MoC
APM provides a set of Exceptions, by default. These Exceptions are associated with Answer Options of Questions. The following table lists the default Exceptions, which you can modify as needed:
Exception ID | Exception Type |
---|---|
Asset Change | Update EAM/CMMS records |
Asset Removal | Update EAM/CMMS records |
Chemical Change | Update facility chemical hazard storage documentation |
Controls parameters | List all pre and post change controls parameters |
Electrical load | Update electrical safe work plans |
Energy Source | Update LOTO documentation and safe work plans |
Exit Route | Revise or replace emergency exit route placards |
Flare addition | Update flare usage documentation |
Heights | Update safe work plans related to working above grade |
Lock out Tag out | Update safe work plans, and applicable LOTO plans |
Machine guarding | Revise existing or add new machine guarding as app |
Material Storage | Update facility chemical hazard storage documentation |
MSDS | Update material safety data sheet |
Procedural | Update applicable Operating or Maintenance procedure |
Process Sewer | Update sewer source and usage documentation |
Solid Waste | Update facility chemical hazard storage documentation |
Storm Drain | Notify local authorities, and update facility possible discharge documentation |
Update and link all updated drawings and diagrams | Drawings/Diagrams |
Update applicable emergency evacuation routing | Ingress/Egress |
Update the process safety information | Process Safety Information |