Catalog Items
Queries Folder
Query Name | Behavior and Usage |
---|---|
Get Event Types to check required rule for Amplification Code | Returns the list of the NERC Event Types to check whether Amplification Code is a required field during event state transition. Note: Currently, the query returns all the NERC Event Types except U1. However, you can modify the query to add or remove any NERC Event Type. |
GAA Contributing Events for the given Primary event Datagrid | Returns the list of Contributing Events that are associated with a Primary Event. You cannot modify or delete the Event ID, Primary Event Key, Contributing Event Key, or Hyperlink fields. You can also add a new Hyperlink field. |
GAA Event Categories | Returns the list of all the event categories and its associated color codes and events. You can modify the columns for the Event Category grid. You cannot modify the ENTY_ID column. Note: When adding or deleting columns, update the required hyperlink URLs. |
GAA Event Types | Returns the list of all the event types and its associated color codes and regulatory organizations. You can modify the columns for the Event Type grid. You cannot modify the Event Type Code column. Note: When adding or deleting columns, update the required hyperlink URLs. |
GAA Mappings list | Returns the list of the mappings between NERC and CEA Codes. You can modify the columns within the Mappings grid. You cannot modify the ENTY_KEY column. |
Gaa reports and performance configuration list | Returns a list of all the configuration data. You can modify the Configuration grid. You cannot modify the Entity ID column. |
Get Contributing Events for Export | Returns the details of Contributing Events for exporting. You can modify this query to determine the fields of the Contributing Event records that must be exported. Important:
|
Get Event Types to exclude from Required fields check | Returns the list of the CEA Event Types to check whether the following fields, Cause Code System, Cause Code Component, Cause Code, Amplification Code, and Verbal Description are required fields during event state transition. Note: Currently, the query returns the following list of CEA Event Types 11-1,11-2,14,14-1,14-2 only. However, you can modify the query to add or remove any CEA Event Type. |
Get Primary and Related Events for Export | Returns the details of Primary Events and Related Events for exporting. You can modify this query to determine the fields of the Primary Event and Related Event records that must be exported. Important:
|
Primary Event Details | Returns the list of all the Primary Events for a GAA Unit, including OMC Events, for the specified period. You cannot modify or delete the Event ID, Primary Event Key, Event Key, or Hyperlink fields. |
Primary Event Details Datagrid | Returns the list of all the Primary Events associated with a Performance record for the associated GAA Unit. This query calls the Primary Event Details or Primary Event Details Excluding OMC query based on your selection in the Performance Records section in the Performance & Reports workspace. You cannot modify or delete the Event ID, Primary Event Key, Event Key, or Hyperlink fields. You cannot modify the Hyperlink column. And you cannot modify the Regulatory and Management reports. You can add a new Hyperlink field. Note: When adding or deleting columns, update the required hyperlink URLs. |
Primary Event Details DataGrid Excluding OMC | Returns the list of all the Primary Events associated with a Performance record for the associated GAA Unit. This query calls the Primary Event Details or Primary Event Details Excluding OMC query based on your selection in the Performance Records section in the Performance & Reports workspace. You cannot modify or delete the Event ID, Primary Event Key, Event Key, or Hyperlink fields. You cannot modify the Hyperlink column. You can add a new Hyperlink field. |
Primary Events for Events List | Returns the list of Primary Events for a GAA Unit during the specified period. Important: When using this query, you must not perform the following actions on the query:
However, you can add a new field. |
Primary Events for Events List with eLog | Returns the list of Primary Events for a GAA Unit during the specified period. Important: When using this query, you must not perform the following actions on the query:
|
Primary Events for Events List with RCA | Returns the list of Primary Events for a GAA Unit during the specified period. Important: When using this query, you must not perform the following actions on the query:
|
Primary Events for Events List with RCA and eLog | Returns the list of Primary Events for a GAA Unit during the specified period. Important: When using this query, you must not perform the following actions on the query:
|
Primary Events Tiles Wrapper Query | Returns the list of Events in the Event Under Review and Approved Events
tabs on the GAA Overview page. You must not delete the Event Key and Unit Entity Key fields. You can add a Hyperlink property to a field but you cannot modify or delete a field that contains this property. You can modify the sub query to add more columns and then, as needed, modify this query to add more columns. You must not modify the Even ID and Unit Name columns. Note: When adding or deleting columns, update the required hyperlink URLs. |
Reports list for Unit Datagrid | Returns the list of Regulatory Reports on the GAA Administrator page. You can add a Hyperlink property to a field but you cannot modify or delete a field that contains this property. You cannot modify an existing Key field and the Key column. |
Retrieve Capacities for a Unit | Returns the list of the capacities for a Unit. You can modify the columns for the Capacities grid for a specified unit. You cannot modify the ENTY_KEY column. Note: When adding or deleting columns, update the required hyperlink URLs. |
Retrieve Event Transition Data | Returns the list of the Event Transition data. You can modify the Event Transition grid. You cannot modify the ENTY_KEY column. |
Retrieve GAA Amplification Codes | Returns the list of the GAA Amplification Codes. You can modify the columns for the Amplification Codes grid. You cannot modify the ENTY_KEY column. Note: When adding or deleting columns, update the required hyperlink URLs. |
Retrieve GAA Cause Codes | Returns the list of the GAA Cause Codes. You can modify the columns for the Cause Codes grid. You cannot modify the ENTY_KEY column. Note: When adding or deleting columns, update the required hyperlink URLs. |
Retrieve GAA Fuel Data | Returns the list of GAA Fuel Code data. You can modify the columns for the Fuel Data grid. You cannot modify the ENTY_KEY column. |
CEA Queries Folder
- Do not delete the columns in any of the queries.
- Do not modify the alias and order of columns any of the queries.
Query Name | Behavior and Usage |
---|---|
CEA Event Report | This query is used to get the events data for Event Report. |
CEA Performance Report | This query is used to get the performance data of All Events Performance Record. |
Get Data for CEA Performance Report for Given Year, Month and Unit | This query is used to get the data for Performance Report. |
All CEA Primary Events | This query is used to get all events for Performance Record calculation. |
CEA Primary Events Excluding OMC | This query is used to get all events except OMC events for Performance Record calculation. |
Graph Queries Folder
Query Name | Behavior and Usage |
---|---|
GAA_Overview - Performance Report Statisitcs | This query is used to populate the Event and Performance Report Statistics section in the GAA Overview page. This query cannot be modified in the query designer. The Performance Indexes Based NMC and Performance Records between date ranges sub-queries can be modified to add, delete, or reorder columns. You cannot modify the Unit ID column. |