Catalog Items

About the ASM Catalog Folder Structure

The main ASM Catalog folder is \\Public\Meridium\Modules\Asset Strategy Management\Management. This folder contains the subfolders, Queries and Reports, which contain baseline queries and reports that are used by default in ASM.

Another Catalog folder is \\Public\Meridium\Modules\Asset Strategy. This folder contains subfolders, Dashboards and Graphs, which contain baseline dashboards and graphs used by default in ASM.

If desired, you can store additional items in the main ASM Catalog folder or in the subfolders. In addition, you can create new subfolders to store additional items.

Note: All Public folders exist by default. Any baseline item in the Baseline folder is also available in the corresponding Public folder. Throughout this documentation, however, we refer to items in the Public folder.

Graphs Folder

The Catalog folder \\Public\Meridium\Modules\Asset Strategy contains subfolders which contain the baseline graphs that are used in ASM dashboards. The following table contains the graph names and details.

GraphBehavior and Usage
Action Count By StateDisplays a graph representing all of the actions separated according to their state. This graph is used in the ASM Dashboard.
Cost of Events per Month by AssetDisplays a graph representing the monthly costs of maintenance for each asset. This graph is used in the Asset Strategy Dashboard.
Criticality DistributionDisplays a graph representing the criticality for assets. This graph is used in the Asset Strategy Dashboard.
Strategy Count By StateDisplays a graph representing all of the strategies separated according to their state. This graph is used in the ASM Dashboard.
Total Cost of UnreliabilityDisplays a graph representing the total cost of unreliability on a monthly basis. This graph is used in the Asset Strategy Dashboard.
Total Unplanned Maintenance CostsDisplays a graph representing the total cost of all unplanned maintenance on a monthly basis. This graph is used in the Asset Strategy Dashboard.

Reports Folder

The Catalog folder \\Public\Meridium\Modules\Asset Strategy Management\Management\Reports contains the baseline report that is used by default in ASM. The following table identifies that report.

Report

Behavior and Usage

Asset Strategy Approval ReportA summary report used to review an asset strategy and determine whether to approve it or send it for rework.

Queries Folder

The Catalog folder \\Public\Meridium\Modules\Asset Strategy Management\Management\Queries contains the baseline queries that are used by default in ASM. The following table identifies and describes the queries.

Note: All Public folders exist by default. Any baseline item in the Baseline folder is also available in the corresponding Public folder. Throughout this documentation, however, we refer to items in the Public folder.
Query Behavior and Usage
Active_Template_Search Returns a list of all asset strategy template records that are currently in the Active state.
Adding Asset Strategies to System StrategyReturns a list of Asset Strategies to add to a System Strategy.
Asset Strategy Action RevisionsReturns a list of columns representing fields from the Action family. The query is also used to support the Implement Actions workspace.
Asset Strategy Actions DetailReturns the costs and details of the asset strategy's mitigating actions. The query is also used to support the Asset Strategy Approval Report .
Asset Strategy Active Actions DetailReturns the details of the asset strategy's active mitigating actions. The query is also used to support the Asset Strategy Approval Report.
Asset Strategy Active Mitigated Financial Risks DetailReturns the details of all of the actions that mitigate financial risks for an asset strategy. The query is also used to support the Asset Strategy Approval Report.
Asset Strategy Active Mitigated Risks DetailReturns the details of all the actions that mitigate risks for an asset strategy. The query is also used to support the Asset Strategy Approval Report.
Asset Strategy DefinitionReturns definition information for a particular asset strategy. The query is also used to support the Asset Strategy Approval Report.
Asset Strategy Financial RisksReturns the financial risks for an asset strategy. The query is also used to support the Asset Strategy Approval Report.
Asset Strategy Risk ProfileReturns the risk profile information for an asset strategy. The query is also used to support the Asset Strategy Approval Report.
Asset Strategy Risk SummaryReturns strategy-level risk information. The query is also used to support the Asset Strategy Approval Report.
Asset_Strategy_Search After prompting you to select a family and a state, returns a list of all asset strategy records that are linked to a record in the selected family and that are currently in the selected state. APM runs this query when you search for any strategy in ASM.
Asset_Strategy_Search_Non_Pending After prompting you to select a family, returns a list of all asset strategy records that are linked to a record in the selected family.
Calibration Task Link Existing QueryThis query is used by the ASM Implement Actions section to locate existing Calibration Tasks for implementation.
EAM Action Mapping Returns a list of fields from the Action family that are used in the Implement as EAM Work Request and EAM Maintenance Plan features. Using this query, you can control the mappings between Action data and the EAM Notifications via the Implement as EAM Work Request and EAM Maintenance Plan features. Using Action Mappings, you can send Action information to your EAM system as a singular work request or a recurring maintenance plan.
Inspection Task Link Existing QueryThis query is used by the ASM Implement Actions section to locate existing Inspection Tasks for implementation.
Locate Assets By EAM System For ImportReturns Equipment and Functional Location records where the value in the CMMS System field of the record matches the SAP System of a selected ASI package. The results of this query are displayed in the Asset Strategy Builder when importing SAP objects into ASI.
Locate Assets For Import Returns a list of equipment records.
Locate Assets For Template ApplicationReturns assets which belong to a family that can be related to asset strategies and that are not already in a Master Template relationship.
Locate Unlinked Work Management Items For AssetsReturns all work management items, for a specified set of assets, that are not linked to an implementation package.
Strategies Without Master Templates After prompting you to select a family, returns a list of: asset strategy records that are linked to a record in the selected family but are not linked to an asset strategy template record through the Master Template Has Asset Strategy relationship. Asset strategy records that are not linked to a record and are not linked to an asset strategy template record through the Master Template Has Asset Strategy relationship. APM runs this query when you select the Add Existing button on the asset strategy or when you choose to apply an asset strategy template as a master in the Apply Template Builder.
Strategy Asset FamiliesReturns the list of asset strategy families.
System_Strategy_Search Returns a list of all system strategy records. APM runs this query when you select the System Strategies tab on the ASM Module Overview.
Template_SearchReturns a list of asset strategy templates.

Dashboards Folder

The Catalog folder \\Public\Meridium\Modules\Asset Strategy\Dashboards contains the baseline dashboards that are used by default in ASM. The following table identifies and describes the dashboards.

DashboardBehavior and Usage
ASM DashboardUsed for the ASM Overview page, which contains the Action Count By Type and Strategy Count by State graphs.
Asset Strategy DashboardDisplays ASM graphs and queries as widgets. This dashboard can also be set as the ASM Overview page dashboard.