SAP Criticality Assessment Interface

About the SAP Criticality Assessment Interface

Using the SAP Criticality Assessment Interface, you can perform the following tasks:
  • Send the Criticality value in APM to update the ABC Indicator field in SAP.
  • Specify a custom Function Module Name used in SAP to which you want to send additional or alternate information.
  • Define the source field mappings between APM and SAP using a baseline Policy. You can change the default Policy to a different one.

Change the Function Module

About This Task

This topic describes how to change the default SAP Function Module to a different one.

Procedure

  1. Access the ACA Administrator page.
  2. In the SAP Criticality Assessment Interface section, in the Function Module Name box, enter the name of the Function Module that you want to use.
  3. Select Save.
    The Function Module is changed.

Change the Criticality Table Policy

About This Task

A default Criticality Table Policy is used to specify the field mappings between APM and SAP. This topic describes how to change the default Policy to a different one.

Procedure

  1. Access the ACA Administrator page.
  2. In the SAP Criticality Assessment Interface section, in the Criticality Table Policy box, enter the name of the Policy that you want to use.
  3. Select Save.
    The Criticality Table Policy is changed and will now be used to specify the field mappings between APM and SAP.