Schedules

About Rounds Pro Schedule

Rounds Pro Schedules are schedule objects that are maintained in the Rounds Pro Schedule Family. These schedules once created can be linked to Measurement Steps.

Advantages of using a schedule:
  • You can organize your schedules and later associate them with Measurement Steps.
  • You can use the same schedule in multiple steps. All these steps will then follow the same schedule. You can thus track all these steps easily.
  • If you update a schedule, the changes are applied to all the steps that use the schedule.

Route Instance Examples Based on a Schedule

This topic provides information on how Route Instances are created with few examples of scheduling.

Table 1. Examples
S.NoRoute Master Schedule StatusStep Schedules (This example route has 5 steps)Expected Result
1Defined for everyday for 8 AMNot Defined for any of the five steps.A Route Instance is created every day at 8AM with all the five steps.
2Defined once every 12 hours starting at 6 AM
Note: Steps are usually scheduled at lower frequency than that for Route Master.
  • Step 1: Not Defined
  • Step 2: Defined once every 24 hours starting at 6 AM
  • Step 3: Defined for every Monday, stating at 6 AM
  • Step 4: Defined for every Tuesday, stating at 6 PM
  • Step 5: Defined for every 12 Hours, stating at 5 AM
Instance Created atSteps Included
6AM on SundayStep 1, Step 2, and Step 5
6PM on SundayStep 1 and Step 5
6AM on MondayStep 1, Step 2, Step 3, and Step 5
6PM on TuesdayStep 1, Step 4, and Step 5
3Not DefinedDefined for everyday at 8 AM for all the steps.This is a Invalid Scenario.

Access a Rounds Pro Schedule

Procedure

  1. Access the Rounds Designer Page.
  2. Select Manage > Schedules.
    The Schedule Management page appears, displaying a list of schedules.

Create a Rounds Pro Schedule

About This Task

You can create a schedule to use it in Measurement steps.

Procedure

  1. Access the Rounds Designer Page.
  2. Select Manage > Schedules.
    The Schedule Management page appears, displaying a list of schedules.
  3. Select .
    The Create Schedule window appears.
  4. In the SCHEDULE NAME box, enter a unique name for the schedule. The name can contain up to 50 characters.
  5. Set a time zone, start date, and frequency for the schedule.
  6. Select Save.
    The schedule is created.