Inspection Management Deployment
Deploy Inspection Management for the First Time
The following table outlines the steps that you must complete to deploy and configure this module for the first time. These instructions assume that you have completed the steps for deploying the basic system architecture.
These tasks may be completed by multiple people in your organization. We recommend, however, that the tasks be completed in the order in which they are listed.
Step | Task | Notes |
---|---|---|
1 | Review the Inspection Management data model to determine which relationship definitions you will need to modify to include your custom equipment and location families. Via Configuration Manager, modify the relationship definitions as needed. | This step is required only if you store equipment and location information in families other than the baseline Equipment and Functional Location families. |
2 | Configure APM to create Task Revision records. | This step is required only if you want Task Revision records to be created every time you create or update a task. These records are used to track historical data related to a task. |
3 | Assign Security Users to one or more of the Security Roles used in IM. | This step is required. Security Users will need permissions to the Inspection Management families before they can use the Inspection Management features. |
4 | Assign Resource Roles to users. | This step is required to define the users who can perform Inspection workflows as Inspectors, supervisors, administrators, contract inspectors, and risk analysts in Inspection Management. |
5 | Modify baseline Application Configuration settings. | This step is required only if you want to modify Application Configurations. The following Application Configurations are defined in the baseline database: Asset Query Path; Associated Relationship Family; Published Query Path; Summary Query Path; Alerts Query Path; Asset Is Successor; Profile Configuration; Method Configuration; Strategy Rule Configuration. |
6 | Define the Inspection Profile for each piece of equipment that you will inspect. | This step is required only if you plan to create Inspection records in baseline families other than the Checklists subfamilies. |
7 | Modify the baseline Asset query. | This step is required only if you want Inspection records to be linked to records in a family other than the Equipment family. |
8 | Define Event Configurations for any new Inspection families that you have created. | This step is required only if you have created custom Inspection families that you want to use within Inspection Management. |
9 | Create a Checklist Configuration Template for custom inspections. | This step is optional. |
10 | Define Taxonomy Configurations for Inspection Families and Checklist Configurations. | This step is required only if you want to link Inspection Families and Checklist Configurations to assets using equipment taxonomy. |
11 | Assign certifications to users. | This step is optional. |
12 | Group inspection work into Work Packs. | This step is optional. |
13 | Configure Inspection Management ActiveMQ settings for MIExecution ServiceConfigure Inspection Management ActiveMQ settings for MIExecution Service. | This step is optional. You can perform this step if you want to modify the default retries or concurrency settings. |
14 | Ensure that the Meridium MIExecution Service is installed and running. | If the basic APM system architecture is already installed, the Meridium MIExecution Service is automatically installed, and the service runs automatically. |
15 | Modify the Inspection Event preferences. | This step is required to avoid creating redundant related records while creating inspection record. |
Configure APM to Create Task Revisions
About This Task
You can configure APM to create records that track changes to Task record values, so that you can keep a historical record of Task data on a given date and time. Throughout this documentation, we refer to these revision-tracking records as Task Revision records. The family caption, however, is not necessarily Task Revision.
APM provides the following Task Revision families, but you can create your own:
- Task Revision
- Inspection Task Revision
We assume that you do not want a Task Revision record to be created when you create a new Task record or update an existing Task record. If, however, you want these Task Revision records to be created, you will need to perform the following step.
Procedure
Results
Configure Inspection Management ActiveMQ settings for MIExecution Service
The MIExecution Service,on each APM Server serves RBI, Inspection and Thickness Monitoring module queues. This service is configured to use a single shared ActiveMQ queue service across APM. Available queue configuration options include retries and concurrency limit.
Procedure
Inspection Management Security Groups and Roles
The following table lists the baseline Security Groups available for users within this module, as well as the baseline Roles to which those Security Groups are assigned.
Security Group | Roles |
---|---|
MI Inspection |
MI Mechanical Integrity Administrator MI Mechanical Integrity Power MI Mechanical Integrity User |
MI Inspection Viewer |
MI APM Viewer MI Mechanical Integrity Viewer |
- Inspector
- Inspection Supervisor
- SC Recommendations Implementer
- SC Recommendations Reviewer
These roles are used in State Management.
Family | MI Inspection | MI Inspection Viewer |
---|---|---|
Entity Families | ||
Alert | View, Insert, Update, Delete | View |
Certification | View, Insert, Update, Delete | View |
Checklist Finding | View, Insert, Update, Delete | View |
Conditional Alerts | View, Insert, Update, Delete | View |
Corrosion | View, Insert, Update, Delete | View |
Equipment | View, Insert, Update, Delete | View |
Event | View, Insert, Update, Delete | View |
Finding | View, Insert, Update, Delete | View |
Human Resource | View | View |
Inspection Method | View, Insert, Update, Delete | View |
Inspection Profile | View, Insert, Update, Delete | View |
Inspection Team Member | View, Insert, Update, Delete | View |
Inventory Group Configuration | View | View |
Potential Degradation Mechanisms | View | View |
RBI Degradation Mechanisms | View | View |
RBI Inspection Auto-Selection Criteria | View | View |
Recommendation | View, Insert, Update, Delete | View |
Reference Document | View, Insert, Update, Delete | View |
Resource Role | View, Insert, Update, Delete | View |
SAP System | View | View |
Security User | View | View |
Strategy | View, Update | View |
Task | View, Insert, Update, Delete | View |
Taxonomy References | View | View |
Time Based Inspection Interval | View, Insert, Update, Delete | View |
Time Based Inspection Setting | View, Insert, Update, Delete | View |
Work Pack | View, Insert, Update, Delete | View |
Relationship Families | ||
Belongs to a Unit | View, Update, Insert, Delete | View |
Checklist Has Finding | View, Insert, Update, Delete | View |
Has Certifications | View, Insert, Update, Delete | View |
Has Degradation Mechanisms | View | View |
Has Findings | View, Insert, Update, Delete | View |
Has Inspection Method | View, Insert, Update, Delete | View |
Has Inspection Profile | View, Insert, Update, Delete | View |
Has Inspection Scope | View, Insert, Update, Delete | View |
Has Inspections | View, Insert, Update, Delete | View |
Has Potential Degradation Mechanisms | View | View |
Has Recommendations | View, Insert, Update, Delete | View |
Has Reference Documents | View, Insert, Update, Delete | View |
Has Roles | View, Insert, Update, Delete | View |
Has Sub-Inspections | View, Insert, Update, Delete | View |
Has Tasks | View, Insert, Update, Delete | View |
Has Task History | View, Insert | View |
Has Task Revision | View, Insert | View |
Has Team Member | View, Insert, Update, Delete | View |
Has Taxonomy Hierarchy Element | View | View |
Has Taxonomy Mapping | View | View |
Has Time Based Inspection Interval | View, Insert, Update, Delete | View |
Has Work Pack | View, Update, Insert, Delete | View |
Is a User | View | View |
Is Planned By | View, Insert, Update, Delete | View |
Is Executed By | View, Insert, Update, Delete | View |
Note that:
- The family-level privileges granted to the following families are also spread to all of their subfamilies:
- Event
- Taxonomy References
- The Has Task History relationship family is inactive in the baseline APM database.
- In addition to the families listed in the preceding table, members of the MI Inspection Security Group have View privileges to additional families to facilitate integration with the Risk Based Inspection module. Since these families are not used elsewhere in Inspection Management, they are not listed in this table.