Overview
Overview of Datasets
A dataset is a fixed set of information that is stored as a Catalog item.
More Details
Datasets contain information that can be viewed and modified in a grid. While queries return the most current information in the database, a dataset displays the same information until it is modified manually. For example, you might use a dataset to store information from an external system so that the data can referenced or used to create graphs in APM.
When a dataset is created, a data type is defined for each column to indicate the type of data that can be stored in cells in that column. When you create or modify a dataset, if you attempt to enter data that conflicts with the data type defined for that column, the data will not be retained. The following types of data can be stored in a dataset:
- Character : Stores alphanumeric data. Cells in columns of this data type will appear as text boxes in which you can enter letters, numbers, and symbols.
- Numeric : Stores numeric data. Cells in columns of this data type will appear as text boxes in which you can enter numbers.
-
Date
: Stores date and time data in the format MM/DD/YYYY. Cells in columns of this data type will display the
button, which can be selected to access a calendar from which a date can be selected. You can also enter dates directly into cells.
- Logical : Stores the value True or False. Cells in columns of this data type will appear as text boxes in which you can enter the value True or False.
You can create new datasets manually within APM , or by importing a Microsoft Excel file (.xlsx), an XML file (.xml), or a text file (.txt or .csv).
After you create a dataset, you can access it, modify it, use it to create graphs, and export it as a Microsoft Excel file, an XML file, or a text file.
About Creating Datasets by Importing Files
You can create a new dataset in APM by importing a Microsoft Excel file (.xlsx), an XML file (.xml), or a text file (.txt or .csv).
When importing a dataset, if you specify a Data Type for a column and that column contains values that are not supported by the selected Data Type, the entire column will be excluded from the dataset.
When importing a file, in the Modify Columns section, if you select the check box in the Unique Value column for a given column and the file that you are importing has the same value in multiple cells within that column, only the first row with a unique value will be imported into the dataset.
About Importing an Excel File
Microsoft Excel files with the file extension .xlsx can be imported to create a dataset. In a Microsoft Excel file, data is organized within grids, and can contain multiple worksheets. When importing a Microsoft Excel file, a dataset can be created only from a single worksheet. If you want to import multiple worksheets from a Microsoft Excel file, you must create a new dataset for each worksheet.
About Importing an XML File
Extensible Markup Language (XML) files that have the file extension .xml can be imported to create a dataset. XML files can be created in text editors, such as Notepad and Microsoft Word, but can also be opened and viewed in an Internet browser.
When importing an XML file, the following data types are supported:
- string: Used for columns that contain alphanumeric values. Columns of this type will be imported using the Character data type.
- double: Used for columns that contain numeric values and may include a - (negative sign) and decimal. Columns of this type will be imported using the Numeric data type.
- dateTime: Used for columns that contain date and time values. Date values should use the format YYYY-MM-DD, and time values should use the 24-hour time format THH:MM:SS (e.g., T14:30:23). Columns of this type will be imported using the Date data type.
- boolean: Used for columns that contain logical data. Data in these columns should be limited to the following values: True, 1, False, and 0. Columns of this type will be imported as a Logical data type.
Each row of the dataset is contained with a Table tag. The attributes within the Table tag correspond to the column names defined via the xs:attribute tags.
About Importing a Text File
Text files with the extension .txt or .csv can be imported to create a dataset. These files contain lines of data that are delimited, or separated, by punctuation marks, with rows of data separated by line breaks.
APM accepts the following characters as delimiters:
- , (comma).
- ; (semicolon).
- | (pipe character).
To maintain the structure of the dataset, delimiters must be used throughout the file, even for cells that do not contain values. To identify an empty cell, you would need to include two consecutive delimiters (e.g., A,B,,D,E).
About Dataset Modification
After you access a dataset, or before you save when creating a dataset manually in APM or creating a dataset by importing a file, you can modify the dataset. It is important to understand APM's capabilities and limitations when modifying datasets.
Details
On the page displaying a dataset, the dataset is displayed as a grid. You can specify column names only during the creation of a dataset; once the dataset is created, the number of columns in the dataset and the names of those columns cannot be altered.
If you need to modify the information contained in a dataset, you can do so in the following ways:
- Modify the data in a cell.
- Add rows.
- Delete rows.
- Move a column by selecting it and dragging it to the desired position.
After a dataset exists in APM, if you need to modify the column structure or the data type of a column, you can perform the following steps:
- Export the dataset.
- Perform the necessary modifications.
- Import the updated file to create a new dataset.
Access the Dataset Page
Procedure
Create a Dataset in APM
About This Task
The following instructions describe how to create a dataset manually within APM. You can also create a dataset by importing a file.
Procedure
Create a Dataset by Importing a File
About This Task
The following instructions describe how to create a dataset by importing a file. You can also create a dataset manually within APM .
Procedure
Access a Dataset
Procedure
Modify a Dataset
Procedure
Save a Dataset
Before You Begin
Saving a dataset is the final step of the process when you create a dataset in APM , create a dataset by importing a file, or modify a dataset. To save a dataset, you should follow one of those procedures, and then complete the steps described in this topic.
Procedure
- If you are creating a dataset:
- If you are modifying a dataset and want to overwrite that dataset's previously saved data:
- If you are modifying a dataset and want to save the modified dataset as a new Catalog item: