Overview
Overview of Data Sources
A data source stores the connection information for a APM database and allows users to access that database. When you log in to APM, you will select the data source that corresponds to the APM database that you want to use.
Data sources are associated with a specific APM Server to indicate which databases are accessible from that server.
Connection information about data sources is stored in MeridiumDatasources.xml, which exists on the APM Server in the C:\ProgramData\Meridium folder. This file is created automatically when you install or upgrade the APM Server. When it is first created during a new installation, it will be empty. It will be updated automatically as you create, modify, and delete data sources.
Note: Data source passwords are encrypted in the file.
Access the Data Sources Page
Procedure
In the Applications menu, navigate to
.
The Data Sources page appears, displaying a list of existing data sources.
Create a Data Source
Procedure
Results
- The new data source appears in the left pane and will appear in the APM login page. Additionally, after saving the data source, the button will appear next to the button to test the connection.