Data Loaders
Download the Data Loader Workbooks
Procedure
Results
Run a Data Import Job
Before You Begin
Procedure
Results
Process Activity Stages
The Process Activity column in the Data Bundles Status page displays the process state management of the various Data Loader jobs that are running or have run in the APM system.
- Prepare: Preparing stage involves Registering, Collecting, Transforming and Transmitting states
- Process: Process stage involves Normalizing, Compiling and Slicing states
- Ingest: Ingest stage involves Ingesting, Synchronizing and Notifying states
The following table contains the list of available stages and status mapping with description:
Process Stage | Status | Description |
---|---|---|
Prepare – Transmitting | In Progress / Failure | The data upload job status is in either In Progress or Failure and the process activity is in Transmitting state of Prepare stage. |
Process – Normalize | In Progress / Failure | The data upload job status is in either In Progress or Failure and the process activity is in Normalizing state of Process stage. |
Process – Compiling | In Progress / Failure | The data upload job status is in either In Progress or Failure and the process activity is in Compiling state of Process stage. |
Process – Slicing | In Progress / Failure | The data upload job status is in either In Progress or Failure and the process activity is in Compiling state of Slicing stage. |
Ingest – Ingesting | In Progress / In Progress with Rejects / Failure | The data upload job status is in either In Progress or In Progress with Rejects or Failure and the process activity is in Ingesting state of Ingest stage. |
Ingest – Synchronizing | In Progress / In Progress with Rejects / Failure / Complete with Rejects / Complete | The data upload job status is in either In Progress or In Progress with Rejects or Failure and the process activity is in Synchronizing state of Ingest stage. |
Done | Complete with Rejects / Complete | The data upload job status is in either Complete or Complete with Rejects and all process activities are Done state. |
Access the Data Bundle Execution Details of an Import Job
Before You Begin
This topic assumes that you have successfully ingested the Data Bundle Execution.
Procedure
Results
Details of the Data Bundle Execution
When you select a job in the Data Bundles Status page, the data import details page appears displaying the detailed import status and the progress of the selected data import job.
The Data Bundle Execution Details page displays the following sections:
Worksheet Field | Description |
---|---|
Overall Job Status |
The section displays the overall details of the job such as Asset name, Status, File name, Start Time, End Time, Bundle ID, and Progress Bar that displays the Process Stage. |
Summary of the Records Processed |
The section displays the summary of the processed records (# of Insert, Delete, Update, Reject and Total Records) in a donut chart. It also displays the System Errors in the job processing, if any. |
System Errors |
The section displays the System errors occurred during processing of the job. |
Rejected Rows |
The section displays all the records that are rejected while processing the job. The details include Sheet Name, Row #, Primary Record Id, Slice ID, Error Code, Message, Timestamp, Data. Select a record to view the full data of the record. You can download the Rejected record data into an .xlsx file using the Export Current Page option available in the Rejected Rows section. |
Event Timeline | The section displays the process activity event timelines. The details include Timestamp, Process state of Step, Status, Message (displays system errors, if any). |
Refresh |
You can use the Refresh option for setting the frequency of refreshing the page (Off, 30 sec, 1 min, 5 min and 10 min). Also, you can manually refresh the page. |
Export the Rejected Data Details of an Import Job
Procedure
- Access the Data Bundle Execution Details of an Import Job.
- In the Rejected Rows section, select
and then select Export Current Page to download the details of the rejected data during the import job.