Upgrade
Upgrade or Update Advanced Visualization to V5.1.3.0.0
The following table provides you the reference to procedures to upgrade from an earlier APM version to the latest version.
Upgrade from | Upgrade to | Procedure |
---|---|---|
V5.1.x | V5.1.3.0.0 | Upgrade from any version V5.1.0.0.0 through V5.1.2.1.0 |
V5.0.x | V5.1.3.0.0 | Upgrade from any version V5.0.1.0.0 through V5.0.5.0.0 |
Upgrade from any version V5.1.0.0.0 through V5.1.2.1.0
This module will be upgraded to V5.1.3.0.0 automatically when you upgrade the components in the basic APM system architecture. No additional steps are required.
If an error occurs, delete the following folders:
- C:\Program Files (x86)\InstallShield Installation Information\<UUID>
- C:\Meridium\temp
Upgrade from any version V5.0.1.0.0 through V5.0.5.0.0
This module will be upgraded to V5.1.3.0.0 automatically when you upgrade the components in the basic APM system architecture. No additional steps are required.
If an error occurs, delete the following folders:
- C:\Program Files (x86)\InstallShield Installation Information\<UUID>
- C:\Meridium\temp