Custom Device
SIS Management: Custom Device Workflow
This workflow describes the process of defining a custom device.
In the following workflow diagram, the blue text in a shape indicates that the corresponding description has been provided in the sections that follow the diagram. For more information, refer to the Interpreting the Workflow Diagrams topic in the APM Product Workflows documentation.
Note: For information on the personas associated with a GE Digital APM module, refer to the APM Product Workflows documentation.

Create Custom Device
Persona: Analyst
Create a Custom Device to store the details of the sensor, logic solver, or final element that you want to use.
Select Device from SERH
Persona: Analyst
Select the devices from SERH that make up the custom device. You can create a device with failure rates based on the operating data in your facility. You can also add multiple elements (e.g., valve, solenoid, actuator, quick exhaust) to a device that you plan to reuse in the design of other protective loops.
Provide Device Details and Failure Rates
Persona: Analyst
Provide the custom device details and failure rates.
Approve Custom Device
Persona: Analyst
Approve the custom device so that it can be used in a Protective Instrument Loop.
SIL Verification
Persona: Analyst
Go to the SIL Verification workflow.