Data Loader

About the Rounds Data Loaders

You can use the Rounds Data Loaders to import content into the Rounds module in bulk.

The Rounds Data Loaders are used to create both records in the following families and relevant relationships between them:

  • Rounds Allowable Values Data Loader
    • Allowable Value
  • Rounds Templates Data Loader
    • Template Group
    • Measurement Location Template
    • Lubrication Requirement Template
    • Checkpoint Template Sequence
    • Checkpoint Condition
  • Rounds Routes Data Loader
    • Route
    • Measurement Location
    • Lubrication Requirement
    • Checkpoint Task
    • Checkpoint Condition
  • Rounds Readings Data Loader
    • Reading

About the Rounds Data Loaders Requirements

This documentation assumes that your organization has completed the deployment of the Rounds module. The Rounds Data Loaders should be used only after the Rounds module has been implemented.

Security Settings

The Security User performing the data load operation must be associated with either the MI Data Loader User or MI Data Loader Admin Security Role, and must also be associated with the MI Operator Rounds Administrator Security Group or a Security Role that is associated with this Security Group.

Assumptions

  • All imported date values are in UTC.
  • Functional Locations and/or Equipment have already been loaded into GE Digital APM.
  • Blank values are not copied to the entities. If there are blank values, those fields will be skipped.
  • No customization (that is, rules changes) is done on the related families that override the baseline families.

About the Rounds Data Loaders Data Models

The following data models detail the elements of data and their relationships in the Routes and Readings Data Loaders and the Template Data Loader.

Rounds Routes and Reading Data Loader Data Model

The following data model illustrates the Routes and Readings Data Loaders:



Rounds Template Data Loader Data Model

The following data model illustrates the Template Data Loader:



About the Rounds Data Loaders General Loading Strategy

This section describes any prerequisites to loading the data and the order in which the data will be loaded.

Note: Before reading this section, review the Data Model section.

Data Import

When importing data using the Rounds Data Loaders:

  • You must use the data loader workbook while considering the rules described in Workbook Layout and Use.
  • The current version of the Rounds Data Loaders can process insertion of up to approximately 500 Measurement Location and Lubrication Requirement records for a single Route record per workbook. When updating existing records, up to approximately 500 Measurement Location and Lubrication Requirement records can be processed for a single Route record per workbook.

Limitations

Due to performance limitations in Rounds Designer, it is recommended that Template Groups contain no more than 150 Measurement Location Templates in a single data load.

Schedule and Date Fields

  • The Rounds Data Loaders require that Schedule values are expressed using the JSON format used in the GE Digital APM database. Valid schedule expressions may be easily generated via the schedule setting feature on a schedule field in a Route or Checkpoint Task record in Record Manager, and then copying the resulting text value to the worksheet.
  • The Route Data Loaders use a non-standard date format. Data should be formatted as yyyy-mm-dd hh-mm-ss (for example, 2015-05-23 17-45-34).

  • All date values are assumed to be in UTC. The time zone of the user loading the data is not relevant.

Prerequisites

  • If you are not using the standard asset hierarchy (Functional Location / Equipment), the Rounds module is configured with the required relationships to any other asset families, and the asset hierarchy is configured to use these families.
  • The sites to which Rounds records are to be assigned have been created.
  • Users to whom Routes will be assigned have both Security User and Human Resource records.
  • Any customization related to the imported families (that is, added fields, custom rules, family policies, etc., which are to be relied upon during the import process) is completed and tested.
  • All custom Unit of Measure values have been added to the global UOM list and UOM conversion sets.
    Note:

    Rounds does not use the Units of Measure Conversions feature. The system code table UOME is the only source for populating drop-down list values within UOM fields.

    The UOM field for a Measurement Location contains all the values from the UOME system code table, sorted by their descriptions.

    The UOM field for a Lubrication Requirement contains a subset of values from the UOME system code table based on specific reference values from the MI_LM_REFERENCES system code table.

  • Licenses for Rounds (that is, the Operator Rounds or Lubrication Management license) and any level of APM Connect are active.
  • If you want Health Indicators to be created automatically for Measurement Locations that are linked to assets, then the Asset Health Indicator Service must be configured and started. Note that Health Indicators can be added or removed at any time in Asset Health Manager Administration.

Load Sequence

When importing data using the Rounds Data Loaders, use the following workflow:

  1. Download the template workbooks provided by GE Digital APM
  2. Identify data requirements.
  3. Extract data from legacy applications to populate the data loader workbook.
  4. Load data using the Rounds Allowable Values Data Loader.
  5. Verify import logs and ensure that all required Allowable Values are loaded successfully.
  6. Load data using the Rounds Templates Data Loader.
  7. Verify import logs and ensure that all required ML Templates, LR Templates, and Template Groups are loaded successfully.
  8. Load data using the Rounds Routes Data Loader.
  9. Verify import logs and ensure that all required MLs, LRs, and Routes are loaded successfully.
  10. Load data using the Rounds Readings Data Loader.
  11. Verify import logs and ensure that all required Readings are loaded successfully.
  12. Conduct tests in GE Digital APM to ensure that the imported data loaded properly.

About the Rounds Data Loader Workbooks Layout and Use

Overview of Rounds Data Loader Workbooks

This section provides a high-level overview and explanation of how the data loader workbooks are constructed.

In order to import data using the Rounds Data Loaders, GE Digital provides separate data loader workbooks for:

  • Rounds Allowable Values.
  • Rounds Templates.
  • Rounds Routes.
  • Rounds Readings.

The workbooks support the baseline Rounds functionality in GE Digital APM. The workbooks must be used to perform the data load. You can modify the data loader workbooks to include custom fields used by your organization.

Each data loader workbook contains one worksheet for each node that will be populated in the data model.

Each worksheet in these data loader workbooks contain field values that must be mapped to the appropriate GE Digital APM family/field combination. The individual sections in this document specify the source and target fields and relationships required between predecessors and successor.

The list of fields tabulated is not exhaustive. The user can add additional field columns to the worksheets and, provided that the field columns are properly mapped within the worksheets, the upload will still be successful.

Data Loader Batch Fields

The Rounds Data Loaders workbooks include columns of data that are used to identify batches of related records. These values are not imported to a field in the GE Digital APM database. Generally, these will be the first few columns in each worksheet. They each use a prefix that identifies the relevant record type being imported, whereas columns that will be imported have IDs that match the field IDs in GE Digital APM, which generally use the prefix MI_.

Rounds Allowable Values Data Loader Workbook

When importing data using the Rounds Allowable Values Data Loader, the data loader will create one Allowable Value record for each row of the worksheet. If the import worksheet specifies an Allowable Value that is an exact match for an existing record, the record is not imported. Since the unique identification of an Allowable Value record includes all its fields, it is not possible to update existing Allowable Value records using the data loader.

Note: Allowable Values records do not support Site Filtering.

On the worksheet, you will specify the allowable values that will be used in Measurement Location Templates and Measurement Locations.

Field Caption

Field ID

Data Type (Length)

Comments

Allowable Value Batch ID

OPR_AL_VL_ID

Character (50)

This field is required for identification during the data load process and must be unique. The value in this field is not imported to GE Digital APM.

Type

MI_OPR_AL_VL_TYPE_CHR

Character (50)

This field is required. The valid values for this field are:

  • Character
  • Numeric

Category

MI_OPR_AL_VL_CATEG_CHR

Character (50)

This field is required.

Value

MI_OPR_AL_VL_VALUE_CHR

Character (50)

This field is required.

Rounds Templates Data Loader Workbook

When importing data using the Rounds Templates Data Loader, the data loader will create records as follows:

  • Template Groups: The data loader will create one Template Group record for each row in the import worksheet. If the Template Group ID specified matches the Template Group ID of an existing Template Group, the existing record will be updated.

    The Template Groups will be loaded into GE Digital APM, and will be filtered based on the designated site name in the Site Reference Name field.

    Note: If you want to set the site reference to be a Global Site Reference, enter the constant ‘*Global*’ in the MI_SITE_NAME column on the spreadsheet.

    The following site inheritance rules are applied when Template Groups are created using the data loader:

    • For the Template Groups where the site reference is set to Global, the Template Groups can contain ML Templates for any Site, and Global ML Templates.
    • For the Template Groups where the site reference is assigned to Site X, the Template Groups can contain Global ML Templates and ML Templates with Site X.
    • When a Global Template Group is applied to a asset assigned to Site X, only the Global ML Templates and Site X ML Templates will be applied.
  • Measurement Location Templates: The data loader will create one Measurement Location Template record for each row in the data loader workbook. If the import worksheet specifies a Template ID value that matches the Template ID of an existing Measurement Location Template record, the existing record will be updated. If the worksheet specifies values for Category or Allowable Value that do not already exist in the database for the specified type (numeric or character) of Measurement Location, the record will not be imported.

    The Measurement Location Templates will be loaded into GE Digital APM, and will be filtered based on the designated site name in the Site Reference Name field.

  • Checkpoint Template Sequence: The data loader will create one Checkpoint Template Sequence record for each row in the worksheet. Since the unique identification of a Checkpoint Template Sequence record includes all its fields, it is not possible to update existing Checkpoint Template Sequence records using the Rounds Templates Data Loader. Updates to existing Template Groups to add or reorder the related Measurement Location Templates must be performed using the Rounds Designer user interface.

    Each Checkpoint Template Sequence record will take the same Site Reference Name that is designated to the Template Group to which it is assigned.

  • Checkpoint Conditions: The data loader will create one Checkpoint Condition record for each row in the Checkpoint Condition worksheet. This worksheet defines the conditions under which the successor Checkpoints for Checkpoint Conditions are displayed in Rounds Data Collection. This worksheet also works together with the Measurement Location worksheet to determine the Checkpoint sequence for Template Groups with Checkpoint Conditions.

    The values specified in the CPC ID field in this worksheet are used by the Checkpoint Template Sequence worksheet to specify when Checkpoints have predecessor Checkpoint Conditions. Additionally, this worksheet uses the values specified in the CTS ID field in the Checkpoint Template Sequence worksheet to specify predecessor Checkpoints for Checkpoint Conditions.

    Note: For more details regarding how to create a Template Group with Checkpoint Conditions using the Rounds Templates Data Loader, see the Example Rounds Templates Data Loader Workbook with Checkpoint Conditions section.
Table 1. Worksheets in Rounds Templates Data Loader Workbook
WorksheetDescription
Template Group Worksheet (MI_DTACLTMP)This worksheet is used to specify the Template Groups.
Measurement Location Worksheet (MI_ML_TMPLT)This worksheet is used to specify Measurement Location Templates that will be related to Template Groups. Note that no relationships are created when this worksheet is imported. The arrangement of Measurement Location Templates is defined by Checkpoint Template Sequence records which are created when the next worksheet is imported.
Checkpoint Template Sequence Worksheet (MI_HSCPTMP)This worksheet is used to specify Checkpoint Template Sequence records that define how ML Templates are arranged into Template Groups. Note that an ML Template can appear in multiple Template Groups, and it can appear in a Template Group more than once.
Lubrication Requirement Worksheet (MI_LR_TMPLT)This worksheet is used to define Lubrication Requirement Templates. Note that no relationships are created when this worksheet is imported.
Checkpoint Condition Worksheet (MI_CHKPCOND)This worksheet is used to specify Checkpoint Conditions that will be related to Checkpoints in Template Groups.

Template Group Worksheet (MI_DTACLTMP)

Field CaptionField IDData Type (Length)Comments
Template Group Batch IDROUNDS_MLTG_IDCharacter (50)This field is required for identification during the data load process and must be unique. The value in this field is not imported to GE Digital APM.
IDMI_DTACLTMP_ID_CCharacter (50)This field is required and must be unique.
Site Reference Name MI_SITE_NAMECharacter (50)This field is required and must match an existing Site name.
Note: If you want to set the site reference to be a Global Site Reference, enter the constant ‘*Global*’ in the MI_SITE_NAME column on the spreadsheet.
DescriptionMI_DTACLTMP_DESCR_CCharacter (255)Please provide a brief description.

Measurement Location Worksheet (MI_ML_TMPLT)

Field CaptionField IDData Type (Length)Comments
Template Group Batch IDROUNDS_MLTG_IDCharacter (50)This field is required for identification during the data load process. It should match the ID of the Template Group to which the ML Template will be linked. Use <Dummy ID> if you want to import standalone records not linked to a Template Group. The value in this field is not imported to GE Digital APM.
Template Item IDROUNDS_MLT_IDCharacter (50)This field is required for identification during the data load process. The value in this field is not imported to GE Digital APM.
Template IDMI_ML_TMPLT_TEMPL_ID_CCharacter (50)This field is required and must be unique.
ML TypeMI_ML_TMPLT_MEAS_LOC_TYPE_CCharacter (50)This field is required. The valid values for this field are:
  • Character
  • Numeric
Site Reference NameMI_SITE_NAMECharacter (50)This field is required and must match an existing Site name.
Note: If you want to set the site reference to be a Global Site Reference, enter the constant ‘*Global*’ in the MI_SITE_NAME column on the spreadsheet.
DescriptionMI_ML_TMPLT_DESC_CCharacter (255)Please provide a brief description.
Unit of MeasureMI_ML_TMPLT_UOM_CCharacter (50)Must be a valid value in the global Unit of Measure list. Disabled if the ML Type field is Character.
StatusMI_ML_TMPLT_STAT_CCharacter (50)The default value for this field is Active.
ScheduleMI_ML_TMPLT_SCHEDULE_CCharacter (255)If specified, must be valid JSON Schedule.
Checkpoint LockedMI_CP_TMPLT_LOCKED_LBooleanThe default value for this field is False.
Requires Equipment ShutdownMI_CP_TMPLT_REQU_EQUI_SHUT_FLGLogicalThe default value for this field is False.
CategoryMI_ML_TMPLT_CATEG_CCharacter (50)All specified values must match the Category field in pre-existing Allowable Value records where the Category and Type match the Category and ML Type defined for this ML.
Allowable ValuesMI_ML_TMPLT_ALLOW_VAL_CMulti-value, max 10 values, Character (255)All specified Values must match the Value field in pre-existing Allowable Value records where the Category and Type match the Category and ML Type defined for this MLT. The | (pipe) character is used to separate each allowable value.
Lower Level 1 ActionMI_ML_TMPLT_LO_LVL1_ACT_CCharacter (50)None
Lower Level 1 Character ValueMI_ML_TMPLT_LO_LVL1_ALRT_CCharacter (50)Must use one of the Allowable Values specified for the MLT. This field is disabled if the ML Type field is Numeric.
Lower Level 1 Numeric Value*MI_ML_TMPLT_LO_LVL1_ALRT_NNumericNone. This field is disabled if ML type field is Character.
Lower Level 1 MessageMI_ML_TMPLT_LO_LVL1_MSG_CCharacter (50)None
Lower Level 2 ActionMI_ML_TMPLT_LO_LVL2_ACT_CCharacter (50)None
Lower Level 2 Character ValueMI_ML_TMPLT_LO_LVL2_ALRT_CCharacter (50)Must use one of the Allowable Values specified for the MLT. This field is disabled if the ML Type field is Numeric.
Lower Level 2 Numeric Value*MI_ML_TMPLT_LO_LVL2_ALRT_NNumericNone. This field is disabled if ML type field is Character.
Lower Level 2 MessageMI_ML_TMPLT_LO_LVL2_MSG_CCharacter (50)None
Lower Level 3 ActionMI_ML_TMPLT_LO_LVL3_ACT_CCharacter (50)None
Lower Level 3 Character ValueMI_ML_TMPLT_LO_LVL3_ALRT_CCharacter (50)Must use one of the Allowable Values specified for the MLT. This field is disabled if the ML Type field is Numeric.
Lower Level 3 Numeric Value*MI_ML_TMPLT_LO_LVL3_ALRT_NNumericNone. This field is disabled if ML type field is Character.
Lower Level 3 MessageMI_ML_TMPLT_LO_LVL3_MSG_CCharacter (50)None
Upper Level 1 ActionMI_ML_TMPLT_UP_LVL1_ACT_CCharacter (50)None
Upper Level 1 Character ValueMI_ML_TMPLT_UP_LVL1_ALRT_CCharacter (50)Must use one of the Allowable Values specified for the MLT. This field is disabled if the ML Type field is Numeric.
Upper Level 1 Numeric Value*MI_ML_TMPLT_UP_LVL1_ALRT_NNumericNone. This field is disabled if ML type field is Character.
Upper Level 1 MessageMI_ML_TMPLT_UP_LVL1_MSG_CCharacter (50)None

Upper Level 2 Action

MI_ML_TMPLT_UP_LVL2_ACT_C

Character (50)

None

Upper Level 2 Character Value

MI_ML_TMPLT_UP_LVL2_ALRT_C

Character (50)

Must use one of the Allowable Values specified for the MLT. This field is disabled if the ML Type field is Numeric.

Upper Level 2 Numeric Value*

MI_ML_TMPLT_UP_LVL2_ALRT_N

Numeric

None. This field is disabled if the ML Type field is Character.

Upper Level 2 Message

MI_ML_TMPLT_UP_LVL2_MSG_C

Character (50)

None

Upper Level 3 Action

MI_ML_TMPLT_UP_LVL3_ACT_C

Character (50)

None

Upper Level 3 Character Value

MI_ML_TMPLT_UP_LVL3_ALRT_C

Character (50)

Must use one of the Allowable Values specified for the MLT. This field is disabled if the ML Type field is Numeric.

Upper Level 3 Numeric Value*

MI_ML_TMPLT_UP_LVL3_ALRT_N

Numeric

None. This field is disabled if ML type field is Character.

Upper Level 3 Message

MI_ML_TMPLT_UP_LVL3_MSG_C

Character (50)

None

Product

MI_ML_TMPLT_PRODUCT_C

Character (50)

None

Minimum Valid Value

MI_ML_TMPLT_MIN_VLDVAL_N

Numeric

None. This field is disabled if ML type field is Character.

Maximum Target Value

MI_ML_TMPLT_MAX_TRGVAL_N

Numeric

None. This field is disabled if ML type field is Character.

Minimum Target Value

MI_ML_TMPLT_MIN_TRGVAL_N

Numeric

None. This field is disabled if ML type field is Character.

Maximum Valid Value

MI_ML_TMPLT_MAX_VLDVAL_N

Numeric

None. This field is disabled if ML type field is Character.

More Information

MI_ML_TMPLT_MORE_INFO_C

Character (255)

None

* For a Numeric ML Template, the limit values must be in descending order (that is, lower level 3<lower level 2<lower level 1<upper level 1<upper level 2<upper level 3).

Checkpoint Template Sequence Worksheet (MI_HSCPTMP)

Field CaptionField IDData Type (Length)Comments
Template Group Batch IDROUNDS_MLTG_IDCharacter (50)This field is required for identification during the data load process. It must match the ID of the Template Group to which the Checkpoint Template Sequence record will be linked. The value in this field is not imported to GE Digital APM.
CTS IDCTS_IDCharacter (50)

This field is required for Conditions under this Checkpoint template.

It defines the CTS ID to be specified in the MI_CHKPCOND_PRED_KEY_N column of the Checkpoint Conditions (MI_CHKPCOND) sheet in the current data loader workbook.

This field is used only during the data load process and must be unique.

The value in this field is not imported to GE Digital APM.

Group ID/Predecessor CTC IDMI_HSCPTMP_PRED_ENTY_KEY_NCharacter (50)This field is required.
  • If the Checkpoint does not have a predecessor Checkpoint Condition, you should specify the Predecessor Template Group ID as defined in the ROUNDS_MLTG_ID column of the Template Groups sheet in the current data loader workbook. The data loader will automatically populate the field on the record with the relevant Entity Key.
  • If the Checkpoint does have a predecessor Checkpoint Condition, specify the CTC ID for the predecessor Checkpoint Condition in this field.
Template IDMI_HSCPTMP_SUCC_ENTY_KEY_NCharacter (50)This field is required.

You should specify the Template ID as defined in the MI_ML_TMPLT_TEMPL_ID_C or MI_ML_TMPLT_TEMPL_ID_C column of the Measurement Location (MI_ML_TMPLT) or Lubrication Requirement (MI_LR_TMPLT) worksheet, respectively, in the current data loader workbook. The data loader will automatically populate the field in the record with the relevant Entity Key.

SequenceMI_HSCPTMP_SEQ_NNumericThis field is required and must be unique within the collection of Checkpoint Template Sequence records associated with any Template Group.
Template Group IDMI_HSCPTMP_REL_TMPG_KEY_NNumericThis field is required for identification during the data load process and must match the ID of the template group to which the Checkpoint Template Sequence is being applied.

The value in this field is not imported to GE Digital APM.

Checkpoint Condition Worksheet (MI_CHKPCOND)

Field CaptionField IDData Type (Length)Comments
Template Group Batch IDROUNDS_MLTG_IDCharacter (50)

This field is required for identification during the data load process. It must match the ID of the Template Group to which the Checkpoint Template Sequence record will be linked.

The value in this field is not imported to GE Digital APM.

CPC IDCPC_IDCharacter (50)This field defines the ID for the Checkpoint Condition. If you want to include conditions in your template, this field is required and must be unique.
Predecessor CTS IDMI_CHKPCOND_PRED_KEY_NNumericUse this field to determine the predecessor Checkpoint for the Checkpoint Condition.

This field specifies the Checkpoint Template Sequence ID (CTS ID) defined in the Checkpoint Template Sequence worksheet for the predecessor Checkpoint.

Sequence NumberMI_CHKPCOND_SEQ_NUM_NNumericThis field defines the sequence for sibling Checkpoint Conditions (that is, Checkpoint Conditions with the same Predecessor CTS ID). If you are adding a Checkpoint Condition for the first time:
  • If no value is specified in this field, a value will be automatically assigned to the Checkpoint Condition during the data load process.
  • If you specify a value in this field, the sequence that you specify will be used to determine the order of sibling Checkpoint Conditions.

If you are updating an existing Checkpoint Condition:

  • If no value is specified in this field, the existing sequence will remain intact.
  • If you specify a value in this field, the sequence that you specify will be used to determine the order of sibling Checkpoint Conditions.
Template Group IDMI_HSCPTMP_REL_TMPG_KEY_NNumeric

This field is required for identification during the data load process and must match the ID of the template group to which the Checkpoint Template Sequence is being applied.

The value in this field is not imported to GE Digital APM.

Field NameMI_CHKPCOND_FLD_NAM_CCharacter (50)This field behaves differently depending on whether the Predecessor CTS ID refers to a Measurement Location or a Lubrication Requirement:
  • If the Predecessor CTS ID refers to a Measurement Location, this field specifies the category for the Measurement Location.
  • If the Predecessor CTS ID refers to a Lubrication Requirement, this field specifies the lubricant type for the Lubrication Requirement.
Field Value for Character TypeMI_CHKPCOND_FLD_VAL_CHAR_CCharacter (250)This field specifies the reading value that, for a predecessor Measurement Location with an ML Type of Character, determines whether the condition has been met to display successor Checkpoints.
Field Value for Numeric TypeMI_CHKPCOND_FLD_VAL_NUM_NNumericThis field specifies the reading value that, for a predecessor Measurement Location with an ML Type of Numeric, determines whether the condition has been met to display successor Checkpoints.
Possible ConditionMI_CHKPCOND_POSS_COND_CCharacter (200)

This field specifies the relationship between the predecessor Checkpoint value and the value in the Checkpoint Condition Field Value field that determines whether to display successor Checkpoints in Rounds Data Collection.

If the predecessor Checkpoint has a Type value of Numeric, enter one of the following values:

  • <
  • <=
  • =
  • >=
  • >

If the predecessor Checkpoint has a Type value of Character, enter the following value in this field: is.

TypeMI_CHKPCOND_TYPECCharacter (50)This field is required. The valid values for this field are:
  • Character
  • Numeric

Lubrication Requirement Worksheet (MI_LR_TMPLT)

Field Caption

Field ID

Data Type (Length)

Comments

Template Group Batch ID

ROUNDS_MLTG_ID

Character (50)

Lubrication Requirement records can be created without being linked to a Route by specifying <Dummy ID> as the Route ID and the Route Batch ID as 1000000000. The value in this field is not imported to GE Digital APM.

You can create orphan Lubrication Requirement Templates using this DL.

Template Item ID

ROUNDS_LRT_ID

Character (50)

This field is required for identification during the data load process. The value in this field is not imported to GE Digital APM.

Template ID

MI_ML_TMPLT_TEMPL_ID_C

Character (50)

This field is required and must be unique.

LR Type

MI_LR_TMPLT_LR_TYPE_C

Character (50)

This field is required. The valid values for this field are:

  • Character
  • Numeric

Description

MI_ML_TMPLT_DESC_C

Character (255)

Please provide a brief description.

Unit of Measure

MI_ML_TMPLT_UOM_C

Character (50)

The field must be a valid value in the global Unit of Measure list. This field is disabled if the LR Type field is Character.

StatusMI_ML_TMPLT_STAT_CCharacter (50)The valid values for this field are Active or Inactive. This field is set to Active by default.
ScheduleMI_ML_TMPLT_SCHEDULE_C

Character (255)

If specified, must be valid JSON Schedule.

Checkpoint LockedMI_CP_TMPLT_LOCKED_L

Logical

The default value for this field is False.

Requires Equipment ShutdownMI_CP_TMPLT_REQU_EQUI_SHUT_FLGLogicalThe default value for this field is False.
LubricantMI_LR_TMPLT_LUBR_CCharacter (50)This field must be a pre-existing Lubricant value in the Lubricant family where the Method and Manufacturer are as specified for this LR Template.
Number of PointsMI_LR_TMPLT_NO_OF_POINTS_NNumericNone
CapacityMI_LR_TMPLT_CAP_NNumericNone
QuantityMI_LR_TMPLT_QTY_NNumericNone
MethodMI_LR_TMPLT_METHOD_CCharacter (50)This field must be a pre-existing Method defined in a Lubricant record.
Skip ReasonMI_LR_TMPLT_SKIP_REAS_CCharacter (50)None
Change Out Triggers Update?MI_LR_TMPLT_CH_OUT_TRIG_UPD_L

Logical

The default value for this field is False.

ComponentMI_LR_TMPLT_COMP_CCharacter (50)None
Lubricant ManufacturerMI_LR_TMPLT_LUBR_MFR_CCharacter (50)None
Capacity Unit Of MeasureMI_LR_TMPLT_CAPTY_UOM_CCharacter (50)None
PriorityMI_LR_TMPLT_PRIOR_CCharacter (50)None

Rounds Routes Data Loader Workbook

When importing data using the Rounds Routes Data Loader, you can:

  • Create Route, Measurement Locations, Lubrication Requirement and Checkpoint Task records.
  • Assign or unassign a Security User to the Route.

When importing data using the Rounds Routes Data Loader, this data loader will create records as follows:

  • Routes: The data loader will create one Route record for each row in the Route worksheet. The Next Date field on the Route record is populated automatically by existing rules based on the value in the Schedule column. The user can however overwrite the Next Date Value by providing a value in the worksheet. If the Schedule is invalid, the Route record will not be created. The Route ID column in the data loader is used for identifying the Routes. If a Route with this ID is already present in the database, it will update the Route.

    The Route created will be loaded into GE Digital APM, and will be filtered based on the designated site name in the Site Reference Name field.

    Note: If you want to set the site reference, to be a Global Site Reference, enter the constant ‘*Global*’ in the MI_SITE_NAME column on the spreadsheet.
    Note: Adding a value in the Schedule column is not mandatory.
  • Security Users: The data loader will create relationships assigning each Route, identified by Route ID, to each Security User listed.

    When you specify a Route ID, only the corresponding users specified in this sheet will be assigned to the Route, regardless of whether other users were previously assigned to it.

    For example, if three users are listed, and you want five users to be listed (that is, you want to add two users), you must include all five users in the sheet. If you include only the two new users, the original three users will be removed from the Route.

    If you include a Route ID in this sheet with no Security Users listed, all existing user assignments will be removed.

    Note that the relationship created is between the Route and the Human Resource record linked to the Security User; therefore, the Human Resource records must already exist before the data loader is used.

  • Measurement Locations / Lubrication Requirement records / Checkpoint Tasks: The data loader will create one Measurement Location or a Lubrication Requirement record and one related Checkpoint Task record for each row of the Measurement Location import worksheet. Measurement Location records / Lubrication Requirement records are processed in batches using the Route ID. The MLs/ LRs are identified by the Checkpoint ID column. If a Measurement Location / Lubrication Requirement with this Checkpoint ID is already present in the database, then the ML will be updated.

    The Next Date, Non-compliance Date, and the Non-compliance Next Check Date fields on the Checkpoint Task record will be populated automatically by existing rules based on the value in the Schedule column. If the Schedule is invalid, the record will not be created.

    Note: Adding a value in the Schedule column is not mandatory.

    Each Measurement Location or Lubrication Requirement record will take the same Site Reference Name that is designated to the predecessor Asset. If there no Site Reference Name that is assigned to the Asset, the ML or LR takes the Site Reference Name from the Route to which the ML or LR is assigned.

  • Sequence Number: The User can provide the Sequence number for the Measurement Locations / Lubrication Requirement records under a Route in the Sequence column on the import worksheet. The data loader will consider the sequence provided and order the Measurement Locations / Lubrication Requirement records based on it. However, if there is any random / incorrect / blank / non-sequential numbers in this column, the data loader will correct them and place them sequentially while importing them. Any new insertion of Measurement Locations / Lubrication Requirement records under a Route will always be at the end of the Route with maximum sequence number under the Route. The data in the Sequence column is ignored when the Measurement Location / Lubrication Requirement record is standalone or the Measurement Location / Lubrication Requirement record is being updated.
    Note: Re-sequencing the Measurement Locations and Lubrication Requirements under a Route is possible using data loaders in V4.1.5.0. or later.

    The data loader will populate an Asset entity key into the new Measurement Location / Lubrication Requirement records, based on matching the value specified in the Related Asset Key column (that is, Functional Location ID for FLOCs or Equipment Technical Number for Equipment) in the Measurement Location import worksheet. If there is no Related Asset Key, it will use the related Asset ID field to search the Equipment and Functional Location families for a matching record and link it to the Measurement Location / Lubrication Requirement record and also populate the Related Asset Key.

    Note: The Asset ID is not required. If a matching Asset ID is not found, the ML is created without linking to any asset and a warning is added to the import log.
    • Provided that the Measurement Location / Lubrication Requirement record has received an Asset Key, the family rules will populate additional information in the Measurement Location / Lubrication Requirement records and create a relationship between the asset (predecessor) and Measurement Location / Lubrication Requirement records (successor).
    • The data loader will link each new Measurement Location / Lubrication Requirement record to an existing Route record that matches the value specified in the Route ID column. If a matching Route ID is not found, the records will not be created.
    • Standalone Measurement Locations / Lubrication Requirement records can be created without being linked to a Route by specifying <Dummy ID> as the Route ID and the Route Batch ID as 1000000000.
    • The data loader will link each Measurement Location / Lubrication Requirement record to the Action record which is specified by the Action ID column and is related to the Strategy record specified by the Strategy ID Column.

    If the Asset Health Indicator service is configured and started, Health Indicator records will be added automatically for each imported Measurement Location record that is linked to an Equipment or Functional Location.

    Note: Health Indicator records are not added for Lubrication Requirements, since there is no Health Indicator Mapping.
  • Checkpoint Conditions: The data loader will create one Checkpoint Condition record for each row in the Checkpoint Condition worksheet. This worksheet defines the conditions under which the successor Checkpoints for Checkpoint Conditions are displayed in Rounds Data Collection. This worksheet also works together with the Measurement Location worksheet to determine the Route sequence for Routes with Checkpoint Conditions.

    The following table shows the relationships between fields in this worksheet and fields in the Measurement Location worksheet that determine which Checkpoints precede or succeed which Checkpoint Conditions.

    Measurement location Worksheet FieldsCheckpoint Condition Worksheet Fields
    ML Identifier (ROUNDS_ML_ID)Parent ML Batch ID (PARENT_ROUNDS_ML_ID)
    Checkpoint ID (MI_CHECK_PT_CHEC_ID_C)Parent ML ID (MI_CHECK_PT_PR_CHEC_ID_C)
    Parent Condition Batch ID (MI_CHKPCOND_BATCH_ID)Condition Batch ID (MI_CHKPCOND_BATCH_ID_C)
    Parent Condition Identifier (MI_CHKPCOND_ID_C)Condition Identifier (MI_CHKPCOND_ID_C)

    When the values in the Parent ML Batch ID and Parent ML ID fields for a Checkpoint Condition match the values in the ML Identifier and Checkpoint ID fields, respectively, for a Checkpoint, this indicates that the Checkpoint Condition is a successor of the Checkpoint.

    When the values in the Condition Batch ID and Condition Identifier fields for a Checkpoint Condition match the values in the Parent Condition Batch ID and the Parent Condition Identifier fields, respectively, for a Checkpoint, this indicates that the Checkpoint Condition is a predecessor of the Checkpoint.

    Note: For more details regarding how to create a Route with Checkpoint Conditions using the Rounds Routes Data Loader, see the Example Rounds Routes Data Loader Workbook with Checkpoint Conditions section.
Table 2. Worksheets in Rounds Routes Data Loader Workbook
WorksheetDescription
Route Worksheet (MI_ROUTE000)This worksheet is used to specify Route records.
Security User Worksheet (MI_Security User)This worksheet is used to assign a security user for the Route identified by Route Id in each row in the Security User (MI_Security User) worksheet. You can also unassign all the Security Users from a Route by leaving the User ID field blank. You may leave all rows blank to make no Route assignment changes.
Measurement Location Worksheet (MI_MEAS_LOC)This worksheet is used to specify the measurement locations that will be linked to each Route. You can import Measurement Locations that are not linked to a Route by specifying <Dummy ID> for the Route ID. Note that Measurement Locations may be related to a Measurement Location Template. If one is specified, the values from the template will be used to populate the fields in the Measurement Location. Required values that are provided from the Measurement Location Template need not be specified again in this worksheet. If this worksheet specifies a value for any field that is populated from the Measurement Location Template, it will be over-written with the value from the Measurement Location Template.
Checkpoint Task Worksheet (MI_CP_TASK0)This worksheet is used to specify the schedule information to be added to the Checkpoint Task records that will be created for each Measurement Location that is imported. Note that it is not required to specify any data on this worksheet. If no data is specified, the Checkpoint Task records will be created with the schedule information from the Measurement Location Template specified in the related Measurement Location.
Checkpoint Condition Worksheet (MI_CHKPCOND)This worksheet is used to specify Checkpoint Conditions that will be related to Checkpoints in Rounds Routes.

Route Worksheet (MI_ROUTE000)

Field Caption

Field ID

Data Type (Length)

Comments

Route Batch ID

ROUNDS_ROUTE_ID

Character (50)

This field is required for identification during the data load process and must be unique. The value in this field is not imported to GE Digital APM.

Route Id

MI_ROUTE000_ROUTE_ID_C

Character (50)

This field is required and must be unique,

  • When you use the data loader to create Route, Measurement Locations and Checkpoint Task records.
  • When you use the data loader to create Route, Measurement Locations and Checkpoint Task records and assign the security users to Routes.
Note: This field is not required and may not be populated on this worksheet when you only assign or un-assign the security users to Routes.
Site Reference NameMI_SITE_NAMECharacter (50)

This field is required and must match an existing Site name

Note: If you want to set the site reference to be a Global Site Reference, enter the constant ‘*Global*’ in the MI_SITE_NAME column on the spreadsheet.

Route Description

MI_ROUTE000_ROUTE_DESC_C

Character (125)

Please provide a brief description.

Status

MI_ROUTE000_STAT_C

Character (50)

The valid values for this field are Active or Inactive. The default value for this field is Inactive.

Schedule

MI_ROUTE000_SCHED_C

Character (2000)

If specified, must be valid JSON Schedule definition.

Note: To enable users to copy the JSON schedule text, an alternative Route with schedule datasheet is provided showing the Schedule Text (copy/paste enabled) field.

Route Scan ID

MI_ROUTE000_BARCD_ID_C

Character (50)

This field is required and must be unique.

Next Date

MI_ROUTE000_NEXT_DATE_D

Date

UTC time formatted as yyyy-mm-dd hh:mm:ss.

Last Date

MI_ROUTE000_LAST_DATE_D

Date

UTC time formatted as yyyy-mm-dd hh:mm:ss.

Security User Worksheet (MI_Security User)

Field CaptionField IDData Type (Length)Comments
Route Batch IDROUNDS_ROUTE_IDCharacter (50)This field is required for identification during the data load process and must be unique. The value in this field is not imported to GE Digital APM.
Route Id MI_ROUTE000_ROUTE_ID_CCharacter (50)This field is required and must be unique. The field needs to be populated on this worksheet when you are assigning the security users to Routes.
User ID SEUS_IDCharacter (50)This field is required for assigning the User to the Route during the load process and must be unique. The Security User and the corresponding Human Resource records must already be part of the baseline database. If the field is left blank, the Route will be un-assigned.

Measurement Location Worksheet (MI_MEAS_LOC)

Field CaptionField IDData Type (Length)Comments
Route Batch IDROUNDS_ROUTE_IDCharacter (50)This field is required for identification during the data load process. It should match the ID of the Route to which the Measurement Location record will be linked. Use <Dummy ID> if you are importing standalone Measurement Location records. It is not imported to GE Digital APM.
ML IdentifierROUNDS_ML_IDCharacter (50)This field is required for identification during the data load process and must be unique. It is not imported to GE Digital APM.
Checkpoint IDMI_CHECK_PT_CHEC_ID_CCharacter (50)This field is required and must be unique. If the value matches an existing Checkpoint ID, the ML record will be updated, otherwise a new ML record will be created.
Parent Condition Batch IDMI_CHKPCOND_BATCH_IDCharacter (50)This field is required only if the Checkpoint has a parent Checkpoint Condition. If the Checkpoint has a predecessor Checkpoint Condition, this field is used for identification during the data load process and must match the batch ID of the predecessor Checkpoint Condition.

The value in this field is not imported to GE Digital APM.

Parent Condition IdentifierMI_CHKPCOND_ID_CCharacter (50)This field is required only if the Checkpoint has a parent Checkpoint Condition. If the Checkpoint has a predecessor Checkpoint Condition, this field is used for identification during the data load process and must match the ID of the predecessor Checkpoint Condition.

The value in this field is not imported to GE Digital APM.

ML TypeMI_MEAS_LOC_MEAS_LOC_TYPE_CCharacter (50)

Numeric

This field is required if Is LR? column contains False or is empty. The valid values for this field are Character or Numeric. The ML Type of the Measurement Location must match the ML Type of the template specified by the Template field, if applicable.
LR TypeMI_MEAS_LOC_MEAS_LOC_TYPE_CCharacter (50)This field is required if Is LR? column contains True. The valid values for this field are Checkoff, Changeout and Tracking. The LR Type of the Lubrication Requirement must match the LR Type of the template specified by the Template ID field, if applicable.
Is LR?ROUNDS_CHECK_PT_IS_LRLogicalThe default value of this field is False. Enter True to specify that a Lubrication Requirement is being loaded.

Description

MI_MEAS_LOC_DESC_C

Character (255)

Please provide a brief description.

Bluetooth Measurement TypeMI_MEAS_LOC_BT_MEAS_TYPE_CCharacter (255)None

Checkpoint Locked

MI_CHECK_PT_LOCKED_L

Logical

The default value of this field is False.

Requires Equipment ShutdownMI_CP_TMPLT_REQU_EQUI_SHUT_FLGLogicalThe default value for this field is False.

Unit of Measure

MI_MEAS_LOC_UOM_C

Character (50)

Must be a valid value in the global Unit of Measure list. This field is disabled if the ML Type field is Character.

Template

MI_MEAS_LOC_TEMPL_C

Character (50)

This field is required and must be unique. Must match an existing ML Template ID. The ML Type of the template specified by the ML Template ID must match the ML Type of Measurement Location, if applicable.

Related Asset KeyMI_CHECK_PT_REL_ASSET_KEY_NNumericIf provided, must be the entity key of an existing Equipment or Functional Location record. The Checkpoint will be linked to this asset.

Scan ID

MI_CHECK_PT_BARCD_ID_C

Character (50)

None

Related Asset Id

MI_MEAS_LOC_RELAT_ASSET_ID_C

Character (50)

If this value matches an existing Equipment ID (for Equipment) or Functional Location (for Functional Locations) the Checkpoint will be linked to this asset.

Asset Description

MI_MEAS_LOC_ASSET_DESCR_C

Character (50)

None

Status

MI_MEAS_LOC_STAT_C

Character (50)

The valid values for this field are Active or Inactive. The default value for this field is Active.

Sequence

MI_MEAS_LOC_SEQ_N

Numeric

This field is not required but if specified, it must be unique on the Route.

Category

MI_MEAS_LOC_CATEG_C

Character (50)

Must match the Category field on an existing Allowable Value record, where the Type field matches the ML Type value specified.

Allowable Values

MI_MEAS_LOC_ALLOW_VAL_C

Multi-value, max 10 values, Character (255)

All specified Values must match the Value field in pre-existing Allowable Value records where the Category and Type match the Category and ML Type defined for this ML. The | (pipe) character is used to separate each allowable value.

Lower Level 1 Action

MI_MEAS_LOC_LO_LVL1_ACT_C

Character (50)

None

Lower Level 1 Character Value

MI_MEAS_LOC_LO_LVL1_ALRT_C

Character (50)

Must use one of the Allowable Values specified for the ML. This field is disabled if the ML Type field is Numeric.

Lower Level 1 Message

MI_MEAS_LOC_LO_LVL1_MSG_C

Character (50)

None

Lower Level 2 Action

MI_MEAS_LOC_LO_LVL2_ACT_C

Character (50)

None

Lower Level 2 Character Value

MI_MEAS_LOC_LO_LVL2_ALRT_C

Character (50)

Must use one of the Allowable Values specified for the ML. This field is disabled if the ML Type field is Numeric.

Lower Level 2 Message

MI_MEAS_LOC_LO_LVL2_MSG_C

Character (50)

None

Upper Level 3 Numeric Value*

MI_MEAS_LOC_UP_LVL3_ALRT_N

Numeric

None. This field is disabled if ML type field is Character.

Upper Level 2 Numeric Value*

MI_MEAS_LOC_UP_LVL2_ALRT_N

Numeric

None. This field is disabled if ML type field is Character.

Upper Level 1 Numeric Value*

MI_MEAS_LOC_UP_LVL1_ALRT_N

Numeric

None. This field is disabled if ML type field is Character.

Lower Level 1 Numeric Value*

MI_MEAS_LOC_LO_LVL1_ALRT_N

Numeric

None. This field is disabled if ML type field is Character.

Lower Level 2 Numeric Value*

MI_MEAS_LOC_LO_LVL2_ALRT_N

Numeric

None. This field is disabled if ML type field is Character.

Lower Level 3 Numeric Value

MI_MEAS_LOC_LO_LVL3_ALRT_N

Numeric

None. This field is disabled if ML type field is Character.

Lower Level 3 Action

MI_MEAS_LOC_LO_LVL3_ACT_C

Character (50)

None

Lower Level 3 Character Value

MI_MEAS_LOC_LO_LVL3_ALRT_C

Character (50)

Must use one of the Allowable Values specified for the ML. This field is disabled if the ML Type field is Numeric.

Lower Level 3 Message

MI_MEAS_LOC_LO_LVL3_MSG_C

Character (50)

None

Upper Level 1 Action

MI_MEAS_LOC_UP_LVL1_ACT_C

Character (50)

None

Upper Level 1 Character Value

MI_MEAS_LOC_UP_LVL1_ALRT_C

Character (50)

Must use one of the Allowable Values specified for the ML. This field is disabled if the ML Type field is Numeric.

Upper Level 1 Message

MI_MEAS_LOC_UP_LVL1_MSG_C

Character (50)

None

Upper Level 2 Action

MI_MEAS_LOC_UP_LVL2_ACT_C

Character (50)

None

Upper Level 2 Character Value

MI_MEAS_LOC_UP_LVL2_ALRT_C

Character (50)

Must use one of the Allowable Values specified for the ML. This field is disabled if the ML Type field is Numeric.

Upper Level 2 Message

MI_MEAS_LOC_UP_LVL2_MSG_C

Character (50)

None

Upper Level 3 Action

MI_MEAS_LOC_UP_LVL3_ACT_C

Character (50)

None

Upper Level 3 Character Value

MI_MEAS_LOC_UP_LVL3_ALRT_C

Character (50)

Must use one of the Allowable Values specified for the ML. This field is disabled if the ML Type field is Numeric.

Upper Level 3 Message

MI_MEAS_LOC_UP_LVL3_MSG_C

Character (50)

None

Product

MI_MEAS_LOC_PRODUCT_C

Character (50)

None

Maximum Target Value

MI_MEAS_LOC_MAX_TRGVAL_N

Numeric

None. This field is disabled if ML type field is Character.

Minimum Valid Value

MI_MEAS_LOC_MIN_VLDVAL_N

Numeric

None. This field is disabled if ML type field is Character.

Minimum Target Value

MI_MEAS_LOC_MIN_TRGVAL_N

Numeric

None. This field is disabled if ML type field is Character.

Maximum Valid Value

MI_MEAS_LOC_MAX_VLDVAL_N

Numeric

None. This field is disabled if ML type field is Character.

More Information

MI_MEAS_LOC_MORE_INFO_C

Character (255)

None

Download Stored Document

MI_MEAS_LOC_DWLD_STRD_DOC_L

Logical

The default value for this field is False.

Action ID

MI_MEAS_ACTION_ID_EXT

Character (50)

This field matches the Action ID (MI_ACTION_ID_C field) of an Action record that is linked to the Strategy identified by the value in the MI_MEAS_STRATEGY_EXT column. If no matching Strategy / Action combination is found, the Measurement Location is not linked to an Action.

Strategy ID

MI_MEAS_STRATEGY_EXT

Character (255)

This field matches the Strategy ID (MI_STRATEGY_ID_C field) of the Strategy (MI_STRATEGY family) containing the Action to which the Measurement Location will be linked.

LubricantMI_LUBR_REQ_LUBR_CCharacter (50)This field must be a pre-existing Lubricant value in the Lubricant family where the Method and Manufacturer are as specified for this LR.
Number of PointsMI_LUBR_REQ_NO_OF_POINTS_NNumericNone
CapacityMI_LUBR_REQ_CAP_NNumericNone
QuantityMI_LUBR_REQ_QTY_NNumericNone
MethodMI_LUBR_REQ_METHOD_CCharacter (50)This field must be a pre-existing Method defined in a Lubricant record.
Skip ReasonMI_LUBR_REQ_SKIP_REAS_CCharacter (50)None
Change Out Triggers Update?MI_LUBR_REQ_CH_OUT_TRIG_UPD_LLogicalThe default value of this field is False.
ComponentMI_LUBR_REQ_COMP_CCharacter (50)None
Lubricant ManufacturerMI_LUBR_REQ_LUBR_MFR_CCharacter (50)This field must be a pre-existing value in a Lubricant record where the Method field is as specified for this LR.
PriorityMI_LUBR_REQ_PRIOR_CCharacter (50)None
Capacity Unit of MeasureMI_LUBR_REQ_CAPTY_UOM_CCharacter (50)None

Checkpoint Task Worksheet (MI_CP_TASK0)

Field CaptionField IDData Type (Length)Comments
Route Batch IDROUNDS_ROUTE_IDCharacter (50)This field is required for identification during the data load process. It should match the ID of the Route to which the Measurement Location record will be linked. Use <Dummy ID> if you are importing standalone Measurement Location records. The value in this field is not imported to GE Digital APM.
ML IdentifierROUNDS_ML_IDCharacter (50)This field is required for identification during the data load process and must be unique. The value in this field is not imported to GE Digital APM.
Next DateMI_TASK_NEXT_DATE_DTDateUTC time formatted as yyyy-mm-dd hh:mm:ss.
ScheduleMI_TASK_SCHEDULE_CCharacter (255)If provided, must be valid JSON Schedule definition.
Note: To enable users to copy the JSON schedule text, an alternative Checkpoint Task with Schedule datasheet is provided showing the Schedule Text (copy/paste enabled) field.
Non-compliance DateMI_CP_TASK0_NON_COMP_DDateUTC time formatted as yyyy-mm-dd hh:mm:ss.
Non Compliance Date IntervalMI_CP_TASK0_NONCMP_DT_INTR_NBRNumericIf provided, must be a positive integer.
Non Compliance Next Check DateMI_CP_TASK0_NON_CMP_NXT_CHK_DDateUTC time formatted as yyyy-mm-dd hh:mm:ss.

Checkpoint Condition Worksheet (MI_CHKPCOND)

Field CaptionField IDData Type (Length)Comments
Route Batch IDROUNDS_ROUTE_IDCharacter (50)This field is required for identification during the data load process. It should match the ID of the Route to which the Measurement Location record will be linked. Use <Dummy ID> if you are importing standalone Measurement Location records.

The value in this field is not imported to GE Digital APM.

Condition Batch IDMI_CHKPCOND_BATCH_IDCharacter (50)

This field specifies the batch ID for the Checkpoint Condition. This field is required for identification during the data load process and must be unique.

The value in this field is not imported to GE Digital APM.

Condition IdentifierMI_CHKPCOND_ID_CCharacter (50)This field is required for identification during the data load process and must be unique.

The value in this field is not imported to GE Digital APM.

Parent ML Batch IDPARENT_ROUNDS_ML_IDCharacter (50)This field is required for identification during the data load process and must match the ML Identifier of the predecessor Checkpoint as defined in the Measurement Location worksheet.

The value in this field is not imported to GE Digital APM.

Parent ML IDMI_CHECK_PT_PR_CHEC_ID_CCharacter (50)This field is required for identification during the data load process and must match the Checkpoint ID for the predecessor Checkpoint as defined in the Measurement Location worksheet.

The value in this field is not imported to GE Digital APM.

Field NameMI_CHKPCOND_FLD_NAM_CCharacter (50)This field behaves differently depending on whether the Predecessor CTS ID refers to a Measurement Location or a Lubrication Requirement:
  • If the Predecessor CTS ID refers to a Measurement Location, this field specifies the category for the Measurement Location.
  • If the Predecessor CTS ID refers to a Lubrication Requirement, this field specifies the lubricant type for the Lubrication Requirement.
Field Value for Character TypeMI_CHKPCOND_FLD_VAL_CHAR_CCharacter (250)This field specifies the reading value that, for a predecessor Measurement Location with an ML Type of Character, determines whether the condition has been met to display successor Checkpoints.
Field Value for Numeric TypeMI_CHKPCOND_FLD_VAL_NUM_NNumericThis field specifies the reading value that, for a predecessor Measurement Location with an ML Type of Numeric, determines whether the condition has been met to display successor Checkpoints.
Possible ConditionMI_CHKPCOND_POSS_COND_CCharacter (200)

This field specifies the relationship between the predecessor Checkpoint value and the value in the Checkpoint Condition Field Value field that determines whether to display successor Checkpoints in Rounds Data Collection.

If the predecessor Checkpoint has a Type value of Numeric, enter one of the following values:

  • <
  • <=
  • =
  • >=
  • >

If the predecessor Checkpoint has a Type value of Character, enter the following value in this field: is.

TypeMI_CHKPCOND_TYPECCharacter (50)This field is required. The valid values for this field are:
  • Character
  • Numeric
Sequence NumberMI_CHKPCOND_SEQ_NUM_NNumericThis field defines the sequence for sibling Checkpoint Conditions (that is, Checkpoint Conditions with the same Predecessor CTS ID). If you are adding a Checkpoint Condition for the first time:
  • If no value is specified in this field, a value will be automatically assigned to the Checkpoint Condition during the data load process.
  • If you specify a value in this field, the sequence that you specify will be used to determine the order of sibling Checkpoint Conditions.

If you are updating an existing Checkpoint Condition:

  • If no value is specified in this field, the existing sequence will remain intact.
  • If you specify a value in this field, the sequence that you specify will be used to determine the order of sibling Checkpoint Conditions.

Rounds Readings Data Loader Workbook

When importing data using the Rounds Readings Data Loader, the data loader will create one Reading record for each row of the import worksheet. The data loader will attempt to link each reading to a Checkpoint record (that is, Measurement Location record or Lubrication Requirement record) based on the related Measurement Location and Lubrication Requirement records specified in the import worksheet. To properly identify the Checkpoint to which Readings are linked, the import must specify either the Entity Key or the Checkpoint ID. If no matching Checkpoint is found, the reading is not imported. The Asset ID and Unit of Measure (if applicable) will be populated on the Reading based on the related Checkpoint, and the fields on the related Checkpoint Task will be updated according to the applicable schedule.

Each Reading record will take the same Site Reference Name that is designated to the Measurement Location or Lubrication Requirement to which it is assigned.

On the worksheet, you will specify the Readings that you want to link to Checkpoints (that is, Measurement Locations or Lubrication Requirements).

Note: If you are importing Readings directly after importing the related Checkpoints, you will need to use the Checkpoint ID.

When Readings are imported, the Status of the Reading is set, and the Checkpoint Task related to the Measurement Location or Lubrication Requirement is updated automatically. In order for the status of each Reading to be set as expected, Readings should be ordered earliest first on the worksheet.

Field Caption

Field ID

Data Type (Length)

Comments

Reading Batch ID

ROUNDS_READING_ID

Character (50)

This field is required.

Related ML Entity Key

MI_READING0_RELAT_ML_ENTIT_KEY_N

Numeric

This field must match the Entity Key of an existing Measurement Location or Lubrication Requirement. Either this field or Checkpoint ID is required.

Checkpoint ID

MI_CHECK_PT_CHEC_ID_C

Character (50)

This field must match the Checkpoint ID of an existing Measurement Location or Lubrication Requirement. Either this field or Related ML Entity Key is required.

Comment

MI_READING0_COMME_C

Character (255)

None

Action Taken

MI_READING0_ACTIO_TAKEN_C

Character (50)

Must use one of the Action Taken values specified for the related Measurement Location.

Reading Value Character

MI_READING0_RDG_VAL_CHAR_C

Character (50)

For Measurement Locations, must use one of the Allowable Values in the Category specified for the related Measurement Location. For Lubrication Requirements, must use a code in the system code table LR_CHAR_POSS_VALS (Possible values for Character type LRs).

This field is disabled if the ML Type of the related Measurement Location is Numeric. It is always enabled for Lubrication Requirements.

Reading Value Numeric

MI_READING0_RDG_VAL_NUM_N

Numeric

For Measurement Locations, if a Category is specified for the related Measurement Location, must use one of the Allowable Values.

This field is disabled if the ML Type of the related Measurement Location is Character or if the LR Type of the related Lubrication Requirement is Check Off.

Taken by

MI_READING0_RDG_TAKEN_BY_C

Character (50)

Must match an existing GE Digital APM User ID.

Reading Taken Date

MI_READING0_RDG_TAKEN_DT_D

Date

UTC time formatted as yyyy-mm-dd hh:mm:ss. Readings for the same Measurement Location or Lubrication Requirement should be ordered earliest first.

Example Rounds Templates Data Loader Workbook with Checkpoint Conditions

This section provides samples of the worksheets in the Rounds Templates Data Loader workbook to illustrate the process of creating a Template Group containing Checkpoint Conditions using the Rounds Templates Data Loader.

Overview

When imported into GE Digital APM, this example workbook creates a Template Group with six Checkpoints and two Checkpoint Conditions, as shown in the following image:



This section assumes that you are familiar with the basic process of creating Templates in a data loader and you are familiar with the fields used in these worksheets. For more information on the fields displayed in the following examples, see the Rounds Templates Data Loader Workbook section for Rounds Data Loaders.

Sample Template Group Worksheet

The Template Group worksheet defines the values for the Template Group Batch ID, the Template Group ID, the Template Group Description, and the Site Reference Name.



The value specified in the ID field determines the name of the Template Group as it will appear in Rounds Designer after the data load process is complete. For example, note that the ID specified in the ID field above appears as the title in the image of the Template Group in Rounds Designer above.

Sample Measurement Location Template Worksheet

The Measurement Location Template worksheet defines values for each Measurement Location in the Template Group.



The values in the Template ID and Description fields appear as the names and descriptions, respectively, of the Checkpoint in the Template Group in Rounds Designer. For example, note that the values in the Template ID and Description fields in the worksheet appear in the image of the Template Group at the beginning of this section as the names and descriptions of the Checkpoints.

In addition to the fields displayed in this image, the Checkpoints with an ML Type value of Character in this example also have the following values defined in the Allowable Values field: Yes and No.

Sample Checkpoint Template Sequence Worksheet

The Checkpoint Template Sequence worksheet specifies the sequence for the Checkpoints in the Template Group. This sequence is determined by the value entered in the Group ID/Predecessor CPC ID field, as shown in the following image:



In the Group ID/Predecessor CPC ID field, you can specify whether the Checkpoint is a successor of a condition:

  • If you do not enter a value, or if you enter the Group ID field value specified in the Template Group worksheet, the Checkpoint sequence is determined by the location of each Checkpoint entry in the worksheet. For example, in the image of the Template Group at the beginning of this section, note that a 1 appears next to Checkpoint-1 and a 2 appears next to Checkpoint-3. Neither of these has a Checkpoint Condition specified in the Group ID/Predecessor CPC ID field in the Checkpoint Template Sequence worksheet.
  • If you enter a CPC ID value in the Group ID/Predecessor CPC ID field, the Checkpoint is a successor of a Checkpoint Condition. For example, in the image of the Template Group at the beginning of this section, note that a value of 1.1.1 appears next to Checkpoint-2. This indicates that Checkpoint-2 is a successor of a Checkpoint Condition that is a successor of Checkpoint-1. Note also that, in the Checkpoint Template Sequence worksheet, Checkpoint-2 has a value of CPC-1 in the Group ID/Predecessor CPC ID field. This value specifies a Checkpoint Condition ID (CPC ID) that is defined in the following worksheet.

Sample Checkpoint Condition Worksheet

The Checkpoint Condition worksheet defines the sequence for Checkpoint Conditions as well as the conditions under which the successor Checkpoints of the Checkpoint Condition are displayed in Rounds Data Collection.



The value in the CPC ID field is used in the Checkpoint Template Sequence worksheet in the Group ID/Predecessor CPC ID field to specify a predecessor Checkpoint Condition for a Checkpoint. As mentioned in the previous section, notice that Checkpoint-2 and Checkpoint-4 in the Checkpoint Template Sequence worksheet both have CPC ID values in their Group ID/Predecessor CPC ID fields.

The value in the Predecessor CTS ID field determines which Checkpoint is the predecessor of the Checkpoint Condition. For example, notice that CPC-1 has a value of CTS-1 in the Predecessor CTS ID field, which references the CTS ID defined for Checkpoint-1 in the Checkpoint Template Sequence worksheet.

No value is required in the Sequence Number field. However, if you enter a value in this field for Checkpoint Conditions with the same predecessor Checkpoint (that is, sibling Checkpoint Conditions), the value you enter in this field will determine the sequence of the sibling Checkpoint Conditions.

The values you enter in the Possible Condition and Field Value for Character/Numeric Type fields determine the conditions under which the successor Checkpoints will appear in Rounds Data Collection. In this example, the successor Checkpoint of CPC-1 (that is, Checkpoint-2 as defined in the Checkpoint Template Sequence worksheet) will only appear when the reading value for the predecessor Checkpoint (Checkpoint-1) is Yes.

Note: When a predecessor Checkpoint has a Type value of Character, the only valid value to enter in the Possible Condition field is is.

Example Rounds Routes Data Loader Workbook with Checkpoint Conditions

This section provides samples of the worksheets in the Rounds Routes Data Loader workbook to illustrate the process of creating a Route containing Checkpoint Conditions using the Rounds Routes Data Loader.

Overview

When imported into GE Digital APM, this example workbook creates a Route with six Checkpoints and two Checkpoint Conditions, as shown in the following image:



This section assumes that you are familiar with the basic process of creating Routes in a data loader and you are familiar with the fields used in these worksheets. For more information on the fields displayed in the following examples, and for more information on the worksheets contained in the Rounds Routes workbook, see the Rounds Routes Data Loader Workbook section for Rounds Data Loaders. This section also does not contain information on the Security User worksheet or the Checkpoint Task worksheet.

Sample Route Worksheet

The Route worksheet specifies IDs used during the data load process as well as Route records used in GE Digital APM.



The value that you specify in the Route ID field determines the name of the Route as it appears in GE Digital APM. For example, note that the ID in this sample worksheet matches the name of the Route in the image at the beginning of this section.

Sample Measurement Location Worksheet

The Measurement Location worksheet defines values for each Measurement Location on the Route.



For Routes with Checkpoint Conditions, to ensure that the Route sequence is loaded as expected, the values for the following fields in the Measurement Location worksheet and the Checkpoint Condition worksheet must match one another:

Measurement location Worksheet FieldsCheckpoint Condition Worksheet Fields
ML Identifier (ROUNDS_ML_ID)Parent ML Batch ID (PARENT_ROUNDS_ML_ID)
Checkpoint ID (MI_CHECK_PT_CHEC_ID_C)Parent ML ID (MI_CHECK_PT_PR_CHEC_ID_C)
Parent Condition Batch ID (MI_CHKPCOND_BATCH_ID)Condition Batch ID (MI_CHKPCOND_BATCH_ID_C)
Parent Condition Identifier (MI_CHKPCOND_ID_C)Condition Identifier (MI_CHKPCOND_ID_C)

For example, note that the value in the ML Identifier and Checkpoint ID fields in the sample Measurement Location worksheet image above match the values in the Parent ML Batch ID and Parent ML ID fields, respectively, in the sample Checkpoint Condition worksheet image below.

Sample Checkpoint Condition Worksheet

The Checkpoint Condition worksheet defines the conditions under which the successor Checkpoints for Checkpoint Conditions are displayed in Rounds Data Collection. This worksheet also works together with the Measurement Location worksheet to determine the Route sequence for Routes with Checkpoint Conditions.



As mentioned above, the values defined in the Condition Batch ID and the Condition Identifier are used in the Measurement Location worksheet to specify successor Checkpoints for Checkpoint Conditions. Also, the values specified in the Parent ML Batch ID and the Parent ML ID fields must match the values defined in the ML Identifier and Checkpoint ID fields, respectively, for the predecessor Checkpoint of a Checkpoint Condition.

No value is required in the Sequence field. However, if a value is entered in this field for Checkpoint Conditions with the same predecessor Checkpoint (that is, sibling Checkpoint Conditions), the value you enter in this field determines the sequence of the sibling Checkpoint Conditions.

The values you enter in the Possible Condition and Field Value for Character/Numeric Type fields determine the conditions under which the successor Checkpoints will appear in Rounds Data Collection. In this sample worksheet, the successor Checkpoint of Condition-2 (that is, Checkpoint-14 as defined in the Measurement Location worksheet) will only appear when the reading value for the predecessor Checkpoint (Checkpoint-13) is less than 32.

Note: When a predecessor Checkpoint has a Type value of Character, the only valid value to enter in the Possible Condition field is is.

About the Rounds Data Loaders Load Verification

Before You Begin

After each worksheet is loaded:
  1. Review the data loader log to identify any errors or warnings.
  2. Update the data loader workbook to correct any errors, and then re-import.
  3. Repeat until the import of each record is error free.

About This Task

Note: It is recommended that a query is executed in GE Digital APM on the relevant family to ensure that records have been created and populated as expected. Imported records should also be spot checked in Record Manager or Rounds Designer to verify that the expected relationships have been created and site references have been set.

Procedure

  1. Log in to GE Digital APM as a Rounds Administrator user.
  2. On the left navigation menu, select Health, and then select Rounds Designer.
    The RD Overview page appears.
  3. Select the Allowable Values tab.
    The Allowable Values section appears, displaying a list of Allowable Values categories. The Allowable Values categories are groups of Allowable Values records that have the same value in the Category field.
  4. Select an Allowable Value category.
  5. Verify that the data appears as expected, and that the values can be edited or new values added to the Category.
  6. Verify that you can create new character (and numeric, if applicable) ML Templates and MLs, using Categories from the imported Allowable Values data.
  7. Verify that the Allowable Values appear as expected.
  8. Select the Templates tab.
  9. Verify that the loaded ML Templates appear as expected.
  10. Select an ML Template to open in Record Manager.
  11. Verify that the record contains the expected values and can be edited.
  12. Select an ML Template row.
  13. Select the Update Existing Checkpoints button.
  14. Verify that the Update Existing Checkpoints for <template name> Template page contains the expected related Checkpoints.
  15. Select the ML Template Groups tab.
  16. Verify that the loaded Template Groups appear as expected.
  17. Select an ML Template group.
  18. Verify that Templates and Conditions can be added, and that the drag-and-drop items to reorder works as expected.
  19. Select the Routes tab.
  20. Verify that the loaded Routes appear as expected.
  21. If the Users are assigned to the Routes via the data loader, select the Routes tab, select a Route, and verify that it has been assigned to a User.
  22. Select a Route to open in Route Management and:
    1. Verify the new and existing MLs, the MLs from Templates, and if Conditions can be added.
    2. Verify that the Routes can be re-ordered.
    3. Verify that the MLs are linked to Assets.
    4. Verify that the asset information is populated.
    5. Verify that the schedules have been populated.
    6. Verify that the readings have been linked to MLs.
  23. Select the Routes tab, select a Route, and verify that it can be assigned to a User.
  24. Ensure that the Route and/or MLs it contains are due.
  25. Log out of GE Digital APM.
  26. Log in to GE Digital APM as Rounds Administrator user.
  27. On the left navigation menu, select Health, and then select Rounds Data Collection.
    The RDC Overview page appears.
    Note: For complete test coverage, this should be done on an applicable mobile device.
  28. Verify that the assigned Route appears on the RDC Overview page.
  29. Verify that the Route can be set for offline use.
  30. Select the Route from the Due or Overdue list and perform an inspection.
    1. Enter readings for some of the Checkpoint, verifying that the Reading box contains the expected Allowable Values, if applicable.
    2. Verify that the alerts are triggered, that alert messages are displayed, and that the actions can be selected as expected.
    3. Add a Recommendation for an ML.
    4. Close the tab.
    5. Mark the Route done.
  31. Log out of GE Digital APM.
  32. Log in to GE Digital APM as Rounds Administrator user.
  33. On the left navigation menu, select Health, and then select Rounds Designer.
    The RD Overview page appears.
  34. Select the Routes tab.
  35. Select the Route for which the inspection was just completed.
  36. Verify that the Route History appears correctly. Check that the correct number of readings are reported.
  37. Verify that the readings that were taken appear against the relevant MLs.
  38. Verify that the recommendation that was created appears against the relevant ML.

If you set up the Asset Health Indicator service to run during the data load, you should also verify that the health indicators have been created as expected:

  1. Access a Measurement Location that was imported in Record Manager, and verify that a Health Indicator record is linked to the Measurement Location.
  2. Alternatively, access the asset related to the Measurement Location in Asset Health Manager to view the health indicators that exist for the asset.
    1. On the left navigation menu, select Admin, and the select Application Settings.
      The Application Settings page appears.
    2. Select AHM.
    3. In the left pane, select the Health Indicator Source Management tab, and then use the filter and search options to find the Measurement Locations to which you want to add health indicators.
    4. Verify that a green check mark is displayed for the Measurement Locations for which related Health Indicator records do not exist.
    5. To create Health Indicator records for Measurement Locations beside which the green check mark appears, but for which there are no records:
      1. Select the check boxes next to the affected Measurement Locations, and then select Exclude.

        A red X appears.

      2. Select Include.

        Health Indicators will now be created.

  3. If health indicators have not been created as expected, you can manually create health indicators by performing the following steps:
    1. On the left navigation menu, select Admin, and then select Application Settings.
      The Application Settings page appears.
    2. Select AHM.
    3. In the left pane, select the Health Indicator Source Management tab, and then use the filter and search options to find the Measurement Locations to which you want to add health indicators.
    4. Verify that a green check mark is displayed against the Measurement Locations for which related Health Indicator records do not exist.
    5. To create health indicator records for Measurement Locations beside which the green check mark appears but there is no record:
      1. Select the check boxes next to the affected Measurement Locations, and then select Exclude.

        A red X appears.

      2. Select Include.

        Health Indicators will now be created.