MOC Administration

Management of Change: MoC Administration

This workflow describes the process for creating Exceptions, Answer Options, Questions, and Checklists that can be used in a Change Project.

In the following workflow diagram, the blue text in a shape indicates that the corresponding description has been provided in the sections that follow the diagram. For more information, refer to the Interpreting the Workflow Diagrams topic in the APM Product Workflows documentation.
Note: For information on the personas associated with a GE Digital APM module, refer to the APM Product Workflows documentation.
Create ExceptionsCreate Answer OptionsCreate QuestionsCreate ChecklistsChange Project

Create Exceptions

Persona: Solution Administrator

Create the Exceptions that represent the action items that will be created automatically when you select Answer Options in a Checklist in a Change Project.

Create Answer Options

Persona: Solution Administrator

Create additional Answer Options that you want to use when you create Questions.

Create Questions

Persona: Solution Administrator

Create the Questions that you can want to associate with Checklists. You must associate each Question with a minimum of two Answer Options. As needed, you can associate an Answer Option with an Exception.

Create Checklists

Persona: Solution Administrator

Create Checklists by adding Questions as Checklist Items to each Checklist.