Inspection Configuration
Access the Inspection Configuration Workspace
Procedure
About Checklist Configuration Templates
Checklist Configuration Templates allow you to define a collection of checklist categories and the items that they contain to create Checklist Templates. Users can create Inspection Events using the Checklist Templates, and the Checklist Finding records are generated based on the selected template.
Using Checklist Configuration Templates
Checklist Configuration Templates should contain checklist categories and items that will result in detailed Checklist Templates that can be used to create Inspection Events. In the Checklist Configuration Templates section, you can create Checklist Configuration Templates that contain multiple checklist categories and items that are defined based on system code tables. You can modify the available checklist categories and items using the MI CHECKLIST CATEGORIES system code table. When you add a category to a Checklist Configuration Template, you can choose which items appear in the checklist. You can continue adding checklist categories and items to your Checklist Configuration Template until you have created a Checklist Template that will be useful for the intended asset. Creating a Checklist Configuration Template with checklist categories and items that correspond closely to existing assets streamlines inspections by including relevant Checklist Finding items in a user-created Inspection Event.
Checklist Configuration Templates and Taxonomy Configuration
The Checklist Configuration Templates that you create can be linked to a Taxonomy Configuration. When a Checklist Configuration Template has been linked to a Taxonomy Configuration, the Checklist Template appears as an option when users create Inspection Events for an asset whose equipment taxonomy matches the Taxonomy Configuration. The Checklist Configuration Template will also appear by default if the equipment taxonomy of the asset does not match an existing Taxonomy Configuration.
Checklist Configuration Templates and Asset Mapping
Asset Mapping allows the Checklist Template categories to be associated with the existing Assets. When creating or editing a Checklist Configuration Template, the Enable Asset Mapping option is available in the Template Name window. If you select this option when creating an Inspection Event using the Checklist Configuration Template, an Asset Mapping section appears, allowing you to map the Assets to the checklist categories.
Example: Fire Tube Boiler
A Checklist Configuration Template named Fire Tube Boilers Inspection Checklist contains the Tubes Waterside checklist category. The Tubes Waterside checklist category contains two items: Borescope Inspection and Corrosion.
When a user creates an Inspection Event, a Checklist Template named Fire Tube Boilers Inspection Checklist appears in the Inspection Event list. If the user creates an Inspection Event using the Fire Tube Boilers Inspection Checklist Checklist Template, the Checklist Finding record displays the Tubes Waterside checklist category with Borescope Inspection and Corrosion listed as Checklist Finding items.
Example: Fire Tube Boiler linked to a Taxonomy Configuration
The Fire Tube Boilers Inspection Checklist is linked to the following Taxonomy Configuration:
- Taxonomy Category: Fixed
- Taxonomy Class: Boiler
- Taxonomy Type: Misc Boiler
When a user creates an Inspection Event for an asset that shares that Taxonomy Configuration, Fire Tube Boilers Inspection Checklist appears in the list of available Checklist Templates for that asset.
About Application Configuration
This topic has been intentionally excluded from the GE Digital APM product documentation website. Contact GE Digital Support to get access to this topic.
Configure Recommendation Status to State Mapping
About This Task
For example, the following Inspection Recommendation records use the Status field.
Recommendation ID | Asset ID | Functional Location ID | Recommendation Headline | Status |
---|---|---|---|---|
REC-21 | HE-1608 CRUDE-HVY. ATMOS. GAS OIL | 016-E-E3104A CRUDE-HVY. ATMOS. GAS OIL | Shell Corrosion | Created |
Rec-2005 | HE-1608 CRUDE-HVY. ATMOS. GAS OIL | C-488 LUBE/SEAL OIL COOLER ~ HXST 105 | General Corrosion | Pending Review |
Rec-244 | HE-1608 CRUDE-HVY. ATMOS. GAS OIL | C-488 LUBE/SEAL OIL COOLER ~ HXST 105 | General Distortion | Pending Review |
Source Family | Status | State |
---|---|---|
Inspection Recommendation | Created | Proposed |
Inspection Recommendation | Pending Review | Pending Approval |
Recommendation ID | Asset ID | Functional Location ID | Recommendation Headline | State |
---|---|---|---|---|
REC-21 | HE-1608 CRUDE-HVY. ATMOS. GAS OIL | 016-E-E3104A CRUDE-HVY. ATMOS. GAS OIL | Shell Corrosion | Proposed |
Rec-2005 | HE-1608 CRUDE-HVY. ATMOS. GAS OIL | C-488 LUBE/SEAL OIL COOLER ~ HXST 105 | General Corrosion | Pending Approval |
Rec-244 | HE-1608 CRUDE-HVY. ATMOS. GAS OIL | C-488 LUBE/SEAL OIL COOLER ~ HXST 105 | General Distortion | Pending Approval |
Currently, GE Digital APM only allows mapping of Status to States. After you update the Inspection Recommendation records using this feature, you can switch back to Status by clearing the Use State Management for Inspection Recommendation check box. However, the existing Inspection Recommendation records cannot be reverted to Status. To align Inspection Recommendations with other performance recommendations, we recommend using State Management to manage Inspection Recommendations.
Before You Begin
- Make sure that the State Functionality is enabled in the State Configuration section of the Inspection Recommendation Family Management.
- Make sure that the Inspection Admin role or the Super User role is assigned to you.
Procedure
Configure Inspection Status to State Mapping
About This Task
For example, the following Inspection records use the Status field.
Inspection Reference | Asset ID | Functional Location ID | Inspection Headline | Status |
---|---|---|---|---|
INSP-24 | HE-1608 CRUDE-HVY. ATMOS. GAS OIL | 016-E-E3104A CRUDE-HVY. ATMOS. GAS OIL | Shell Corrosion | Draft |
INSP-25 | HE-1608 CRUDE-HVY. ATMOS. GAS OIL | C-488 LUBE/SEAL OIL COOLER ~ HXST 105 | General Corrosion | Pending Approval |
INSP-26 | HE-1608 CRUDE-HVY. ATMOS. GAS OIL | C-488 LUBE/SEAL OIL COOLER ~ HXST 105 | General Distortion | Pending Approval |
Source Family | Status | State |
---|---|---|
Inspection | Draft | Draft |
Inspection | Pending Approval | Pending Approval |
Inspection Reference | Asset ID | Functional Location ID | Inspection Headline | State |
---|---|---|---|---|
INSP-24 | HE-1608 CRUDE-HVY. ATMOS. GAS OIL | 016-E-E3104A CRUDE-HVY. ATMOS. GAS OIL | Shell Corrosion | Draft |
INSP-25 | HE-1608 CRUDE-HVY. ATMOS. GAS OIL | C-488 LUBE/SEAL OIL COOLER ~ HXST 105 | General Corrosion | Pending Approval |
INSP-26 | HE-1608 CRUDE-HVY. ATMOS. GAS OIL | C-488 LUBE/SEAL OIL COOLER ~ HXST 105 | General Distortion | Pending Approval |
Before You Begin
- Make sure that the State Functionality is enabled in the State Configuration section of the Inspection family and Custom states are added, which will be mapped to the custom statuses.
- Make sure that the Inspection Admin role or the Super User role is assigned to you.
Procedure
About Event Configurations
By default, each of the baseline Inspection families has its own Event Configuration. The Event Configuration determines:
- The General Finding record that will be created automatically for each subcomponent of the piece of equipment that you inspected. The subcomponents are determined by the value that you specify in the Item Category field in the linked Inspection Profile records.
- The datasheet that the inspection reviewer will see.
- The Inspection Family Configuration that will be used to display the Inspection record and all records to which it is linked.
If you create new Inspection families, you must create an Event Configuration for those families.
In the baseline database, an Event Configuration is defined for each baseline Inspection family. The following columns are displayed in the Event Configurations grid:
- Family: Displays the family caption.
- Auto Generate: Automatically generates General Findings records based on the Inspection Scope of the task being addressed.
- Reviewer's Datasheet: Displays the datasheet caption that was specified when the Event Configuration was defined for the family.
- Related Families: Displays any related families associated with the family caption. Based on your security privileges, you can adjust the available preferences for each family.
Modify the Asset Query Path and the Alerts Query Path
About This Task
Procedure
Modify Profile Configuration
Procedure
- Modify the Taxonomy Profile Configuration
- Modify the Profile System Code Configuration
- Modify the Profile Query Configuration
- Modify the Profile Query Configuration
Results
Delete a Taxonomy Profile Configuration
Procedure
Modify Method Configuration
Procedure
- Modify the Method System Code Configuration
- Modify the Method Query Configuration
Add or Modify Event Configuration
Procedure
- Add an Event Configuration
- Steps: Modify an Event Configuration
Modify or Delete Family Preferences
Procedure
- Modify Related Family Preferences
- Delete a Related Family
- Steps: Delete a Related Family
- Delete a Related Family
- Delete a Related Family
Delete an Event Configuration
Procedure
Access a Checklist Configuration Template
About This Task
Procedure
Create a Checklist Configuration Template
Procedure
Delete a Checklist Configuration Template
Procedure
Add Categories and Items to a Checklist Configuration Template
About This Task
After creating a Checklist Configuration Template, you can select a checklist category from which you want to add items to the template. The selected checklist category is used to sort your selected items in the template. You can add multiple checklist categories that each contain one or more items to your Checklist Configuration Template.