Hazards Analysis Upgrade
Upgrade or Update Hazards Analysis to V5.1.0.0.0
The following table provides you the reference to procedures to upgrade from an earlier GE Digital APM version to the latest version.
Upgrade from | Upgrade to | Procedure |
---|---|---|
V5.0.x | V5.1.0.0.0 | |
V4.6.2 or a later V4.6.x release | V5.1.0.0.0 | |
V4.6.1.x or earlier | V5.1.0.0.0 |
Note: For more information on upgrading to GE Digital APM V4.6.2.0.0 or a later V4.6.x release, refer to the Upgrade documentation for the corresponding version.
|
Upgrade from any version V5.0.1.0.0 through V5.0.2.0.0
This module will be upgraded to V5.1.0.0.0 automatically when you upgrade the components in the basic GE Digital APM system architecture. No additional steps are required.
Upgrade from any version V4.6.2.0.0 through V4.6.6.0.0
The following tables outline the steps that you must complete to upgrade this module to V5.1.0.0.0. These instructions assume that you have completed the steps for upgrading the basic GE Digital APM system architecture.
These tasks may be completed by multiple people in your organization. We recommend, however, that the tasks be completed in the order in which they are listed.
Step | Task | Notes |
---|---|---|
1 | Update entity key parameters from :n to :k for the following catalog queries:
| This step is required only if you have previously modified the queries. This step will be completed automatically when you upgrade the components in the basic GE Digital APM system architecture. |
2 | Update Asset Hierarchy parameter from -1 to #ahhome for the following catalog queries: For example, (? :ah :id=entity_key) = '-1' must be updated to (? :ah :id=entity_key) = (#:ahhome)
| This step is required only if you have previously modified the queries. This step will be completed automatically when you upgrade the components in the basic GE Digital APM system architecture. |
3 | Following queries have been modified to improve the performance. Revert these queries to Baseline to see the improved performance.
| This step is required only if you have previously modified the queries. |
Update the Query Parameter Type
About This Task
After the database for GE Digital APM is upgraded, if the entity key fields are of the type string, you must modify the catalog query parameters to use the correct type by performing the following steps:
Procedure
Revert the Hazard Analysis Queries to Baseline
This action is required only if you have modified the Hazard Analysis queries.