Compliance Management Deployment

Deploy Compliance Management

The checklists in this section of the documentation contain all the steps necessary for deploying and configuring this module whether you are deploying the module for the first time or upgrading from a previous version.
Important: You must have an active license in Compliance Management, Inspection Management, and Policy Designer to use this module.

Deploy Compliance Management for the First Time

The following table outlines the steps that you must complete to deploy and configure this module for the first time. These instructions assume that you have completed the steps for deploying the basic system architecture.

These tasks may be completed by multiple people in your organization. GE Digital recommends, however, that the tasks be completed in the order in which they are listed.

StepTaskNotes
1Review the Compliance Management data model to determine which relationship definitions you will need to modify to include your custom equipment and location families. Via Configuration Manager, modify the relationship definitions as needed. This step is required only if you store equipment and location information in families other than the baseline Equipment and Functional Location families.
2Assign users to the MI Inspection Security Group to provide privileges to the Compliance Management families.This step is required.
3

Assign Security Users to one or more of the Security Roles used in Compliance Management.

This step is required.

Security Users will need permissions to the Compliance Management families before they can use the Compliance Management features.

4Create Inspection Strategy records using Record Manager. This step is required. You should create Compliance Strategy records that adhere to the compliance standards of a regulatory body that requires inspections.
5Design a policy to use for a Compliance Strategy Template.This step is required. You can create this policy using the Policy Designer.
6Create a query that will return the assets that you want to link to the Compliance Strategy Template.This step is optional. You can also add assets to the Compliance Strategy Template by individual asset.
7Create a Compliance Strategy Template using the administrative features of Compliance Management. This step is required.
8Link assets to the Compliance Strategy Template.This step is required.
9Map the Policy to the Compliance Strategy Template that you created.This step is required.
10Configure Inspection Management ActiveMQ settings for MIExecution Service.This step is optional. You can perform this step if you want to modify the default retries or concurrency settings.
11Ensure that the Meridium MIExecution Service is installed and running.If the basic GE Digital APM system architecture is already installed, the Meridium MIExecution Service is automatically installed, and the service runs automatically.

Compliance Management Security Groups and Roles

The following table lists the baseline Security Groups available for users within this module, as well as the baseline Roles to which those Security Groups are assigned.

Important: Assigning a Security User to a Role grants that user the privileges associated with all of the Security Groups that are assigned to that Role. To avoid granting a Security User unintended privileges, before assigning a Security User to a Role, be sure to review all of the privileges associated with the Security Groups assigned to that Role. Also, be aware that additional Roles, as well as Security Groups assigned to existing Roles, can be added via Security Manager.

Security Groups

The following families adhere to the security groups listed in the table below:
  • Asset Has Compliance Template
  • Asset Has Inspection Plan
  • Compliance Recommendation
  • Recommendation Revision
  • Compliance Policy Mapping
  • Compliance Strategy
  • Compliance Strategy Template
  • Compliance Template Has Mapping
  • Inspection Plan Has Recommendations
  • Has Inspection Plan Revision
  • Implements Compliance Recommendation
  • Inspection Plan
  • Inspection Plan Revision
  • Suggested Compliance Templates
Security GroupPermissions
MI Inspection
  • View
  • Insert
  • Update
  • Delete
MI Inspection ViewerView
MI RBI AdministratorView
MI RBI AnalystView
MI RBI ViewerView
MI Thickness Monitoring AdministratorView
MI Thickness Monitoring InspectorView
MI Thickness Monitoring UserView
MI Thickness Monitoring ViewerView

Security Roles

Compliance Management security roles can perform the following tasks:
TaskDescription
ApproveChange the state of an Inspection Plan to Approved.
Apply TemplatesApply suggested Compliance Strategy Templates to assets in the Assets without Templates section of the Compliance Management Overview page.
CreateCreate an Inspection Plan or Compliance Strategy Template.
ModifyModify Inspection Plans and Compliance Recommendations by changing States, deleting Compliance Recommendations, and implementing Compliance Recommendations as Inspection Tasks.
Suggest TemplatesSuggest Compliance Strategy Templates to be linked to assets in the Assets without Templates section of the Compliance Management Overview page.
ViewAccess a Compliance Recommendation, Inspection Plan, or Compliance Strategy Template.
The following security roles are available in Compliance Management:
Security RoleInspection Plan PrivilegesCompliance Strategy Template PrivilegesAssigned Security Group
MI Compliance AdministratorView
  • Apply Templates
  • Create
  • Modify
  • Suggest Templates
MI Compliance Analyst
  • Create
  • Modify
  • Apply Templates
  • Suggest Templates
  • View
MI Inspection Plan Approver
  • Create
  • Modify
  • Approve
  • Apply Templates
  • Suggest Templates
  • View
  • MI ASM Analyst

Configure Inspection Management ActiveMQ settings for MIExecution Service

The MIExecution Service, on each GE Digital APM Server serves RBI, Inspection and Thickness Monitoring module queues. This service is configured to use a single shared ActiveMQ queue service across APM. Available queue configuration options include retries and concurrency limit.

Procedure

  1. On the GE Digital APM Server, access the folder that contains the MIExecution Service files.
    Note: If you have installed GE Digital APM in the default location, you can locate the folder in C:\Program Files\Meridium\ApplicationServer\mi-execution
  2. Access the appsettings.json file in an application that can be used to modify JSON files (for example, Notepad++).
  3. In the file, locate the following text:
    "Queue_Config": {
    	    "Queues": [
    	      {
    	        "Name": "MI_IM_Queue", 
    	        "ConcurrencyLimit": 8,
    	        "Retries": 5
    	      }
    	    ]
              }
    Note: ConcurrencyLimit indicates the maximum number of messages that will be consumed concurrently. Retries indicates the number of times it retries to send the messages to ActiveMQ if it fails.
  4. Update the key values as desired.
  5. Save and close the file.
    The updated settings will be applied when the MIExecution Service is stopped and restarted.