Thickness Monitoring Upgrade
Upgrade or Update Thickness Monitoring to V5.0.7.0.0
Upgrading or updating to the V5.0.7.0.0 is a two-step process. You need to first upgrade to APM V4.6.2.0.0 or later and then follow the steps to upgrade or update to V5.0.7.0.0.
The following table provides you the reference to procedures to upgrade from an earlier APM version to the latest version.
Upgrade from | Upgrade to | Procedure |
---|---|---|
V5.0.0.0.0 through V5.0.6.0.0 | V5.0.7.0.0 | Upgrade from any version V5.0.0.0.0 through V5.0.6.0.0 |
V4.6.2.0.0 through V4.6.11.0.0 | V5.0.7.0.0 | Upgrade from any version V4.6.2.0.0 through V4.6.11.0.0 |
Upgrade from any version V5.0.0.0.0 through V5.0.6.0.0
This module will be upgraded to V5.0.7.0.0 automatically when you upgrade the components in the basic APM system architecture. No additional steps are required.
Upgrade from any version V4.6.2.0.0 through V4.6.11.0.0
The following tables outline the steps that you must complete to upgrade this module to V5.0.7.0.0. These instructions assume that you have completed the steps for upgrading the basic APM system architecture.
These tasks may be completed by multiple people in your organization. We recommend, however, that the tasks be completed in the order in which they are listed.
Step | Task | Notes | ||||||||||||||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
1 | Uninstall the previous version of the Meridium Device Service on all of the machines that will connect to devices that will be used with Thickness Monitoring. | This step is required only if you will use any device to collect data that you transfer to Thickness Monitoring. | ||||||||||||||||||||||||
2 | Install the Meridium Device Service on all of the machines that will connect to devices that will be used with Thickness Monitoring. | This step is required only if you will use any device to collect data that you transfer to Thickness Monitoring. If you are using HTTPS to connect to APM, follow the instructions in HOW TO: V4 Thickness Monitoring - Devices - Dataloggers and Secure HTTPS Browsers on Windows Machines. | ||||||||||||||||||||||||
3 | If you have previously modified the following Pipe Properties records, follow the steps mentioned in KBA 000035691 to get the updated values for the records.
| This step is optional. | ||||||||||||||||||||||||
4 | Update entity key parameters from :n to :k for the following catalog queries:
|
This step is required only if you have previously modified the queries. This step will be completed automatically when you upgrade the components in the basic APM system architecture. | ||||||||||||||||||||||||
5 | Revert the following queries to baseline to remove the references to the MI_ENTITIES family that has been deprecated:
|
This step is required only if you have previously modified the queries. This step will be completed automatically when you upgrade the components in the basic APM system architecture. | ||||||||||||||||||||||||
6 | Family keys stored in the TM Family Preferences are upgraded to store Family IDs. | This step will be completed automatically when you upgrade the components in the basic APM system architecture. | ||||||||||||||||||||||||
7 | Configure Thickness Monitoring ActiveMQ Settings for MIExecution Service. | This step is optional. You can perform this step if you want to modify the default retries or concurrency settings. | ||||||||||||||||||||||||
8 | Ensure that the Meridium MIExecution Service is installed and running. | If the basic APM system architecture is already installed, the Meridium MIExecution Service is automatically installed, and the service runs automatically. | ||||||||||||||||||||||||
9 | Update the following query to add the system field mentioned. Public/Meridium/Modules/Thickness Monitoring/Piping Rotation/Queries/Rotation History for Component Column Name: CRT_DT (CRT_DT) | Refer to KBA 000068267 for more details. | ||||||||||||||||||||||||
10 | If you use the following query and want to use it in APM
V5.0.7.0.0, you must export the query and import it into APM
V5.0.7.0.0. Public/Meridium/Modules/Thickness Monitoring/Queries/Measurements Near or Less than T-Min Note: The query is no longer used in APM and has been removed.
| This step is optional. | ||||||||||||||||||||||||
11 | Revert the following queries to baseline to fix the query compilation error:
| This step is required only if you have previously modified the queries. |
Install the Meridium Device Service
About This Task
Procedure
Update the Query Parameter Type
After the database upgrade for APM, if the entity key fields are of the type string, you must modify the catalog query parameters to use the correct type by performing the following steps.
Procedure
Revert the Thickness Monitoring Queries to Baseline
This action is required only if you have modified the Thickness Monitoring queries.
About This Task
- Assets Near or Past Retirement
- Assets with TM Tasks
- Corrosion Distribution
- Excessive Corrosion
- Remaining Life Less than 180 Months
- Thickness Inspections
- TM Assets
- TM Assets Requiring a Calculation
Procedure
Configure Thickness Monitoring ActiveMQ Settings for MIExecution Service
The MIExecution Service,on each APM Server serves RBI, Inspection and Thickness Monitoring module queues. This service is configured to use a single shared ActiveMQ queue service across APM. Available queue configuration options include retries and concurrency limit.