Supported Software and Devices
All APM Components
Supported Third Party Components | APM V5.0.7.0.0 |
---|---|
.NET Framework 4.7.2 and .NET Core 6.0 | ![]() |
ASI for SAP
Supported Third Party Components | APM V5.0.7.0.0 |
---|---|
SAP ECC 6.0 (Enhancement Packs [EhP] 1 through 8) The following SAP system versions are required to update items in SAP with changes made in ASI:
|
![]() |
SAP S/4 HANA on-premises (1509, 1610, 1709, 1809, 1909, 2020, 2021, 2022, 2023) | ![]() |
Calibration Management
Supported Third Party Components | APM V5.0.7.0.0 |
---|---|
CMX Calibration Management Software Version 2 (2.10.114.0) |
![]() |
GE Device Driver 1.6.0.0 |
![]() |
APM Client Web Browser
Supported Third Party Components | APM V5.0.7.0.0 |
---|---|
Google Chrome New versions of Google Chrome are released every 4 weeks. Each version includes security updates, new features, and possible breaking changes. To ensure compatibility, GE Vernova recommends that you use the latest Google Chrome version available. |
![]() |
Microsoft Edge New versions of Microsoft Edge are released every 4 weeks. Each version includes security updates, new features, and possible breaking changes. To ensure compatibility, GE Vernova recommends that you use the latest Microsoft Edge version available. |
![]() |
Metrics and Scorecards
Supported Third Party Components | APM V5.0.7.0.0 |
---|---|
Microsoft SQL Server Analysis Services 2014 | ![]() |
OT Connect
Supported Third Party Components | Notes | APM V5.0.7.0.0 |
---|---|---|
OT Connect OPC HDA Protocol Adapter | Tested internally with:
|
![]() |
OT Connect OPC DA Protocol Adapter Note: The OPC DA Protocol Adapter is available with APM V4.4.0.0.2. | Tested internally with:
|
![]() |
OT Connect OSI PI Protocol Adapter Requires Pi AF Client 2018 SP3 Patch 2.
Note: The OSI PI AF available with APMV4.4.0.0.2. | Tested internally with:
|
![]() |
OT Connect GE Historian Protocol Adapter Requires Historian 7.2+ Client Access Assembly, targeting supported historian servers 4.0 and above.
Note: The GE Historian Protocol Adapter is available with APMV4.4.0.0.2. | Tested internally with:
|
![]() |
- OPC Foundation Historical Data Access (OPC-HDA) specification version 1.20, (AKA 1.2). The OPC HDA server offers the following capabilities:
- LastReading
- StartToEndReadings
- SubscribeReadings
- OPC DA Protocol Adapter that can connect to OPC Classic DA 3.0 servers. The OPC DA server offers the following capabilities:
- LastReading
- SubscribeReadings
- OSI PI Protocol Adapter that can connect to PI Server 2010 and later through the Asset Framework (AF) Protocol. The OSI PI Protocol Adapter offers the following:
- LastReading
- SubscribeReading
- GetStartEndReadings
- GetBeforeEndReadings
- GE Historian Protocol Adapter that can connect to Proficy Historian 4.0 and later through the Client Access API. The GE Historian Protocol Adapter offers the following Capabilities:
- LastReading
- SubscribeReading
- GetStartEndReadings
- GetBeforeEndReadings
- OT Connect does not support OPC PI Server Collectives.
- To support direct consumption of Readings into Asset Health Indicators (AHIs) and triggered Policies, the server does need to implement the End aggregate.
Report Designer
Supported Third Party Components | Notes | APM V5.0.7.0.0 |
---|---|---|
Microsoft Visual Studio 2017 Professional | None | ![]() |
Microsoft Visual Studio 2019 Professional | None | ![]() |
Microsoft SQL Server Data Tools - Business Intelligence for Visual Studio 2017 (15.8.0) |
| ![]() |
Microsoft SQL Server Data Tools - Business Intelligence for Visual Studio 2019 | ![]() |
Rounds
APM Components | Supported Third Party Components | APM V5.0.7.0.0 |
---|---|---|
Rounds (iOS, Android and Windows tablet devices) | Any operating system that meets the APM Client operating system requirements | ![]() |
Rounds Pro Mobile App
APM Components | Supported Third Party Components | APM V5.0.7.0.0 |
---|---|---|
Rounds Pro Mobile App (iOS, Android and Windows tablet devices) | Any operating system that meets the APM Client operating system requirements | ![]() |
R Scripts
Supported Third Party Components | APM V5.0.7.0.0 |
---|---|
DeployR Open 8.0.0 Note: The APM testing environment uses DeployR Open 8.0.0. | ![]() |
DeployR Enterprise 8.0.0 Note: The APM testing environment uses DeployR Enterprise 8.0.0. | ![]() |
Machine Learning Server 9.2.1 or 9.3.0 Note: The APM testing environment uses Machine Learning Server 9.3.0. | ![]() |
Rules
Supported Third Party Components | APM V5.0.7.0.0 |
---|---|
Microsoft Visual Studio 2017 or 2019 Professional | ![]() |
MSXML | ![]() |
SAP Interfaces
Supported Third Party Components | Notes | APM V5.0.7.0.0 |
---|---|---|
SAP ECC 6.0 (Enhancement Packs [EhP] 1 through 8) | None | ![]() |
SAP S/4 HANA on-premises 1509, 1610, 1709, 1809, 1909, 2020, 2021, 2022, 2023 |
| ![]() |
SQL Server Report Server
Supported Third Party Components | Notes | APM V5.0.7.0.0 |
---|---|---|
Microsoft SQL Server Reporting Services 2014 | You can view a report designed using a lower version of Microsoft SQL Server Data Tools (SSDT) in a higher version of SQL Server Report Server (SSRS). However, you cannot view a report designed using a higher version of SSDT in a lower version of SSRS. | ![]() |
Microsoft SQL Server Reporting Services 2016 | ![]() | |
Microsoft SQL Server Reporting Services 2017 | ![]() | |
Microsoft SQL Server Reporting Services 2019 | ![]() |
Supported Devices
Any management policy applied to mobile devices must be set up to allow the required permissions for the APM mobile application. If restrictions are placed on iOS, Android, or Windows devices by a global policy or mobile device management system, then device storage, scanning, photography, location services, and other functionality may be disabled.
If you are using a Windows device, ensure that Windows App Store access is enabled.
Calibration Management Devices
Device | V5.0.7.0.0 |
---|---|
Fluke 74x Documenting Process Calibrator | ![]() |
Fluke 75x Documenting Process Calibrator | ![]() |
Fluke 729 Automatic Pressure Calibrator | ![]() |
GE Druck Calibrators:
| ![]() |
*Calibration Management use the Devices Interface, which is a UI that is configured to support the transfer of data between APM and devices that APM supports.
Rounds Devices
Device | Notes | V5.0.7.0.0 |
---|---|---|
Android, iOS, or Windows tablets that meets the APM Client requirements. | None | ![]() |
Barcode Functionality | ||
Device cameras for Android, iOS, and Windows tablets |
This feature is available only when using the APM mobile application. | ![]() |
Zebra TC-75X Touch Computer Integrated Barcode Scanner |
Devices used in the APM testing environment:
| ![]() |
RFID Functionality | ||
Zebra TC-75X Touch Computer NFC RFID reader |
Device used in the APM testing environment:
| ![]() |
Thickness Monitoring Supported Devices
Device | APM V5.0.7.0.0 |
---|---|
GE DMS Go | ![]() |
GE DMS Go+ | ![]() |
GE DMS2 | ![]() |
Olympus (Panametrics) 37DL Plus Ultrasonic Thickness Gage | ![]() |
Olympus (Panametrics) 38DL Plus Ultrasonic Thickness Gage | ![]() |
* Thickness Monitoring use the Devices Interface, which is a UI that is configured to support the transfer of data between APM and devices that APM supports.