Instrumentation System Planning Workflow
Calibration Management: Instrumentation System Planning Workflow

Define Instrumentation Systems
Persona: Analyst
Create an Instrumentation Systems record.
This record is used to describe the Instrumentation System and to manage the calibrations and calibration schedules for the entire system. This record is site filtered.
Select Asset
Persona: Analyst
This asset represents the parent-level asset against which a Calibration Task will be defined and scheduled to calibrate the system.
Define Calibration Task
Persona: Analyst
Select Instrumentation System and create a Calibration Task record. This is to specify the schedule for performing the calibration for the entire system and assign the task to the user. This Calibration Task is linked to the parent asset of the Instrumentation System that is defined in Select Asset. When the calibration record is approved and closed, this Calibration Task is recycled to its next due date based on the defined interval.
Link Assets
Persona: Analyst
After creating an Instrumentation System record, link one or more child assets that need to be calibrated as part of the system. These child assets can be Functional Locations and/or Equipment. The child assets may be from the same Functional Location that is linked to the Instrumentation System or from a different Functional Location.
The selected child assets should already be a part of the Calibration Profile and have Applied Templates.
Define Calibration Task Scope
Persona: Analyst
In the Instrumentation System, you can group and organize asset-level calibration applied templates and review summary results. The Task Scoping process allows you to select all or a subset of calibration strategies (applied templates) that need to be collectively managed for the assets in the Instrumentation System. Typically, the strategies and schedule for all sub-assets within the Instrumentation System are similar, based on the criticality of the system/loop. It is possible that within the same Instrumentation System, calibration strategies may differ from one asset to another even though the schedule of the system/loop is the same. To facilitate this, you can scope the task at the Instrumentation System level by selecting the calibration strategies (applied templates) of the related sub-assets. Task scope can be modified to add or remove assets later.
One Instrumentation System can have one or more Calibration Tasks and each Calibration Task can have its task scope defined.
After defining the task scope, the child assets with their applied templates against the Calibration Task appear under Calibration Queue in the Calibration Management Overview page.
Calibration Assessment
Persona: Analyst / Calibration Technician
Go to the Calibration Assessment Workflow.
Perform either a manual calibration or an automated calibration for the child assets of the Instrumentation System. When the calibration event is created for any child asset, the summary event is automatically created. The PASS/FAIL results of the child event is automatically rolled up and marks the summary event as PASS or FAIL.
After the calibrations are completed and approved for all the child assets defined in the current task scope, the summary event can be approved. This recycles the Calibration Task associated with the Instrumentation System.