SQL Server Analysis Services

Hardware Requirements

The following hardware components are the basic hardware that are required for supporting SQL Server Analysis Services in APM Metrics and Scorecards module. These requirements are specified only for the APM software. Additional hardware may be required on a SQL Server Analysis Services machine where other components are installed. These requirements may not be sufficient and may change depending upon how your system is configured.

ComponentRequirement
CoreTwo Processor Cores, 2+ GHz
RAM8 GB RAM
Hard Drive25 GB of available hard drive space

Software Requirements

One of the following software is required on any machine that will serve as the SQL Server Analysis Services server.

Software Name and VersionWhere You Can Obtain It
SQL Server Analysis Services 2014 (Multi-Dimensional mode only)Microsoft
SQL Server Analysis Services 2016 (Multi-Dimensional mode only)