Query Timeouts

About Query Timeouts

Using Query Timeouts, you can specify the query time-out limit. The query time-out limit is the amount of time in seconds that the APM system will allow a new or modified query to attempt to return results before timing out.

This setting allows you to control the performance of the queries in your system by enforcing a requirement that they meet a specific performance goal. This setting is used in the query design when a Security User whose query privilege setting is Restricted By Timeout Limit tries to save a new or modified query.

Before a Security User whose query privilege is Restricted By Timeout Limit can save a new or modified query, they will have to run the query so that the APM system can determine if it runs within the time-out limit. Otherwise, the save options will remain disabled. If a query time-out limit has been specified in that database, when the query runs, the APM system will allow the query to run until the specified query time-out limit has been met. After the time-out limit is reached:
  • If the query has not returned results, a message will appear, indicating that the query cannot be saved, and the save options will remain disabled.
  • If the query has returned results, the save options will be enabled, and the Security User can save the query.

Access the Query Timeout Limits Page

Procedure

In the Applications menu, navigate to ADMIN > Operations Manager > Query Timeouts.
The Query Timeout Limits page appears.

What To Do Next

Specify the Limit for Query Timeout

About This Task

The following instructions provide details on specifying the query time-out limit for Security Users who are restricted by query time-outs. These instructions do not provide a recommendation on choosing the time-out value itself. The value that you choose should match the amount of time that your organization has defined as a reasonable amount of time for a query to run before returning results. The value you enter must be a whole number (i.e., not a decimal value).

Procedure

  1. Access the Query Timeout Limits page.
  2. In the Query Timeout Limit (in minutes) for Restricted Users box, enter the number that represents amount of time to which you want to limit query runs.
  3. Select .
    A confirmation message appears, indicating that the query timeout is created.