Performance
GAA Performance Workflow
This workflow describes the process for creating and reviewing the Performance records for a GAA Unit.
In the following workflow diagram, the blue text in a shape indicates that the corresponding description has been provided in the sections that follow the diagram. For more information, refer to the Interpreting the Workflow Diagrams topic in the APM Product Workflows documentation.
Note: For information on the personas associated with a APM module, refer to the APM Product Workflows documentation.

GAA Administration
Persona: Solution Administrator
Define an event when operating status or capability of a GAA Unit changes.
Go to the GAA Administration workflow.
Unit
Persona: Solution Administrator
Defining GAA Unit provides GAA Unit record, Unit Capacity record, and GAA Report record.
Create Performance Record
Persona: Analyst
Create a Performance record for the selected GAA Unit.
Review or Approve Performance Record
Persona: Solution Administrator
Use state management to review or approve the Performance record for the selected GAA Unit.
GAA Reporting
Persona: Solution Administrator or Analyst
Generate Regulatory or Management reports based on events or performance.
Go to the GAA Reporting.