Capacity Event Types Affecting Performance Records
Capacity Event Types Affecting Performance Records
In Performance records, the following fields are populated using the sum of the values in the Event Duration field in Primary Event records that are linked to the Performance record:
- Planned and Ext Outage Hrs: Populated using the sum of the values in the Event Duration field in Primary Event records in which the value in the Capacity Event Type field is either PE or PO.
- Ext Sched Outages Hrs: Populated using the sum of the values in the Event Duration field in Primary Event records in which the value in the Capacity Event Type field is any of the following Capacity Event Types: ME, DM, PE, SE, DE, or DP.
-
Eqv Upl Frcd Derate Hrs RS (G) and Eqv Upl Frcd Derate Hrs RS (N): Populated with calculated values when the Primary Event records to which it is linked have a Capacity Event Type of D1, D2, D3, D4, PD, or RS with values entered for both the Gross Derate Amount and the Net Derate Amount in the following cases:
- If a Reserved Shutdown event occurred during a Derate event.
- If a Derate event occurred during a Reserved Shutdown event.
- A Derate event started and ended during a Reserved Shutdown event.
- A Derate event started during a Reserved Shutdown event but ended after the Event End date of the Reserved Shutdown.
- A Derate event and a Reserved Shutdown event had the same Event Start and Event End dates.
Note: If none of the following cases have occurred during the month for which the Performance record stores generation data, the Eqv Upl Frcd Derate Hrs RS (G) and Eqv Upl Frcd Derate Hrs RS (N) fields will be populated with the value 0 (zero).