Create a Relationship
POST
Creates a relationship.
Consumes
This API call consumes the application/json
media types via the Content-Type request header.
Request Syntax
POST/custdev/core/relationship
Request Body
body Meridium.Api.CustDev.Core.RelDevDTO(optional)
Request Body Example
{
"familyKey": "64251800815",
"predFamilyKey": "64251789393",
"predEntityKey": "64263626261",
"succFamilyKey": "64251784124",
"succEntityKey": "64263626258"
}
Return Type
array[Meridium.Api.CustDev.Core.
RelDevDTO
]
Produces
This API call produces the application/json
media type according to the Accept request header. The media type will be conveyed by the Content-Type
response header.
Success Response
200
Success