Studio

Configure the APM Connect Administration Center for the Studio

About This Task

Important: This step is required only if you have the APM Connect Studio license. If you are deploying APM Connect Base with a Basic or Plus License, skip this procedure.

Procedure

  1. Open a web browser.
    Tip: APM Connect is most compatible with Google Chrome or Mozilla Firefox web browsers. It is not recommend using Internet Explorer to access the APM Connect Administration Center.
  2. Enter the following URL into your web browser: http://localhost:8080/apmconnect/.
  3. If prompted, log in to the APM Connect Administration Center.
  4. In the Menu pane, in the Settings section, select the Configuration tab.

    The Configuration pane appears.

  5. Select the CommandLine/primary (5 Parameters) group to expand the workspace.
  6. According to recommendations in the information in the following table, enter the necessary parameters.
    ParameterDescriptionRecommend or Default Value
    Host The IP address of the CommandLine.localhost
    PortThe port number on which the CommandLine is queried.8002
    Job generation folderThe path to the folder where Jobs are generated. <root:>\APMConnect\Utilities\cmdline\generationCache
    User component pathThe path to the folder where user components are stored.<root:>\APMConnect\Utilities\cmdline\custom_components
    The default parameters are configured as shown in the following image.

Install the Studio

About This Task

Important: This step is required only if you have the APM Connect Studio license. If you are deploying APM Connect Base with a Basic or Plus License, skip this procedure and proceed to the next step in the APM Connect Base deployment workflow.

Procedure

  1. On the machine on which you installed APM Connect, access the Talend Studio installation package.
  2. Open the file TalendStudioInstall.exe.
  3. In the Setup-Talend Studio window, select Next.

    The License Agreement window appears.

  4. Read the entire license agreement, and then select one of the following options:
    • I accept the agreement: If you agree to the terms of the license agreement and want to continue. These instructions assume that you want to continue.
    • I do not accept the agreement: This option is selected by default. If you do not agree to the terms of the license agreement and do not want to continue, select Cancel to exit the installer.
    Next is enabled.
  5. Select Next.

    The Select Destination Location screen appears.

  6. Select Next.

    The Select Components screen appears.

  7. Select the Add Start Menu Entry box, then select the Add Desktop Icon box, and then select Next.
  8. Select Next.
  9. In the Select Start Menu Folder window, select Next.
  10. In the Ready to Install window, select Install.

    The Installing screen appears, displaying an installation progress bar.

  11. When the installation completes, in the Completing the Talend Studio Setup Wizard window, select Finish.

Results

The installation is complete, and Talend Studio desktop icon is available.