Asset Hierarchy Configuration
Asset Hierarchy Configuration
APM is built on the premise that, within your company, there are multiple records that can be organized into a hierarchy. This organization relies on the parent-child relationship between records to represent the fact some records can belong to other records.
The Hierarchy can be modified to reflect custom asset families. However, the baseline configuration relies on the Functional Location family and the fields in each Functional Location record to define which location each represents. Because there is only one Functional Location family, it is used to store data about all of your locations, where the values in each Functional Location record identify which type of location it is.
More Details: Baseline Configuration
In the baseline configuration, there are two levels reflected in the Asset Hierarchy: the Root and a secondary level. The primary level of the Hierarchy, the Root, reflects the Functional Location relationships. The second level of the hierarchy reflects Equipment related to Functional Locations. The hierarchy first displays the Root Functional Location, and drills down to child Functional Locations based on your selections. The hierarchy will continue to do so until there are no child relationships for the selected Functional Location. Then, using the criteria defined in the second level, the hierarchy will display Equipment records related to the selected Functional Location.
The baseline configuration is as follows:
-
Root: The primary level of the hierarchy.
- Parent Family: Functional Location
- Relationship: Functional Location Has Functional Location(s)
- Child Family: Functional Location
- Parent Priority: 0
- Display Field: ENTY_ID
- Taxonomy Category: Taxonomy Category
- Taxonomy Class: Taxonomy Class
- Taxonomy Type: Taxonomy Type
-
Secondary Level: The second level of the hierarchy.
- Parent Family: Functional Location
- Relationship: Functional Location Has Equipment
- Child Family: Equipment
- Parent Priority: 0
- Display Field: ENTY_ID
- Taxonomy Category: Taxonomy Category
- Taxonomy Class: Taxonomy Class
- Taxonomy Type: Taxonomy Type
- The link to each parent uses a different relationship family.
- A priority has been defined for each relationship family in the Asset Hierarchy configuration.
To find the duplicate keys, run the below query in GE Digital APM:
SELECT MV_AST_HRCY_DUP.parent_enty_key
, PAR_FMLY.FMLY_CAPTION_TX "PARENT_FMLY"
, MV_AST_HRCY_DUP.enty_key "CHILD_ENTY_KEY"
, CHILD_FMLY.FMLY_CAPTION_TX "CHILD_FMLY"
, MV_AST_HRCY_DUP.enty_id "CHILD_ENTY_ID"
, MV_AST_HRCY_DUP.the_level
, MV_AST_HRCY_DUP.path
FROM MIV_MI_AST_HRCY_MV_DUP MV_AST_HRCY_DUP
JOIN MI_FAMILIES PAR_FMLY ON PAR_FMLY.FMLY_KEY = MV_AST_HRCY_DUP.parent_fmly_key
JOIN MI_FAMILIES CHILD_FMLY ON CHILD_FMLY.FMLY_KEY = MV_AST_HRCY_DUP.fmly_key
ORDER BY MV_AST_HRCY_DUP.enty_key Asc
Access the Asset Hierarchy Configuration Page
Procedure
Modify the Asset Hierarchy Configuration
About This Task
Procedure
Schedule an Asset Hierarchy Rebuild
About This Task
For information on scheduling a job, refer to Schedule a Job.