Upcoming End of Life Features

Inspection Field Data Collection

As part of the continuous improvement process, the next generation Integrity Mobile application is released with the APM V5.0.0.0.0. The new application provides a convenient user interface and is supported across all major platforms. As part of this enhancement, the existing GE Digital APM Inspection Field Data Collection application feature will reach end of life and will be no longer available with the Q3 2024 release. We recommend all customers to migrate to the new Integrity Mobile application that provides similar functionalities in an intuitive way.