Limits

About a Limit

If you want to receive alerts on a device when you record reading values that meet certain criteria, you can define the criteria and the health indicators in the Limits section of the Step Details page. You can configure limits and health indicators for either numeric or Picklist reading types only. You cannot configure for character type readings.

For character reading type, a message appears indicating that limits are not available for character reading type.

For Picklist reading type, you can add Limits for the available Picklist values only.

A Limit defines:

  • The Limit values for the readings recorded for a Step.
  • Limit colors.
  • Health indicators to indicate the upper and lower threshold levels.
  • A message to be displayed in Rounds Pro mobile application when you enter the readings.
Note: A message can be a warning or an alert. For more details, refer to About Status Criteria for Numeric Health Indicators.
The limits, health indicators, and display messages for alerts or health indicators appear on the following pages:
  • Route Steps and the Step Details screens on Rounds Pro mobile application when the readings are entered for a Step.
  • The Route Instances Details pages accessed from the Open Instances and Instance History pages in the web application, which reflect the last reading collected and saved to the server using Rounds Pro mobile application.

Access a Health Indicator

Procedure

  1. Access the Rounds Designer page.
  2. Access a Step of a route instance, for which you want to access a Limit.
  3. In the Step Details page, expand the LIMITS section, and select the Generate Health Indicators button.

    The health indicators that are available appear in the list.

Create a Health Indicator

Procedure

  1. In the Rounds Designer page, Access a Step of a route instance, in which you want to create a health indicator.
  2. Select the Generate Health Indicators button.
    The upper and lower-level limit values and the fields to configure the health indicators appear in the section.

    For character reading type, no fields are displayed. A message appears indicating that readings will be tracked as a history only Health Indicator.

    Note:
    • You can select the Generate Health Indicators option in both the cases: Create New Step and Create Step from Template.
    • Health Indicator Name is same as that of Step Name and Health Indicator Description is same as that of Step Description. Hence, when you update the step, the health indicator details are also updated.
    • Health indicators are also generated based on the selected Picklist Type. If you select the Picklist Type as Numeric, a numeric health indicator is generated, and if you select the Picklist Type as Character, a character health indicator is generated.
    • When you delete a step that has the associated health indicator, the health indicator details also get deleted with the step details.
    • In the LIMITS section, when you change the option from Generate Health Indicators to None, the health indicators details get deleted.
  3. As needed, enter values in the available fields.
  4. Select .
    The health indicator is saved to the GE Digital APM database.

Delete a Health Indicator

Procedure

  1. Access the Rounds Designer page.
  2. Access a Step of a route instance, for which you want to access a Limit.
  3. In the Step Details page, expand the LIMITS section, and select None.
    Note: When health indicators exist, the Generate Health Indicators option is selected.
    The Dropping Limits Confirmation window appears, asking you to confirm if you want to delete the Limit values.
    Note: If the step is not assigned with any Limit values to generate Health Indicators, the confirmation window does not appear.
  4. Select Continue.

    The health indicators details are deleted.

Results

The health indicator details under the Limit section are deleted from the GE Digital APM database.