Rounds Pro Deployment
Deploy Rounds Pro for the First Time
The following table outlines the steps that you must complete to deploy and configure this module for the first time. These instructions assume that you have completed the steps for deploying the basic system architecture.
These tasks may be completed by multiple people in your organization. We recommend, however, that the tasks be completed in the order in which they are listed.
Step | Task | Notes |
---|---|---|
1 |
Review the data model to determine which relationship definitions you will need to modify to include your custom Equipment and Functional Location families. Modify any relationship definitions as needed via Configuration Manager. | This step is required only if you have asset data in families outside of the baseline Equipment and Functional Location families. |
2 |
Assign Security Users to the following Rounds Pro Security Groups:
| This step is required. |
3 | Install the Rounds Pro mobile application on the mobile device that you plan to use for data collection. | This step is required only if you will use a mobile device for data collection. For information on installation of Rounds Pro on mobile devices see the following sections: |
4 | Set the local time zone on the mobile device that you will use for data collection, typically the user time zone. | This step is required only if you will use a mobile device for data collection. |
6 | Configure ActiveMQ settings for Rounds Service | This step is required. |
Configure ActiveMQ settings for Rounds Service
The Rounds Service is responsible for syncing the data between GE Digital APM Server and the Rounds Pro app, it is also responsible to handle the changes on Steps and Step Templates and works with the core scheduling service. Rounds Service should be running on all GE Digital APM Application Servers. Ensure the Rounds Service is Running on all the APM Servers. This service is configured to use a single shared ActiveMQ queue service across APM. Available queue configuration options include retries and concurrency limit. Changes to the following settings are optional.