Event Management

GAA Event Management Workflow

This workflow describes the process for managing events that occur in a GAA Unit.

In the following workflow diagram, the blue text in a shape indicates that the corresponding description has been provided in the sections that follow the diagram. For more information, refer to the Interpreting the Workflow Diagrams topic in the APM Product Workflows documentation.
Note: For information on the personas associated with a GE Digital APM module, refer to the APM Product Workflows documentation.
GAA Administration WorkflowUnitCreate EventReview EventRoot Cause Analysis (RCA)GAA ReportingAsset Health Management ViewApprove EventeLog

eLog

Persona: Solution Administrator

Create or associate log entries to document events that occur during shifts for power generation.

Go to the eLog workflow.

GAA Administration

Persona: Solution Administrator

Define an event when operating status or capability of a GAA Unit changes.

Go to the GAA Administration workflow.

Unit

Persona: Solution Administrator

Defining GAA Unit provides GAA Unit record, Unit Capacity record, and GAA Report record.

Create Event

Persona: Operator or Supervisor

Define an event when operating status or capability of a GAA Unit changes.

Review Event

Persona: Analyst

Use state management to track the progress of an event and review the event for Unit Level approval.

Approve Event

Persona: Solution Administrator

Use state management to track the progress of an event and review the event for submittal to NERC.

Root Cause Analysis (RCA)

Persona: Analyst

Create an RCA for the selected event.

Go to the Root Cause Analysis.

GAA Reporting

Persona: Solution Administrator or Analyst

Generate Regulatory or Management reports based on events or performance.

Go to the GAA Reporting.

Asset Health Management View

Persona: Analyst

Navigate to the Asset Health Management View to see all the Health Indicators for the selected GAA Unit.

Go to the Manage Health Indicators Workflow.