Troubleshooting Scenarios

Loading data via the ASM template dataloader gives a warning

Description

After exporting the ASM template data from the template export option, then you attempt to modify the data and re-load it via the ASM template dataloader displays the following warning message:
A field with the ID 'MI_RISK_RISK_MATRI_C' was not found in the family 'Risk'. No data will be loaded for this column

in the dataloader log.

Cause

The exported spreadsheet has a column Risk Matrix Name (MI_RISK_RISK_MATRI_C), which has incorrect field ID. The correct field ID is MI_RISKASSE_RM_NAME_C.

Solution

Perform the following step:

You need to replace the field ID from MI_RISK_RISK_MATRI_C to MI_RISKASSE_RM_NAME_C in the Risk sheet of the dataloader template to resolve the issue.

Invalid Error Message when Creating a new Asset Strategy

Description

When you attempt to create a new Asset Strategy in GE Digital APM, an error is displayed as Invalid Number Specified.

Cause

When you select Create Strategy, this calls the asset hierarchy. Since the asset hierarchy was not loading or failing, it causes the Create Strategy workflow to fail.

Solution

Perform the following step:

Create the missing Asset hierarchy using the Unified Asset Ingestion Data loader and then create a new Asset strategy.