Upgrade Logs

Review Upgrade Logs for a Policy

About This Task

When the GE Digital APM database is upgraded to V5.0.0.0.0 or later from an earlier version, the logs that provide information, such as modifications to existing policy models, upgrade issues that were not addressed automatically, and the applicable APM version number, are saved to the policy records. You can review this information and identify changes that are required to ensure that the policy continues to function as expected after the upgrade.
Note: The Upgrade Logs tab is displayed only if the policy has a value in the Upgrade Log field. When you first execute or access the policy after your APM system is upgraded, the policy record may be upgraded, and the Upgrade Log field updated. However, if you use a query to view the value in this field, it may not reflect the final upgrade status.

Procedure

  1. Access the policy for which you want to review the logs.
  2. Select the Upgrade Logs tab.
    The Upgrade Logs workspace appears.
  3. Review the upgrade log information.

Results

The log includes information and warning messages. If there are any warning messages, you may need to modify the policy model for the policy to function as originally intended.

Delete Upgrade Logs for a Policy

Before You Begin

You must be a member of the MI Policy Designer security group to delete the upgrade log.

About This Task

You can delete the policy upgrade log information that is no longer needed.

Procedure

  1. Access the policy for which you want to delete the upgrade logs.
  2. Select the Upgrade Logs tab.
    The Upgrade Logs workspace appears.
  3. Select Delete Upgrade Logs.
    A window with a confirmation message appears.
  4. Select OK.

Results

The upgrade log information is deleted from the GE Digital APM database; it is replaced with the APM version number, user ID, and the timestamp indicating when the upgrade log was deleted.