Inventory Grouping Workflow

About Inventory Grouping Workflow

The Inventory Grouping feature allows you to group RBI Components that belong to a process unit. After you group the components, GE Digital APM calculates the value in the Inventory Group Mass field for the inventory group.

This workflow provides the basic, high-level steps for the Inventory Grouping feature. The steps and links in this workflow do not necessarily reference every possible procedure. For more details, follow the links in the below steps.

Follow the below steps to configure Inventory Group to calculate the Inventory Groups Mass:

  1. Access the Inventory Groups workspace.
  2. Create an Inventory Group Configuration record for the appropriate process unit. This record stores the details of the name and description of the group, and the process unit that is associated with the group.
  3. Link RBI Components to the inventory group.
  4. In RBI, access the components that belong to the inventory group.
  5. Create an RBI 581 Risk Analysis for each component linked to the inventory group.
  6. Access the RBI 581 Consequence Evaluation record associated with each analysis that you have created in the previous step, and then in the Common section of the datasheet, select the Use Calculated Inventory check box.

    The Inventory Group and Inventory Group Mass fields in the RBI 581 Consequence Evaluation are populated automatically.

    Tip: If the Use Calculated Inventory check box is already selected, clear the check box, and then select it. This will update the inventory group mass value.

Access the Inventory Groups Workspace

Before You Begin

  • You can access the Inventory Groups workspace only if the RBI 581 license is active.

Procedure

  1. Access the Risk Based Inspection Overview page.
  2. Select the Actions button.
  3. Select the Manage Inventory Groups option.
    The Inventory Groups workspace appears, displaying the following information:
    • The left pane: Provides a list of all the process units (i.e., Functional Location records in which the Is a Unit? check box is selected) in GE Digital APM. The icon next to a process unit indicates that the process unit contains an inventory group. If you select a process unit, a list of inventory groups in the process unit appears in the left pane.
    • The details section: Displays the following information based on what you select in the left pane:

      • If you select Process Units in the left pane, the details section displays the Process Units with Inventory Groups section, which displays the number of RBI Components linked to each Inventory Group of the Process Units. If you select a Process Unit in the list, the datasheet for the associated Functional Location appears. If you select an Inspection Group in the list, the datasheet for the associated Inventory Group appears.
        Tip: Select to access the Table Settings window, where you can set column preferences for the table.
      • If you select a process unit in the left pane, the details section displays the datasheet for the associated Functional Location.
      • If you select an inventory group in the left pane, then the details section displays the datasheet of the Inventory Group Configuration record. You can also access a list of components associated with the inventory group by selecting the Linked Components tab.

What To Do Next

Note:
  • When you are on the Risk Based Inspection Overview page of a Functional Location which is a Process Unit, selecting Manage Inventory Groups option will navigate to the associated Process Unit in the Inventory Groups workspace.
  • Inventory Grouping is not supported on assets which are not process units.

Create an Inventory Group Configuration Record

Before You Begin

  • You can create or modify an Inventory Group Configuration record only if you are a super user or a member of the MI RBI Administrator or MI RBI Analyst Security Groups.

Procedure

  1. Access the Inventory Groups workspace.
  2. In the list on the left pane of the workspace, select the process unit in which you want to create an Inventory Group Configuration record.
    The inventory groups in the process unit appear.
  3. In the list on the left pane of the workspace, select .
    A blank datasheet for the Inventory Group Configuration appears in the Details section.
  4. As needed, enter values in the available fields.
  5. In the upper-right corner of the datasheet, select .
    The Inventory Group Configuration record is created. The newly created group is listed on the left pane of the workspace.

Results

  • The Linked Components tab is enabled.

What To Do Next

Delete an Inventory Group Configuration Record

Before You Begin

  • You can delete an Inventory Group Configuration record only if you are a super user or a member of the MI RBI Administrator or MI RBI Analyst Security Groups.

Procedure

  1. Access the Inventory Groups workspace.
  2. In the list on the left pane of the workspace, select the process unit that is linked to the Inventory Group Configuration record that you want to delete.
    The inventory groups in the process unit appear.
  3. In the list on the left pane of the workspace, select the Inventory Group Configuration that you want to delete.
    The datasheet for the Inventory Group Configuration appears in the Details section.
  4. In the upper-right corner of the datasheet, select .
    The Confirm Delete dialog box appears, asking you to confirm that you want to delete the inventory group.
  5. Select Yes.
    The Inventory Group Configuration record is deleted.

Results

  • If you create an RBI 581 Risk Analysis for components that once belonged to the deleted inventory group, the value in the Inventory Group Mass field will no longer be populated automatically.

Access the Inventory Groups in a Process Unit

About This Task

You can also access the inventory group of a component.

Procedure

  1. Access the Unit Summary workspace for the process unit for which you want to access inventory groups.
  2. In the upper-right corner of the workspace, select , and then select Manage Inventory Groups.
    The Inventory Groups workspace appears on a new page, displaying a list of inventory groups in the process unit in the left pane and the datasheet for the corresponding Functional Location in the details section.
    Tip: If you are a member of the RBI Admin or RBI Analyst Security Groups, you can create an Inventory Group Configuration record in the Inventory Groups workspace.