Upgrade Logs

Review Upgrade Logs for a Family Policy

About This Task

When the GE Digital APM database is upgraded to V5.0.0.0.0 from an earlier version, the logs that provide information, such as modifications to existing policy models and upgrade issues that were not addressed automatically, are saved to the family policy records. You can review this information and identify changes that are required to ensure that the family policy continues to function as expected after the upgrade.
Note: The Upgrade Logs tab is displayed only if the family policy has a value in the Upgrade Log field.

Procedure

  1. Access the family policy for which you want to review the logs.
  2. Select the Upgrade Logs tab.
    The Upgrade Logs workspace appears.
  3. Review the upgrade log information.

Results

The log includes information, warning, and error messages. If there are any error messages, you have to modify the policy model, for the family policy to function as originally intended.

Delete Upgrade Logs for a Family Policy

About This Task

You can delete the family policy upgrade log information that is no longer needed.

Procedure

  1. Access the family policy for which you want to delete the upgrade logs.
  2. Select the Upgrade Logs tab.
    The Upgrade Logs workspace appears.
  3. Select Delete Upgrade Logs.
    A window with a confirmation message appears.
  4. Select OK.

Results

The upgrade log information is deleted from the GE Digital APM database; it is replaced with the user ID and the timestamp indicating when the upgrade log was deleted.