Search Configuration

Search Configuration

You can use the search configuration options to change the way that records are returned by the global search. For example, you can specify the information that is shown in search results or whether or not a certain family or field should be included in the search results at all.

Excluding Families from Search

When you exclude a family from search, records in that family are not returned by the global search tool. In addition, records in any excluded families will not be returned in any Search window used in GE Digital APM. Therefore, you will not be able to select the records in workflows that use the Search window to select records. For example, in Policy Designer, you could not assign one of these records to a policy instance.

By default, in the baseline GE Digital APM database, the familied listed in the KBA 000040087 are included in the search.

About The Search Index

The search index is used to return the results of the Global search in GE Digital APM. The search index is updated automatically, and, for performance reasons, is designed to update incrementally.

When only a few records are added to the database, those records appear in the Global search results almost immediately. However, when large data loads are performed or records updated in bulk (e.g., during an initial implementation), it takes a longer amount of time for the records to be indexed, and therefore for them to appear in the Global search results.

Important: You should not rebuild the search index solely because newly added records do not appear in the Global search results after completing a large data load or bulk record import.
Tip: If a large data load is performed for a specific family and the records are not indexed immediately, you can use the Reindex Family functionality to rebuild the index for that family.

The search index typically only needs be rebuilt manually after a database upgrade. However, in some cases the search index may become out of sync with the data in your database. For example, if you add records to the database directly rather than via Record Manager in the GE Digital APM application, the search index will not include those changes and you must rebuild the search index manually. If occurrences such as this happen regularly in your company’s implementation of GE Digital APM, you may want to schedule the search index to be built on a regular basis.

Access the Search Configuration Page

Procedure

  1. Access the Operations Manager page, and then select Search Configuration.

    The Search Configuration page appears.

  2. In the left pane, select the family for which you want to configure search results.

    The workspace for the selected family appears, displaying the family search settings.

Build the Search Index

Procedure

  1. Access the Search Configuration page.
  2. To build the search index, perform the following steps:
    1. Select Build Index.
      The Rebuild window appears.
    2. Select OK.
      The search index will be built, and all expected results will be included in the global search. To verify whether the operation has completed successfully, you can view the generated Meridium.Service.Search_<Date>.txt log file at <installdir>\ProgramData\Meridium\Logs\.
      Tip: To access the ProgramData folder, you must show the hidden folders on your system.
      Note: When the index is being built, the color of the Search icon changes.
  3. To rebuild the search index for a specific family:
    1. Select a family in the left pane.
    2. Select Reindex Family.
      The search index for the specific family is rebuilt. Now, you do not need to rebuild the entire index if there are any changes to the search configuration options or if a large data load is performed for a specific family.
      Note: This functionality is not available if a family is excluded from search.
  4. To schedule the search index to be built at a future time or on a recurring schedule, select Schedule.
    The Edit Schedule window appears. Enter the values in the required fields. For more information on creating a schedule, see Schedule a Job. The search index will be built according to the schedule, and the expected results will be included in the global search. You can view the status of the scheduled job by accessing ADMIN > Operations Manager > Job Monitoring Dashboard.