About This Task
When the GE Digital APM database is upgraded to V5.0.0.0.0 from an earlier version, the logs that provide information, such as modifications to existing policy models and upgrade issues that were not addressed automatically, are saved to the policy records. You can review this information and identify changes that are required to ensure that the policy continues to function as expected after the upgrade.Note: The Upgrade Logs tab is displayed only if the policy has a value in the Upgrade Log field.
Procedure
- Access the policy for which you want to review the logs.
- Select the Upgrade Logs tab.
The Upgrade Logs workspace appears.
- Review the upgrade log information.
Results
The log includes information, warning, and error messages. If there are any error messages, you have to modify the policy model, for the policy to function as originally intended.