Inventory Grouping Workflow
About Inventory Grouping Workflow
The Inventory Grouping feature allows you to group RBI Components that belong to a process unit. After you group the components, GE Digital APM calculates the value in the Inventory Group Mass field for the inventory group.
This workflow provides the basic, high-level steps for the Inventory Grouping feature. The steps and links in this workflow do not necessarily reference every possible procedure. For more details, follow the links in the below steps.
Follow the below steps to configure Inventory Group to calculate the Inventory Groups Mass:
- Access the Inventory Groups workspace.
- Create an Inventory Group Configuration record for the appropriate process unit. This record stores the details of the name and description of the group, and the process unit that is associated with the group.
- Link RBI Components to the inventory group.
- In RBI, access the components that belong to the inventory group.
- Create an RBI 581 Risk Analysis for each component linked to the inventory group.
-
Access the RBI 581 Consequence Evaluation record associated with each analysis that you have created in the previous step, and then in the Common section of the datasheet, select the Use Calculated Inventory check box.
The Inventory Group and Inventory Group Mass fields in the RBI 581 Consequence Evaluation are populated automatically.
Tip: If the Use Calculated Inventory check box is already selected, clear the check box, and then select it. This will update the inventory group mass value.
Access the Inventory Groups Workspace
Before You Begin
- You can access the Inventory Groups workspace only if the RBI 581 license is active.
Procedure
What To Do Next
- When you are on the Risk Based Inspection Overview page of a Functional Location which is a Process Unit, selecting Manage Inventory Groups option will navigate to the associated Process Unit in the Inventory Groups workspace.
- Inventory Grouping is not supported on assets which are not process units.
Create an Inventory Group Configuration Record
Before You Begin
- You can create or modify an Inventory Group Configuration record only if you are a super user or a member of the MI RBI Administrator or MI RBI Analyst Security Groups.
Procedure
Results
- The Linked Components tab is enabled.
What To Do Next
Delete an Inventory Group Configuration Record
Before You Begin
- You can delete an Inventory Group Configuration record only if you are a super user or a member of the MI RBI Administrator or MI RBI Analyst Security Groups.
Procedure
Results
- If you create an RBI 581 Risk Analysis for components that once belonged to the deleted inventory group, the value in the Inventory Group Mass field will no longer be populated automatically.
Link Components to an Inventory Group
Before You Begin
- Create an Inventory Group Configuration record.
- You can link RBI Components to an Inventory Group only if you are a super user or a member of the MI RBI Administrator or MI RBI Analyst Security Groups.
Procedure
Results
- In the RBI Component records that you have linked, the Inventory Group field is populated with the value in the Inventory Group Name field of the inventory group.
- If you create an RBI 581 Risk Analysis for a component that you have linked to the inventory group, then in the associated RBI 581 Consequence Evaluation, the Use Calculated Inventory check box is selected, and the value in the Inventory Group Mass field is calculated.
- The value in the Inventory Group Mass field in the RBI 581 Consequence Evaluation associated with the remaining components in the inventory group is updated. Tip: To view the updated value in the Inventory Group Mass field, you must clear the Use Calculated Inventory check box, and then select it.
Unlink Components from an Inventory Group
Procedure
Results
- The value in the Inventory Group Mass field in the RBI 581 Consequence Evaluation of the remaining components in the inventory group is updated.Tip: To view the updated value in the Inventory Group Mass field, you must clear the Use Calculated Inventory check box, and then select it.