Database Comparison Tool

About the GE Digital APM Database Comparison Tool

Using the GE Digital APM Database Comparison Tool, you can compare different databases. The following table identifies the purposes of available comparisons, and when you need to initiate each comparison.

Note: Note: All comparisons are made against the same constant: the baseline GE Digital APM database for the target version.

Variable

Purpose of Comparison

When to Perform Comparison

The content of the baseline GE Digital APM database for the source version.

Allows you to see the changes that GE Digital APM has made since releasing the version from which you are upgrading.

Before upgrading your database.

The content of your customized database for the source version.

Allows you to see how the content of the baseline database for the target version compares to the changes you have made in the source version.

Before upgrading your database.

The content of your customized database for the target version.

Allows you to see how the content of the baseline database for the target version compares to the changes you have made in that version.

After upgrading your database.

You can use the GE Digital APM Database Comparison Tool to:

The GE Digital APM Database Comparison Tool works like a builder, which contains two screens:

  • Connection Information: Lets you specify the connection information to the database whose content you want to compare against the content of the baseline database for the target version.



    Comparison Details: Lets you run the comparison to identify the differences between the content of the two databases that you are comparing.



    On this screen, you can also:

Run the Comparison Against a Pre-Upgraded Database

Before You Begin

  1. On the GE Digital APM Server, navigate to C:\Windows\assembly to verify that the 64-bit version of the Oracle.DataAccess component is installed.
  2. If it is installed, then skip the rest of the steps in this Before You Begin section and proceed to step 1 in the Steps section.

    -or-

    If the 64-bit version of the component it is not installed, then obtain it from Oracle and install it on the GE Digital APM Server. You must then complete the following additional steps.

    1. On the GE Digital APM Server, navigate to the folder C:\Windows\Microsoft.NET\Framework64\V4.0.30319\CONFIG\.
    2. Using a text editor (e.g., Notepad), open the file machine.config.
    3. In the file, between the opening and closing <configuration> tags, add the following content.


    4. Save the file, and then close it.

      You can now proceed to step 1 in the Steps section.

Procedure

  1. On the GE Digital APM Server, navigate to the folder C:\Program Files\Meridium\Client\100.0.0.0.0, and then open the file DatabaseReport.exe.

    The GE Digital APM Database Comparison Tool appears, displaying the Connection Information screen.



  2. In the Meridium Datasource box, enter the name of the data source that you want to use in the comparison.
  3. In the Meridium User Name box, enter the User ID for a Security User that can log in to the specified data source.
    Note: The specified Security User must be a Super User.
  4. In the Meridium Password box, enter the password associated with the specified Security User.
  5. In the Source Version box, enter the seven-digit database version that matches the version of your source database that is being compared. You must enter the version in the format vvvmmzz, where:
    • vvv is a three-digit number representing the main version.
    • mm is a two-digit number representing the maintenance release version, if applicable. If the maintenance release version is a single digit, you must prepend zero (0) to it. If there is no maintenance release version, you must enter 00.
    • zz is a two-digit number representing the hot fix version, if applicable. If the hot fix version is a single digit, you must prepend zero (0) to it. If there is no hot fix version, you must enter 00.

    For example, the database version number for V3.5.1MR6HF2 would be 3510602.

    If you do not know the main version, service pack version, and hot fix version of your database, you can find it using either of the following methods:

    • Run the following query against the database:

      Select modl_ver_nbrfrom mi_modules, where modl_nm = 'Meridium Core';

    • In Configuration Manager, on the About Meridium APM window (accessed via the Help menu), for the GE Digital APM Framework Tools license, locate the value in the Version column. The database version you should enter in the Source Version box is this version number without the periods.



  6. In the Path to Database Upgrade content box, if a path is provided, confirm that it is the correct path pointing to the newer V4.X baseline content. If a path is not provided, you may enter the appropriate path.

    The path identifies the location of the newer baseline content file (e.g., MI_DB_Master_4000000.zip). The default path is C:\Meridium\DbUpg.

  7. When you are finished specifying connection information, select Next.

    If your database connection entries are valid, the Comparison Details screen appears.



    The following information appears in the Summary Information section:

    • Comparison From: The database versions that will be compared, using the format <source version> to <target version>, where:

      • <source version> is the version of the source database that you are comparing against. The source version on the left should match the value in the Source Version box on the Connection Information screen.
      • <target version> is the version of the database content to which you are upgrading. The target version on the right should match the file that you specified in the Path to Database Upgrade content box on the Connection Information screen.
    • User: The credentials of your Windows user.
    • Last Comparison Time: The date and time of any previous database comparison performed with this database. If the comparison has never been performed with this database, then the current date and time is displayed.
  8. Select Run Comparison.
    A progress bar appears.

    Eventually, a command prompt window will appear, displaying the progress of the various comparison stages.



    When the comparison is complete, the command prompt window closes automatically, and the comparison results appear in the Upgrade Comparison section of the Comparison Details screen.



About the Pre-Upgrade GE Digital APM Database Comparison Tool Comparison Results Grid

When you perform a pre-upgrade database comparison, the results appear in a grid on the Comparison Details screen.



The grid contains the name of each item that was identified as different during the comparison process. You can determine the general difference using the Baseline Changes and Custom Changes columns. You can select any hyperlink in the left-most Item Name column to display more detailed comparison results using WinMerge.

The comparison results grid contains the following columns:

  • Item Name: The name of the item. You can select any hyperlink in the Item Name column to display more detailed comparison results using WinMerge.

  • Item Path: If the item is a Catalog item, this column displays the Catalog folder path. If the item is not a Catalog item, this column repeats the item name.

  • Type: The type of item.

  • Baseline Changes and Custom Changes: Contain black circles indicating that changes exist. In general, the Baseline Changes column contains a black circle if the baseline item has changed since the previous version. Likewise, the Custom Changes column contains a black circle if you have made custom changes to that item or if the item does not exist in your upgraded database.

The following table illustrates the possible combination of dots per item and explains how you can interpret those combinations.

Baseline Changes

Custom Changes

Explanation

Example

 

The baseline item has changed between the two versions.

-and-

The item in your pre-upgrade database is the same as the item in the baseline database.

You are upgrading from V3.6.0.x to V4.0.0.0.

In V3.5.0.0.0, the baseline family Asset Strategy was modified.

You have not modified this family in your database.

 

The baseline item has not changed between the two versions.

-and-

There is difference between the baseline version of this item and the item in your upgraded database.

You are upgrading from V3.6.0.x to V4.0.0.0.

The baseline query Reading History has not been modified since the last version release.

You have modified this query prior to the upgrade.

The baseline item has changed between the two versions or is new to the later version.

-and-

There is a difference between the baseline version of this item and the item in your upgraded database, or this item does not exist in your upgraded database.

You are upgrading from V3.6.0.x to V4.0.0.0.

In V3.5.0.0.0, the baseline query Asset Query was modified.

You have modified this query prior to the upgrade.

You can select any column heading to sort the results by the values in that column. You can also filter the results by selecting in any column heading, and then selecting the value by which you want to filter the results. For example, to see only queries in the results, you would select in the Type column heading, and then select the Query check box, as shown in the following image.



The result would then contain only queries, as shown in the following image.



After you apply a filter, it will be displayed below the results, as outlined in red in the following image.



You can remove a filter by selecting below the grid.

Run the Comparison Against an Upgraded Database

About This Task

These instructions assume that you want to compare your upgraded database to the baseline version.

Important: The comparison process can take an hour or longer, depending upon the size of the databases being compared, available memory, and other factors. After you start the process, you should not close the progress window unless you want to stop the comparison process. You can continue working in other windows while the comparison is running.

Procedure

  1. On the GE Digital APM Server, on the Apps interface, in the Meridium APM Applications section, select Database Upgrade Manager.
    The Meridium APM Database Comparison Tool window appears, displaying the Connection Information screen.

  2. In the Meridium Data Source box, enter the predefined data source that points to your upgraded GE Digital APM database.
  3. Enter the name of a GE Digital APM Security User defined in your database.
  4. Enter the password for that Security User.
  5. Enter the version of the upgraded source database. For V4.0.0.0.0, this value would be 4000000.
  6. In the Path to Database Upgrade content box, ensure that the correct path to the content is provided.
    The path identifies the location of the baseline .zip file for the upgraded version. The default path is C:\Meridium\DbUpg, but this path could have been changed manually via the GE Digital APM Server and Add-ons installer when GE Digital APM was installed or upgraded.
  7. Select Next.
    The Comparison Details screen appears.


    The following information appears in the Summary Information section:

    • Comparison From: The database versions that will be compared, using the format:

      <source version> to <target version>

      ...where

      • <source version> is the version of the source database that you are comparing against. The source version on the left should match the value in the Source Version box on the Connection Information screen.
      • <target version> is the version of the database content to which you are upgrading. The target version on the right should match the file that you specified in the Path to Database Upgrade content box on the Connection Information screen.
    • Connection Information: The name of the current database.
    • File Path: The path to the Database Upgrade content .zip file.
    • User: The credentials of your Windows user.
    • Last Comparison Time: The date and time on which the database comparison for this database was last run. If the comparison has never been run for this database, the current date and time is displayed.
  8. Select Run Comparison.
    A progress bar appears, displaying the progress of the comparison process. Eventually, a command prompt window will appear, displaying the progress of the various comparison stages.


    When the process is complete, the command prompt window closes automatically, and the comparison details appear in the Upgrade Comparison section on the Comparison Details screen of the GE Digital APM Database Comparison Tool.

About the Post-Upgrade GE Digital APM Database Comparison Tool Comparison Results Grid

When you perform a post-upgrade database comparison, the results appear in a grid on the Comparison Details screen.



The grid contains the name of each item that was identified as different during the comparison process. The comparison results grid contains the following columns:

  • Item Name: The name of the item. You can select any hyperlink in the Item Name column to display more detailed comparison results using WinMerge.

  • Item Path: If the item is a Catalog item, this column displays the Catalog folder path. If the item is not a Catalog item, this column repeats the item name.

  • Type: The type of item.

  • Custom Changes: The cells in this column contain black circles indicating that custom changes have been made to the associated item.

You can select any column heading to sort the results by the values in that column. You can also filter the results by selecting in any column heading, and then selecting the value by which you want to filter the results. For example, to see only items that are in Entity Families in the results, you would select in the Type column heading, and then select the Are in These and Entity Family check boxes, as shown in the following image.



The result would then contain only queries, as shown in the following image.



After you apply a filter, it will be displayed below the results, as outlined in red in the following image.



You can remove a filter that you have applied by selecting next to the filter.

Revert Items to Baseline

Before You Begin

  • Create a data source.

Procedure

  1. On the GE Digital APM Server, navigate to Meridium/Upgrade/DBUpgrade, and then open the file RevertToBaselineApp.exe.
    The Revert To Baseline Login Screen window appears.

  2. Enter a valid data source, user name, and password, and then select Next.
    Note: The value in the Meridium Data Source box should match exactly the Data Source ID of the data source.

    The Revert To Baseline screen appears, displaying the families that you can revert to baseline.



  3. Select the row containing the family whose element you want to revert to baseline, and then select Revert To Baseline.
    Tip: You can enter a value in the Search box to search for a specific family.
    Note: If you want to revert records and links for a family for which the value in the Is Composite Family column is Yes, you will need to revert the records and links for the parent family of that family. If this is the case, based on the following table, please select the appropriate parent family for the child family whose records and links you want to revert to baseline.
    Child Family to RevertParent Family to Select
    MI_STRMAPPMI_STMPCNFG
    MI_RRSKMDTMI_RRSKMAP

    MI_CLMND_PR

    MI_MPPG_QRY

    MI_DATA_GRP

    MI_PROTDEFI

    MI_RISKTHRE

    MI_PROBDEFI

    MI_CONSDEFI

    MI_RISKCATE

    MI_RISKMATR

    The Various Options For Revert window appears.



  4. Select the check box for the revert to baseline action that you want to execute, and then select OK.
    Note: If you selected the Datasheets check box, before selecting OK, you will need to select a datasheet in the drop-down list box next to the Datasheets check box.

    If you selected the Associated Pages, Datasheets, Privileges, Project, or Behavior check box, the Success window appears, displaying a message indicating that the revert to baseline action has been completed. The following image shows the Success window after the action of reverting Privileges to baseline has been completed.



    1. Select OK.

      The Success and Various Options For Revert windows close.

    -or-

    If you selected the Records and Link check box, the Revert to Baseline - Records and Links window appears.



    1. In the list on the left side of the window, select the family that contains the records and links that you want to revert to baseline.

      The selected records and links appear in the list on the right side of the window.

    2. If you want to revert the records and links for records in the family, in the list on the right side of the window, select the check box next to each record that you want to revert to baseline, and then select Revert Selected.

      -or-

      If you want to revert customized template values for the family to baseline, select a family on the left side of the window, and then, in the My Template Defaults row that appears, select Compare. Then, on the My Template Defaults window that appears, select Revert.

      A message appears, indicating that the selected records and links have been reverted to baseline.

    -or-

    If you selected the State Management check box, the State Management Mapper window appears.



    The family of the item that you selected in the Comparison Results grid is highlighted in the tree in the Entity Families section of the State Management Mapper window. In the Custom section, a list of the customized states for the family appears. In the Baseline section, a list of the baseline states for the family appears.

    The customized states for the family also appear in the Custom Source column in the grid in the State Management Baseline Mapping section.

    1. In the State Management Baseline Mapping section, in each cell in the Select Target column, select the baseline target for each customized state in the Custom Source column.
      Note: If you select Auto Map, the GE Digital APM Database Comparison Tool will automatically assign baseline targets where possible. If you select Load Map, a window appears on which you can select a previously saved map of baseline target assignments.

      The selected targets appear in the cells in the Baseline Target column.

    2. Select Revert Single Family or Revert Multiple.

      If you selected Revert Single Family, a message appears, asking if you want to save the current mapping and revert to it.



      1. Select Yes.

        A confirmation message appears.



      2. Select OK.

        The selected states are converted.

      -or-

      If you selected Revert Multiple, the Browse For Folder window appears.



      1. Navigate to the folder containing all of the families whose states you want to convert, and then select OK.

        A message appears, asking you to confirm that you want to continue.



      2. Select Yes.

        A confirmation message appears.



      3. Select OK.

        The selected states are converted.

  5. As needed, repeat steps 1 through 2 to revert additional items to baseline.

Save the Results to a .ZIP File

About This Task

After running the pre- or post-upgrade version of the GE Digital APM Database Comparison Tool, if you save comparison results to a .ZIP file using the following instructions, you can reload those results at a later time. These instructions assume that you have already launched the GE Digital APM Database Comparison Tool.

Procedure

  1. On the Comparison Details screen, select Save Results.

    The Select file to save result window appears. The folder path is set by default to C:\Meridium\DbUpg.



  2. If you want to save the results to a location other than C:/Meridium/DbUpg, navigate to the location where you want to save the results.
  3. In File name box, enter a name for the .zip file.
  4. Select Save.
    The results are saved to the .zip file with the specified name in the specified location.

Reload Previous Comparison Results

About This Task

Using the pre- or post-upgrade version of the GE Digital APM Database Comparison Tool, if you have saved previous comparison results to a .ZIP file, you can reload those results by following these instructions. These instructions assume that you have already launched the GE Digital APM Database Comparison Tool.

Procedure

  1. On the Connection Information screen, select Load Results.
    The Select export of result window appears. By default, the folder path is set to C:\Meridium\DbUpg.


  2. If the results that you want to reload are stored in a location other than C:/Meridium/DbUpg, navigate to the location containing the exported results.
  3. Select the .zip file containing the results that you want to reload, and then select Open.
    A progress bar appears, indicating the progress of the loading process.


    When the process is complete, the comparison results appear on the Comparison Details screen.



Export Comparison Results to an Excel File

About This Task

If you have run a database comparison using the pre- or post-upgrade version of the GE Digital APM Database Comparison Tool and want to make the result available to users who do not have access to the GE Digital APM Server, you can save the results to a Microsoft Excel file. The Excel file will contain the data that appears in the grid on the Comparison Details screen of the GE Digital APM Database Comparison Tool. It will not present a detailed side-by-side comparison.

These instructions assume that you have already launched the GE Digital APM Database Comparison Tool.

Procedure

  1. On the Comparison Details screen, select Export.
    The Select file to save result window appears. By default, the folder path is set to C:\Meridium\DbUpg.

  2. If you want to export the results to a location other than C:/Meridium/DbUpg, navigate to the location to which you want to export the results.
  3. In File name box, enter a name for the Excel file, and then select Save.
    The results are saved to the Excel file with the specified name in the specified location, and a message appears, indicating that the file was saved successfully. The content of the Excel file will look similar to this:

    The file contains one worksheet, ExportToExcel, with the following columns of information:

    • ModifiedID: Displays the value that appeared in the Item Name column in the GE Digital APM Database Comparison Tool.
    • ItemPath: Displays the value that appeared in the Item Path column in the GE Digital APM Database Comparison Tool.
    • ItemType: Displays the value that appeared in the Type column in the GE Digital APM Database Comparison Tool.
    • HasBaselineChanges: Displays a value indicating whether or not a black circle appeared in the Baseline Changes column in the GE Digital APM Database Comparison Tool. If no black circle appeared, then the value is False. If a black circle appeared, then the value is True.
    • HasCustomChanges: Displays a value indicating whether or not a black circle appeared in the Custom Changes column in the GE Digital APM Database Comparison Tool. If no black circle appeared, the value is False. If a black circle appeared, the value is True.

View Detailed Differences in WinMerge

About This Task

In the comparison results grid, for any item in the grid, you can access a detailed comparison of the differences between that item in your customized database and the baseline database for the target version. The detailed differences will be displayed in WinMerge. Information on using WinMerge exceeds the scope of the GE Digital APM documentation, but can be found in the WinMerge Help system.

Procedure

  1. In the comparison results grid, select the hyperlinked name of the item whose differences you want to view.
    The Difference Details screen appears.


  2. If differences are referenced in the upper section, select Baseline Changes.
    If differences are referenced in the upper section, select Baseline Changes.

    -or-

    If differences are referenced in the lower section, select Custom Changes.

    The sections shown in the following images can be accessed via the appropriate tabs:

    • In this section, the XML code for the item exists in one file per version (e.g., an entity family).



    • In this section, the item exists in multiple files per version (e.g., a query), which you can use to select the two specific files that you want to compare.



  3. In the section displaying the detailed differences, scroll through the differences using WinMerge tools.
  4. In the section that allows you to select two specific files that you want to compare, select the two files, right-click, and then select Compare.


    WinMerge appears, displaying the results of the comparison.