Database Server Installation
Deploy the GE Digital APM Database Server for the First Time
The installation and configuration steps differ depending on whether you are connecting to an Oracle or SQL Server Database. Use the checklist appropriate to the type of database that you are using.
Use the checklist appropriate to the type of database that you are using.
Oracle Checklist
The following checklist should be used to install and configure an Oracle Database Server, create the GE Digital APM schema, and configure the GE Digital APM Server for use with Oracle.
You should complete these steps in relatively the same order in which they are listed in the table.
Step | Task | Notes |
---|---|---|
1 | Ensure that the GE Digital APM Database Server machine meets the system requirements. | This step is required. |
2 | On the GE Digital APM Database Server, install the Oracle Server software. | This step is required. |
3 | On the GE Digital APM Database Server, create the Oracle database. | This step is required. |
4 | On the GE Digital APM Database Server, configure the Oracle database. | This step is required. |
5 | On the GE Digital APM Database Server, create the GE Digital APM Oracle schema. | This step is required. |
6 | On the GE Digital APM Database machine, Create the Oracle Scheduler Database. | This step is required. |
7 | On the GE Digital APM Database machine, Create the Oracle Scheduler Schema. | This step is required. |
8 | On the GE Digital APM Database machine, Create the Localization Oracle Database. | This step is required. |
9 | On the GE Digital APM Database machine, Create the Localization Oracle Schema. | This step is required. |
10 | On the GE Digital APM Server, create an initial data source. | This step is required. |
11 | In GE Digital APM, build the search index. | This step is required. |
Install the Oracle Server Software
About This Task
The first step in setting up the database server for the GE Digital APM schema is to install the Oracle Server software on the database server machine. Instructions for installing the Oracle Server software exceed the scope of this documentation. For information on performing the installation, refer to the Oracle installation documentation that is specific to your database server platform. If you plan to create a database via the Oracle Universal installer, then, before proceeding, you should review the section in this documentation on Creating and configuring the Oracle database.
What To Do Next
Create the Oracle Database
Before you create the Oracle schema that will contain the GE Digital APM repository, you must install the Database Server software on the GE Digital APM Database Server machine. The creation of the Oracle database exceeds the scope of this documentation. For details on creating an Oracle database, consult the Oracle documentation that is specific to your database platform.
When the database is created, the database character set must be specified. If you are creating a Unicode database, use the character set AL32UTF8. This is the most recent and recommended Unicode database character set.
What To Do Next
Configure the Oracle Database
After you have created the Oracle database, you will need to configure it. Details on configuring the Oracle database exceed the scope of this documentation. For details on configuring an Oracle database, consult the Oracle documentation that is specific to your database platform. Note, however, that the Oracle database must meet the following requirements:
The following database parameter values are recommended and must persist from one database startup to the next.
Database parameter value |
Notes |
---|---|
dml_locks=5000 |
The dml_locks parameters should be set to a large value to avoid the possibility of waiting for a lock. |
open_cursors=500 |
It is not uncommon for one GE Digital APM user to have multiple cursors open simultaneously. For this reason, you should set this value accordingly. |
parallel_max_servers=0 |
The GE Digital APM schema is not configured for parallel query. Therefore, we recommend that you disable this feature. Enabling parallel query when the database and schema are not properly configured can severely degrade system performance. |
parallel_min_servers=0 |
The GE Digital APM schema is not configured for parallel query. Therefore, we recommend that you disable this feature. Enabling parallel query when the database and schema are not properly configured can severely degrade system performance. |
processes=500 |
None |
query_rewrite_enabled=true |
None |
timed_statistics=true |
Setting timed_statistics allows for minimum maintenance and enables reporting on internal wait events, which can be used to reconfigure your database. |
Memory_target= 4G |
Suggested minimum |
Default values for database parameters that are not mentioned in the above list meet or exceed recommendations for a GE Digital APM database configuration. GE Digital APM recommends that you monitor the database so that changes can be made as necessary to accommodate the needs of your specific installations. For more information on these and other database parameters, consult the Oracle documentation.
What To Do Next
Create the GE Digital APM Oracle Schema on the GE Digital APM Database Server
About This Task
The following instructions provide details on creating the GE Digital APM Oracle schema. After you have created the Oracle schema using these instructions, the schema will be referred to as the GE Digital APM database throughout this documentation.
To perform these steps, you will need Oracle DBA privileges on the GE Digital APM Database Server machine. These instructions assume that:
- You are logged in to your GE Digital APM Database Server machine with DBA privileges and have a connection to Oracle.
- You are familiar with running SQL scripts and the associated terminology.
Procedure
What To Do Next
Create the Oracle Scheduler Database
Before you create the Oracle schema that will contain the GE Digital APM repository, you must install the Database Server software on the GE Digital APM Database Server machine.
Create an Oracle database that will be used by the GE Digital APM Scheduler. You may set the database name as apm_scheduler. The creation of the Oracle database exceeds the scope of this documentation. For details on creating an Oracle database, consult the documentation that is specific to your database platform.
When the database is created, the database character set must be specified. If you are creating a Unicode database, use the character set AL32UTF8. This is the most recent and recommended Unicode database character set.
What To Do Next
Create the Oracle Scheduler Schema
About This Task
The following instructions provide details on creating the Scheduler Oracle schema.
To perform these steps, you will need Oracle DBA privileges on the GE Digital APM Database Server machine. These instructions assume that:
- You are logged in to your GE Digital APM Database Server machine with DBA privileges and have a connection to Oracle.
- You are familiar with running SQL scripts and the associated terminology.
Procedure
What To Do Next
Create the Localization Oracle Database
Before you create the Oracle schema that will contain the GE Digital APM repository, you must install the Database Server software on the GE Digital APM Database Server machine.
Create an Oracle database that will be used by the GE Digital APM Localization. You may set the database name as apm_localization. The creation of the Oracle database exceeds the scope of this documentation. For details on creating an Oracle database, consult the documentation that is specific to your database platform.
When the database is created, the database character set must be specified. If you are creating a Unicode database, use the character set AL32UTF8. This is the most recent and recommended Unicode database character set.
What To Do Next
Create the Localization Oracle Schema
About This Task
The following instructions provide details on creating the Localization Oracle schema.
To perform these steps, you will need Oracle DBA privileges on the GE Digital APM Database Server machine. These instructions assume that:
- You are logged in to your GE Digital APM Database Server machine with DBA privileges and have a connection to Oracle.
- You are familiar with running SQL scripts and the associated terminology.
Procedure
What To Do Next
SQL Server Checklist
The following checklist should be used to install and configure a SQL Server Database Server, create the GE Digital APM database, and configure the GE Digital APM Server for use with the SQL Server.
You should complete these steps in relatively the same order in which they are listed in the table.
Step |
Task |
Notes |
---|---|---|
1 | Ensure that the GE Digital APM Database Server machine meets the system requirements. | This step is required. |
2 | On the GE Digital APM Database Server, install the SQL Server software. | This step is required. |
3 | On the GE Digital APM Database Server, create the SQL Server database. | This step is required. |
4 | On the GE Digital APM Database Server, configure the SQL Server database. | This step is required. |
5 | On the GE Digital APM Database server machine, Create the SQL Server Scheduler Database. | This step is required. |
6 | On the GE Digital APM Database server machine, Configure the SQL Server Database. | This step is required. |
7 | On the GE Digital APM Database server machine, Create the SQL Server Localization Database. | This step is required. |
8 | On the GE Digital APM Database server machine, Configure the SQL Server Localization Database. | This step is required. |
9 | On the GE Digital APM Server, create an initial data source. | This step is required. |
10 | In GE Digital APM, build the search index. | This step is required. |
Install the SQL Server Software
About This Task
When you prepare to install SQL Server on the Database Server, you should consider the following notes:
Procedure
- GE Digital APM requires mixed-mode authentication for SQL Server installations. The documentation and scripts supplied by GE Digital assume that the SQL Server instance allows mixed-mode authentication.
- The GE Digital APM database must be owned by the SQL Server login referenced in the GE Digital APM data source. Being a member of the SQL Server db_owner role is not sufficient. GE Digital provides a script to properly configure the SQL Server database for use with GE Digital APM.
- The database supplied by GE Digital (via a .bak file) was created with the SQL Server collation Latin1_General_CI_AS.
What To Do Next
About Creating and Configuring the SQL Server Database
After you have installed the SQL Server software on the Database Server machine, you can create the GE Digital APM database by restoring a database backup file that is provided by GE Digital. For example, the restore database option in SQL Server Management Studio could be used to create the database. Specific instructions for creating the GE Digital APM database are not included in this documentation.
After you have created the database, you will need to configure it. To create and configure the GE Digital APM database, you must have access to:
- Microsoft SQL Server Management Studio.
- A privileged SQL Server account with sysadmin rights in the target instance.
- Two files from the GE Digital APM distribution package that will be extracted on the GE Digital APM Server:
- GE Digital APM, which is included in the file
GE Digital APM
in the GE Digital APM distribution package.
-and-
- MI_SQL_DB_Configure.sql, which was extracted from the GE Digital APM distribution package.
- GE Digital APM, which is included in the file
GE Digital APM
in the GE Digital APM distribution package.
These instructions assume that you are familiar with SQL Server Management Studio or another third-party tool for running SQL scripts.
MI_SQL_DB_Configure.sql
script.What To Do Next
Create the SQL Server Database
The following instructions provide details on locating the files that are needed for creating and configuring the SQL Server database. To create the database, you will restore a backup file that is included in your GE Digital APM distribution package. For example, the restore database option in SQL Server Management Studio could be used to create the database. Specific instructions on creating the SQL Server database are not included in this documentation.
Steps
- On the GE Digital APM Server, access the GE Digital APM distribution package, and then navigate to the Database folder.
- Open the MI_DB_MASTER_<version>.zip file, and then extract the contents of the file to a folder on the C: drive.Important: The name of the folder to which you extract the files must not contain any spaces.
- Open _Setup\NewInstall\SQLServer, and then locate the MI_<version>.BAK file.
- Place the MI_<version>.BAK file in a location where it can be referenced by the SQL Server service, and then restore the file.
The GE Digital APM database is created.
What To Do Next
Configure the SQL Server Database
About This Task
The following instructions explain how to configure a SQL Server database for use by GE Digital APM. These instructions assume that the SQL Server database has already been created by restoring a backup file using SQL Server Management Studio or another third-party tool.
These instructions provide details on configuring the GE Digital APM SQL Server database using the script MI_SQL_DB_Configure.sql
, which is included in your GE Digital APM distribution package. This script ensures that the database will be properly configured for use with GE Digital APM.
When you run the script MI_SQL_DB_Configure.sql
, the following database settings will be configured automatically:
- The database will be set to read/write mode.
- The database will be configured to allow multiple users.
- The database will be set to Full recovery mode.
- A SQL Server login will be created, and this login will own the database.
- The SQL Server database name, SQL Server login name, and password will all match.
Procedure
- Open a SQL Server Management Studio query window that is connected via a privileged login.
- Open the file MI_SQL_DB_Configure.sql, and then copy its contents into the SQL Server Management Studio query window.
- Set the @dbname variable to the name of the GE Digital APM SQL Server database that you created.
- Execute the edited script.
- As needed, use SQL Server Management Studio to modify the password. These are the same login credentials that will be used when you create the GE Digital APM data source that will connect to this database.
- Create the custom server-level error messages, which are required by the GE Digital APM system. These error messages must be created at the instance level. Creating them requires a privileged login assigned to either the System Administrator (sysadmin) or Server Administrator (serveradmin) fixed server roles. To create the GE Digital APM error messages:
- Make sure that you are connected to the Database Server with SQL Server Management Studio as a System Administrator or Server Administrator user
- Execute the stored procedure MI_ERRORS_CRT_ALL_MSGS. This procedure was supplied with the GE Digital APM database and can be executed by using the command
exec <databasename>..MI_ERRORS_CRT_ALL_MSGS
, where<databasename>
is the name of the database you created in the preceding steps.
What To Do Next
Create the SQL Server Scheduler Database
Create SQL Server database that will be used by the GE Digital APM Scheduler. You may set the database name as apm_scheduler. The creation of the SQL Server database exceeds the scope of this documentation. For details on creating an SQL Server database, consult the documentation that is specific to your database platform.
What To Do Next
Configure the SQL Server Scheduler Database
About This Task
The following instructions explain how to configure a SQL Server database for use by GE Digital APM Scheduler. These instructions assume that the SQL Server database has already been created by restoring a backup file using SQL Server Management Studio or another third-party tool.
Procedure
- Create an empty database with username. You may set the database name as apm_scheduler.
- Run MI_SQL_DB_Configure.sql to configure the database (password).
- Open a SQL Server Management Studio query window that is connected via a privileged login.
- Open the GE Digital APM distribution package and navigate to the Database folder.
- Open the file MI_DB_MASTER_<version>.zip, and then extract the contents of the file <version>.zip to a folder on the C: drive.
- Open the file <version>.zip, and then open the subfolder _Setup\NewInstall\SQLServer.
- Execute the Scheduler.sql script. This script will create the required objects for APM Scheduler.
- On the GE Digital APM server, navigate to C:\ProgramData\Meridium.
- Open the appsettings.Global.json file using a text editor.
- Modify the following values:
Create the SQL Server Localization Database
Create SQL Server database that will be used by the GE Digital APM Scheduler. Name the database as apm_localization. The creation of the SQL Server database exceeds the scope of this documentation. For details on creating an SQL Server database, consult the documentation that is specific to your database platform.
What To Do Next
Configure the SQL Server Localization Database
About This Task
The following instructions explain how to configure a SQL Server database for use by GE Digital APM Localization. These instructions assume that the SQL Server database has already been created by restoring a backup file using SQL Server Management Studio or another third-party tool.
Procedure
- Open a SQL Server Management Studio query window that is connected via a privileged login.
- Open the GE Digital APM distribution package and navigate to the C:\Meridium\DbUpg\DBBackupFiles folder.
- Open the subfolder \SQL.
- Restore database using the backup file apm_localization.bak. This database includes the required objects for GE Digital APM localization.
- Run MI_SQL_DB_Configure.sql to configure the database (password).
- On the GE Digital APM server, navigate to C:\ProgramData\Meridium.
- Open the appsettings.Global.json file using a text editor.
- Modify the following values: