Access the Sub Group Summary Page
Access the Sub Group Summary Page
About This Task
Procedure
- Access the GAA Wind Overview page.
- Select Show Sub Group Summary.The Sub Groups window appears, displaying a list of all Sub Groups.Note: If you select Show Sub Group Summary when only one Sub Group exists in GE Digital APM, the Sub Group Summary page for that Sub Group appears.
- Select the Sub Group whose Sub Group Summary page you want to access.
- Select Navigate to Sub Group.The Sub Group Summary page for the selected Sub Group appears, displaying the following workspaces:
- Events: Contains a table of Events associated with the Sub Group for the start date and end date specified in the GAA Wind Overview page. The table contains the following columns:
- UNIT NAME: Represents the Unit Name field of the Event.
- ERROR CODE: Represents the Error Code field of the Event.Note: If the Event has an error,
appears next to the value in this column.
- START DATE (Timezone Value): Represents the Start Date field of the Event.Note: The Timezone Value indicates the value of the timezone selected in the Consider Dates in dropdown list in the Filter.
- END DATE (Timezone Value): Represents the End Date field of the Event.Note: The Timezone Value indicates the value of the timezone selected in the Consider Dates in the dropdown list in the Filter.
- DURATION: Represents the Duration field of the Event. The duration of the Event is displayed in the hh:mm:ss format.
- DESCRIPTION: Represents the Description field of the Event.
- IEC STATE: Represents the IEC Event Type field of the Event.Note: If the value in the IEC Event Type field of the Event is IU,
appears next to the value in this column.
- NERC STATE: Represents the NERC Type field of the Event.
- ACTUAL PRODUCTION: Represents the production value of the Event.
- EDITED: Contains check boxes to indicate if the Event has been edited.Note: A selected check box in this column indicates that the Event has been edited (that is, the value in any of the fields of the Event have been modified or the Event was created by splitting another Event), whereas a cleared check box indicates that the Event has not been edited.
The From and To values in the Filter By Date Range filter will also be considered in the timezone which is selected in the Consider Dates in dropdown list in the Filter.
The event data retrieved includes the following spanning events as well.
- If the start time stamp of an Event is earlier than the value specified in the From box in the Filter window.
- If the end time stamp of an Event is later than the value specified in the To box in the Filter window.
- Performance: Contains Performance Records associated with the Sub Group.
- Reports: Contains reports (that is, Performance Reports or Sub Group Reports) associated with the Sub Group.
Note:- You can perform the following actions on the table that contains the events.
- Sort or filter data.
- Group columns.
- Reorder or resize columns.
- Change page numbers.
- Set your preferences to view the number of records per page.
- The changes made to the table are unique to each Sub Group and user session. If you sign out of GE Digital APM or refresh the page, the changes made to the table are not retained.
- Events: Contains a table of Events associated with the Sub Group for the start date and end date specified in the GAA Wind Overview page. The table contains the following columns: