Cross Domains Configuration

About Cross Domains

You can add and configure multiple domains to retrieve user information from multiple Active Directory servers to GE Digital APM during the LDAP synchronization process.

Configuring Multiple Cross Domains for Synchronizing User Information

You can add and configure multiple cross domains in the Cross Domains page. The configured cross domains are used to create multiple LDAP domain records. After the LDAP domain records are created, using the LDAP synchronization process, you can retrieve the user information for the Microsoft Active Directory users associated with the Microsoft Active Directory domains that have been defined in GE Digital APM.

Note: If Single Sign-On (SSO) authentication is enabled for the users to access GE Digital APM, you can use only one cross domain to retrieve user information from the associated Active Directory server using the LDAP synchronization process.

Access the Cross Domains Page

Procedure

In the Applications menu, navigate to ADMIN > Operations Manager > Cross Domain Configuration.
The Cross Domains page appears.

Configure a New Cross Domain

Procedure

  1. In the Applications menu, navigate to ADMIN > Operations Manager > Cross Domain Configuration.
  2. In the pane that displays the list of domain names, select .
    The workspace to configure a new domain appears.
  3. In the Domain Name box, enter the name of the server or the domain that you want to configure.
    Note: The Domain name includes a domain suffix. For example, enter domain.com instead of domain in the Domain Name box.
  4. In the User Name box, enter the user name of the domain administrator.
  5. In the Password box, enter the password that is associated with the specified User Name.
  6. In the Used For drop-down list box, select an appropriate value for which you want to use the domain.
    Note: If you want to configure the domain to synchronize user information by running the LDAP synchronization process, select LDAP.
  7. Select .

Modify a Cross Domain

Procedure

  1. In the Applications menu, navigate to ADMIN > Operations Manager > Cross Domain Configuration.
  2. In the pane that displays the list of domain names, select the domain that you want to modify.
    The workspace for the selected domain appears.
  3. As needed, modify the fields.
  4. Select .
    The domain is modified.

Delete a Cross Domain

Procedure

  1. In the Applications menu, navigate to ADMIN > Operations Manager > Cross Domain Configuration.
  2. In the pane that displays the list of domain names, select the domain that you want to delete.
    The workspace for the selected domain appears.
  3. Select .
    The Confirm Delete window appears.
  4. Select Yes.
    The domain is deleted.