Automatic Data Loader
About the Automatic Data Loader Job
The Automatic Data Loader can load .xlsx files created with Microsoft Excel version 2007 and above or .zip files into the system from an on-premises installation of APM Connect.
- The file name length is not more than 100 characters.
- The file path of the scan directory is not more than 150 characters from root.
- The file name does not contain any special characters.
- Data loader templates are followed for loading the data in excel files.
GE Digital APM provides a method to automatically load data into the system from correctly formatted .xlsx or a .zip file containing correctly formatted .csv files. You must place your data loader workbook in the correct directory for a successful data load.
The job monitors a configured load directory for the presence of a file in a subdirectory and stages the contents of the file into the system. Multiple files moved into the directory are processed in descending order according to the last modified time stamp on each file.
The system logs the staging progress and archives the files in an archive directory. If data fails to stage or upload, a message is written to the log indicating the reason for failure, and the source files are moved to the FAILED FILES directory.
A service then retrieves the staged workbooks, and, using an administrative account, the service invokes the appropriate data loader to load the data contained in the workbooks.
Set up the Automatic Data Loader Job
Before You Begin
APM Connect must be installed.
Procedure
Results
The job conductor indicates that the job ran successfully, and the automatic data loader directories will be created if they do not already exist.
You can now place workbooks in the appropriate data loader directory.
Configure the Context File
Before You Begin
The context file provides the automatic data loader job with the information it needs to locate the directories and log the file it requires.
You should have imported the automatic data loader job.
Procedure
Use the Automatic Data Loader
Use the Automatic Data Loader job to manually or programmatically load asset data to GE Digital APM.
About This Task
By default, the Automatic Data Loader job processes the files in the directories based on the alphanumeric directory name and then the time stamp of the files from oldest to most recent.
Procedure
- Identify the directory that corresponds to the data loader you are using.
- Move the data loader files (either a correctly formatted .xlsx or a .zip file that contains correctly formatted .csv files) into the identified directory.
The Automatic Data Loader Directories
The automatic data loader job uses directories within the directory identified in the SCAN_DIR parameter to identify the data loader to use for a particular workbook.
Data Loaders and Directories
Data Loader Name | Directory Name |
---|---|
APM Family | FamilyDataLoader |
Asset Criticality Analysis (ACA) | ACAMatrixDataLoader |
Asset Criticality Analysis (ACA Checklist) | ACACheckListDataLoader |
Asset Ingestion Loader | AssetIngestionLoader |
Asset Strategy Management (ASM) | ASMDataLoader |
Asset Strategy Management (ASM) Templates | ASMTemplateDataLoader |
Calibration | CalibrationBatchDataLoader |
Custom Asset Hierarchy | Custom Asset Hierarchy Loader |
Equipment and Functional Location | EquipmentFunctionalLocationLoader |
Failure Modes and Effects Analysis (FMEA) | FMEAAnalysisDataLoader |
Failure Modes and Effects Analysis (FMEA) Analysis Templates | FMEAAnalysisTemplateDataLoader |
Failure Modes and Effects Analysis (FMEA) Asset Templates | FMEAAssetTemplateDataLoader |
Generation Availability Analysis (GAA) Amplification Codes | GAA GADS Amplification Code |
Generation Availability Analysis (GAA) Cause Code | GAA GADS Cause Code |
Generation Availability Analysis (GAA) Events | GAA Events |
GAA Wind Asset Hierarchy | GAA Wind Asset Hierarchy |
GAA Wind Events | GAA Wind Events |
GAA Wind Sub Group Capacity | GAA Wind Sub Group Capacity |
Geographic Information System (GIS) | GISDataLoader |
Hazards | HazardAnalysisBatchDataLoader |
Inspection Management (IM) Assets | ManageInspections |
Inspection Management (IM) Functional Location | ManageInspectionsFL |
Production Loss Analysis (PLA) Admin | PLA Admin Data |
Production Loss Analysis (PLA) Plan | PLA Plan Data |
Production Loss Analysis (PLA) Production Event | Production Event Data |
Reliability Centered Maintenance (RCM) | RCMAnalysisDataLoader |
RCM Analysis Template | RCMAnalysisTemplateDataLoader |
Risk Based Inspection (RBI) 580 | ManageRBI580 |
Risk Based Inspection (RBI) 581 | ManageRBI581 |
Risk Based Inspection (RBI) Corrosion Loop | Load RBI Corrosion Loop |
Risk Matrix | RiskMatrixDataLoader |
Role | RoleDataLoader |
Root Cause Analysis (RCA) | Manage RCA |
Rounds Allowable Values | AllowableValuesBatchDataLoader |
Rounds Readings | ReadingsBatchDataLoader |
Rounds Routes | Rounds Route |
Rounds Templates | TemplateBatchDataLoader |
Tags to Assets Relationship | ManageTagLinks |
Taxonomy | TaxonomyLoader |
Thickness Monitoring (TM) Equipment | ManageTMLGroup |
Thickness Monitoring (TM) Functional Location | ManageTMLGroupFL |
Work History | WorkHistoryLoader |
Policy Instance Data Loader | PolicyInstanceBatchDataLoader |