Reference Information: Query Joins, Functions, and Hyperlinks
About GE Digital APM Inner Joins
When you use two related entity families as query sources, GE Digital APM creates an inner join between the two entity families by default. This inner join causes the query results to include only the records that are linked through the specified relationship.
If two entity families are not related through a relationship family, you can manually create an inner join to connect one or more fields in one family to one or more fields in the other family.
The following table shows the line style that appears in the design canvas to represent GE Digital APM inner joins.
Join Type | Line Style |
---|---|
GE Digital APM Inner Join |
![]() |
Example: Inner Join
Suppose you add the Equipment entity family, Work History entity family, and Has Work History relationship family as query sources. Assuming that the Has Work History family relates the Equipment family to the Work History family, GE Digital APM will create an inner join between the Equipment and Work History families by default. As a result, the query results will return only Equipment records that are linked to a Work History record through the Has Work History relationship. The query results will not include any Equipment records that are not linked to a Work History record or any Work History records that are not linked to an Equipment record.
About GE Digital APM Outer Joins
An outer join allows you to return records that satisfy the join conditions and records from one family for which there are no matching records in the other family.
You can modify the default inner join to manually create an outer join for families that are related through a relationship family.
The following table shows the line styles that appear in the design canvas to represent GE Digital APM outer joins.
Join Type | Line Style |
---|---|
GE Digital APM Outer Left Join |
![]() |
GE Digital APM Outer Right Join |
![]() |
Example 1: Creating a GE Digital APM Outer Join
If you use two unrelated families as query sources, such as the Centrifugal Pump family and the Rotary Pump family, you can create an outer join to view all Centrifugal Pumps and Rotating Pumps whose manufacturer is the same and all Centrifugal Pumps with a different manufacturer. If the Centrifugal Pump family was added as a query source as Table #1 and the Rotary Pump family was added as Table #2, this would create a left join, which would be indicated in the SQL code.
On the other hand, if you wanted to view all Rotary Pumps and Centrifugal Pumps whose manufacturer is the same and all Rotary Pumps with a different manufacturer, you would create a right join, which would be indicated in the SQL code.
Example 2: Creating a GE Digital APM Outer Join
You can modify a relationship-driven inner join to create an outer join. For example, suppose that you use the Centrifugal Pump entity family, the Failure entity family, and the Asset Has Failure relationship family as query sources. If your system is configured such that the Asset Has Failure family relates the Centrifugal Pump family to the Failure family, GE Digital APM would create an inner join between the two entity families automatically.
If you ran the query using the default join, the results would include all Centrifugal Pump records that are linked to a Failure record. If you wanted to modify those results, however, to view all Centrifugal Pumps with their linked Failure records and all Centrifugal Pumps that did not have linked Failure records, you would need to modify the inner join to create an outer join. This would return Centrifugal Pumps with and without linked Failure records, but not Failure records without linked Centrifugal Pump records. For example, you could configure a query to show all the Centrifugal Pump records, where only three are linked to Failure records.
This type of join is considered a left join, as indicated by the following SQL code:
SELECT [Centrifugal Pump].[ASSET_ID_CHR] "Asset ID", [Failure].[EFAIL_ASSETID_CHR] "Failure ID"
FROM [Centrifugal Pump]RIGHT JOIN SUCC [Failure] ON {Asset Has Failure}
You could also decide to return all Failure records with their linked Centrifugal Pump records and all Failure records that do not have linked Centrifugal Pump records.
This type of join is considered a right join, as indicated by the following SQL code:
SELECT [Centrifugal Pump].[ASSET_ID_CHR] "Asset ID", [Failure].[EFAIL_ASSETID_CHR] "Failure ID"
FROM [Centrifugal Pump]RIGHT JOIN SUCC [Failure] ON {Asset Has Failure}
About Manual Joins
In many cases, you will want to query the database for information that exists in more than one family. When you do so, you may also want to join a field in a family with a similar field in another family, which will create an ad hoc association between the two families. By joining a field in one family to a field in another family, you create a query join.
Details
There are two types of manual joins in GE Digital APM:
- Manual Inner Join: Returns a row for every record where the values in the joined fields in both families are equal. An inner join returns only those records that satisfy the join conditions, so any unmatched records are dropped from the result set.
-
Manual Outer Join: Returns a row for every record in one family, and a row for every record where the values in the joined fields in both families are equal. An outer join can be either a left outer join or a right outer join. When you add query sources to the grid in the Conditions section and join their fields, the family that you added first is referred to as Table #1, and the family that you added second is referred to as Table #2.
- A left outer join returns every record in Table #1, regardless of whether each record is linked to a record from Table #2. The results also include the records in Table #2 in which the value in the joined field is equal to that in Table #1.
- A right outer join returns every record in Table #2, regardless of whether each record is linked to a record in Table #1. The results also include the records in Table #1 in which the value in the joined field is equal to that in Table #2.
The following table shows the line styles that appear in the design canvas to represent manual joins.
Join Type | Line Style |
---|---|
Manual Inner Join |
![]() |
Manual Outer Left Join |
![]() |
Manual Outer Right Join |
![]() |
Example: Manual Inner Join
Suppose that you notice that two pieces of equipment, such as a centrifugal pump and an air cooled heat exchanger, have been malfunctioning recently. You suspect that the failures could be caused by human error during installation. You decide to query the database to find instances where these pieces of equipment were installed on the same day by the same person.
To do so, you would need to add the Centrifugal Pump family and the Air Cooled Heat Exchanger family as query sources. You would then need to join the Asset Installation Date fields and the Responsible Installer fields between the two families via an inner join. Doing so would return only records where a centrifugal pump was installed by the same person on the same date as an air cooled heat exchanger.
What is a Function?
A function is a SQL component that manipulates data and returns a value that is not stored in the database, but is derived from calculating or reformatting values. Functions can be used to calculate or reformat values:
- Stored in the database.
- Based on static data (e.g., the current date).
In SQL code, a function can be included as part of the SELECT statement, WHERE clause, the GROUP BY clause, or the HAVING clause, or it can exist outside of these SQL components. You can write functions in the SQL code, or in the Expression Builder.
You can use the following functions in GE Digital APM:
- Aggregate Functions
- Character Functions
- Conversion Functions
- Number/Mathematical Functions
- The DECODE Function
- Date Functions
Example 1: SUM Function Contained within the SELECT Statement
In the following SQL code, the SUM function is displayed in bold text.
SELECT [Asset].[ASSET_ID_CHR] "Asset ID", Sum([Failure].[EFAIL_TOTCST_FROM]) "Total Failure Cost"
FROM [Asset] JOIN SUCC [Failure] ON {Asset Has Failure}
WHERE [Failure].[EFAIL TOTCST FRM] > 50000
GROUP BY [Asset].[ASSET ID CHR]
In this example, the SUM function is contained within the SELECT statement.
Example 2: SUM Function Contained within the SELECT Statement and in the HAVING Clause
In the following SQL code, the SUM function is displayed in bold text and appears twice: once in the SELECT statement and once in the HAVING clause.
SELECT [Asset].[ASSET_ID_CHR] "Asset ID", Sum([Failure].[EFAIL_TOTCST_FROM]) "Total Failure Cost"
FROM [Asset] JOIN SUCC [Failure] ON {Asset Has Failure}
GROUP BY [Asset].[ASSET ID CHR]
HAVING Sum([Failure].[EFAIL TOTCST FROM]) > 5000
About the GROUP BY Clause
A GROUP BY clause is used to group query results.
The GROUP BY Clause
Suppose that you want to see the total number of failures your equipment has experienced per equipment manufacturer.
You would add the Asset Manufacturer field and the Failure ID field to the grid in the Conditions section. The Total row indicates that you want to group the results by manufacturer and display a total count of failures for each manufacturer that is returned. The sort preference indicates that you want to sort the results in descending order according to the failure count.
In the results, each row represents a different manufacturer and the total count of failures for each manufacturer that is returned.
In this example, the query results are grouped by one field only, so each manufacturer appears only one time. You can, however, group query results by more than one field. When you group a query by multiple rows, the query determines all possible combinations of results and returns each distinct combination. Therefore, the more fields you group by, the more results you will see.
Continuing with this example, if you add the Asset ID field to the query, the results will contain many more rows because there are more combinations to display. In this case, one manufacturer may be displayed twice if that manufacturer manufactures multiple equipment items.
About Aggregate and Analytic Functions
Aggregate functions perform a calculation on a set of values and return a single value. Analytic functions compute an aggregate value based on a set of values, and, unlike aggregate functions, can return multiple rows for each set of values. Throughout this documentation, we refer to queries that contain aggregate functions as aggregate queries, and queries that contain analytic functions as analytic queries.
If you want to run a query using only aggregate functions, the query will return one row with a column for each field. If you want to run a query using an aggregate function in conjunction with the GROUP BY clause, the query will return one row for each value found in the grouped field.
Aggregate functions are used in conjunction with the GROUP BY clause, which specifies how the query results will be grouped and displayed. In other words, if you use any aggregate functions on fields in a query, then all remaining fields must appear in the GROUP BY clause.
Aggregate functions and analytic functions can be selected in the Total cell of the grid in the Conditions section.
Analytic functions compute an aggregate value based on a set of values, and, unlike aggregate functions, can return multiple rows for each set of values. Use analytic functions to compute moving averages, running totals, percentages, or top-N results within a group.
If you want to run a query using an analytic function, the query will return one row for each field in the defined range of fields used to perform the calculations.
Analytic Function | Format of Code Using the Function |
---|---|
AVG | AVG(field) OVER([PARTITION BY field1[, field2, ...]] ORDER BY field1[, field2, ...]) |
CUME_DIST | CUME_DIST() OVER([PARTITION BY field1[, field2, ...]] ORDER BYfield1[, field2, ...]) |
FIRST_VALUE | FIRST_VALUE(field) OVER([PARTITION BY field1[,field2, ...]] ORDER BY field1[, field2, ...]) |
LAST_VALUE | LAST_VALUE(field) OVER([PARTITION BY field1[,field2, ...]] ORDER BY field1[, field2, ...]) |
MAX | MAX(field) OVER([PARTITION BY field1[,field2, ...]] ORDER BY field1[, field2, ...]) |
MIN | MIN(field) OVER([PARTITION BY field1[, field2, ...]] ORDER BY field1[, field2, ...]) |
NTILE | NTILE(number) OVER([PARTITION BY field1[,field2, ...]] ORDER BY field1[, field2, ...]) |
ROW | ROW_NUMBER() OVER([PARTITION BYfield1[, field2, ...]] ORDER BY field1[, field2, ...]) |
SUM | SUM(field) OVER([PARTITION BY field1[,field2, ...]] ORDER BY field1[,field2, ...]) |
About Character Functions
Example: REPLACE Function
Suppose that you want to view the Failure ID of the failure associated with each piece of equipment or location in your database. Failure IDs are stored with a dash in the syntax, and you want to display them with a double colon instead of the dash.
In this case, you might configure a query on the Asset and Failure families, joined via the Asset Has Failure relationship, and add the Asset ID and Failure ID fields to the query.
In this example, to return the Failure IDs and replace the dash with a double colon, you would configure an expression using the REPLACE function. You would also configure the alias to ensure that the column displays the text Failure ID.
In this case, the expression syntax is:
REPLACE([Failure].[Failure ID], '-', '::')
The syntax indicates that you want to replace the dash (-) with a double colon (::).
More Examples of Character Functions
Function | Description | Example | Stored Value | Result |
---|---|---|---|---|
CONCAT | Concatenates two field values and displays the result. | CONCAT ([Asset)ID], [Asset Type]) |
Asset ID: T-101 Asset Type: Tank | T-101Tank |
& | Concatenates two or more field values and adds delimiters between the values. | [Asset ID] &':' & [Asset Type] |
Asset ID: T-101 Asset Type: Tank | T-101:Tank |
LOWER | Displays the value in all lowercase letters. | LOWER ([Asset Type]) | Tank | Tank |
UPPER | Displays the value in all uppercase letters. | UPPER ([Asset Type]) | Tank | Tank |
SUBSTR | Displays a specific number of characters depending on the starting point you specify and the number of characters that you specify should be returned. |
SUBSTR ([Asset ID],0,3) Zero (0) specifies the starting point (from left to right) and three (3) specifies the number of characters after the starting point that you want to display. | PMP-101 | PMP |
IsNull | Displays a specified value when a null value is found. | IsNull ([Asset Type],'No Value Listed') | Asset Type field contains a null value | No Value Listed |
LTRIM | Displays the value with the specified characters removed from the beginning (left) of the string. | LTRIM ([PhoneNumber], '(540)-') | (540) 344-9205 | 344-9205 |
RTRIM | Displays the value with the specified characters removed from the end (right) of the string. | RTRIM ([Failure ID], '-0123456789') | FAIL-1234 | FAIL |
About Conversion Functions
A Conversion function is used to modify query results by reformatting the data. You can use this type of function if you want to reformat the data to simplify it (e.g., you could remove unnecessary zeros from dates, where 01/07/2007 could be converted to 1/7/2007) or if you want to reformat the data so it appears as a different data type completely (e.g., you could spell out a month instead of representing the month with a number, where 01/07/2007 could be converted to January 7, 2007).
Description | Function |
---|---|
Convert a number or date to a character | CastChar |
Convert a character to a date | CastDate |
Convert a character to a number | CastNum |
About Date Functions
Example: MI_DateAdd
You might configure a query on the Air Cooled Heat Exchanger family, and add the Asset ID, Asset Description, Asset Inspection Date, and Next Inspection Date fields to the query.
In this example, to return the next inspection date, you would configure an expression using the MI DateAdd function. You would also configure the alias of this column to indicate that the column returns the next inspection date.
The expression syntax is:
MI DateAdd('mm', 6, [Air Cooled Heat Exchanger].[Asset Inspection Date])
The following table lists more examples of how you can use the MI DateAdd function.
Parameter | Example | Description | Stored Value | Result |
---|---|---|---|---|
yy | MI DateAdd(' yy ', 1, [Air Cooled Heat Exchanger].[Asset Installation Date]) | Adds one year to the date on the Asset Installation Date field in Air Cooled Heat Exchanger records. | 11/01/2009 | 11/01/2010 |
mm | MI DateAdd(' mm ', 6, [Air Cooled Heat Exchanger].[Asset Installation Date]) | Add six months to the date on the Asset Installation Date field in Air Cooled Heat Exchanger records. | 11/01/2009 | 05/01/2010 |
dd | MI DateAdd(' dd ', 4, [Air Cooled Heat Exchanger].[Asset Installation Date]) | Adds four days to the date on the Asset Installation Date field in Air Cooled Heat Exchanger records. | 11/01/2009 | 11/05/2009 |
hh | MI DateAdd(' hh ', 4, [Air Cooled Heat Exchanger].[Asset Installation Date]) | Adds four hours to the date on the Asset Installation Date field in Air Cooled Heat Exchanger records. | 11/01/2009 4:00:00 | 11/01/2009 8:00:00 |
mi | MI DateAdd(' mi ', 4, [Air Cooled Heat Exchanger].[Asset Installation Date]) | Adds four minutes to the date on the Asset Installation Date field in Air Cooled Heat Exchanger records. | 11/01/2009 4:00:00 | 11/01/2009 4:04:00 |
mi | MI DateAdd(' mi ', -4, [Air Cooled Heat Exchanger].[Asset Installation Date]) | Subtracts four minutes from the date on the Asset Installation Date field in Air Cooled Heat Exchanger records. | 11/01/2009 4:00:00 | 11/01/2009 3:56:00 |
ss | MI DateAdd(' ss ', 4, [Air Cooled Heat Exchanger].[Asset Installation Date]) | Adds four seconds to the date on the Asset Installation Date field in Air Cooled Heat Exchanger records. | 11/01/2009 4:00:00 | 11/01/2009 4:00:04 |
Example: MI_DatePart
Suppose that you want to view only the month in which the shell and tube heat exchangers were installed in your facility. If all Shell and Tube Heat Exchanger records in your database contain an Asset Installation Date field, and the values are stored in the format mm/dd/yyyy, you could do so using the MI DatePart function.
You might configure a query on the Shell and Tube Heat Exchanger family, and add the Asset ID, Asset Description, and Installation Month fields to the query.
In this example, to return the month in which each shell and tube heat exchanger was installed, you would configure an expression using the MI DatePart function. You would also configure the alias to indicate that the column returns the year the piece of equipment was installed.
The expression syntax is:
MI DatePart('mm', [Shell and Tube Heat Exchanger].[Asset Installation Date])
Using this syntax, instead of displaying the installation date in the stored format of mm/dd/yyyy, the query results will display only the value representing the month.
The following table lists more examples of how you can use the MI DatePart function.
Parameter | Example | Description | Stored Value | Result |
---|---|---|---|---|
yy | MI DatePart('yy', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | Displays only the year from a stored date value. | 11/01/2009 | 2009 |
yyyy | MI DatePart('yyyy', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | |||
year | MI DatePart('year', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | |||
q | MI DatePart('q', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | Displays a number representing the quarter of the year based on a stored date value. | 11/01/2009 | 4 |
MI DatePart('qq', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | ||||
quarter | MI DatePart('quarter', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | |||
m | MI DatePart('m', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | Displays only the month from a stored date value. | 11/01/2009 | 11 |
mm | MI DatePart('mm', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | |||
month | MI DatePart('month', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | |||
wk | MI DatePart('wk', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | Displays a number representing the week of the month based on a stored date value. | 11/01/2009 | 1 |
weekofmonth | MI DatePart('weekofmonth', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | |||
d | MI DatePart('d', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | Displays only the day from a stored date value. | 11/01/2009 | 01 |
dd | MI DatePart('dd', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | |||
day | MI DatePart('day', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | |||
dw | MI DatePart('dw', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | Displays a number representing the day of the week based on a stored date value (where 1 = Sunday, 2 = Monday, etc.). | 11/01/2009 | 1 |
weekday | MI DatePart('weekday', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | |||
y | MI DatePart('y', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | Displays a number representing the day of the year based on a stored date value. | 11/01/2009 | 305 |
dy | MI DatePart('dy', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | |||
dayofyear | MI DatePart('dayofyear', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | |||
hh | MI DatePart('hh', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | Displays only the hour from a stored date value. | 11/01/2009 4:00:00 | 4 |
hour | MI DatePart('hour', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | |||
n | MI DatePart('n', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | Displays only the minutes from a stored date value. | 11/01/2009 4:00:00 | 00 |
mi | MI DatePart('mi', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | |||
minute | MI DatePart('minute', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | |||
s | MI DatePart('s', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | Displays only the seconds from a stored date value. | 11/01/2009 4:00:00 | 00 |
ss | MI DatePart('ss', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | |||
second | MI DatePart('second', [Shell and Tube Heat Exchanger].[Asset Installation Date]) |
Example: NOW
Suppose that you want to see the tasks that are assigned to a specific user and due in the next thirty days. If Task records contain the Next Date field that stores the date on which the task is due, you could do so using the NOW function.
You might configure a query on the Task family, and add the Task ID, Next Date, and Task Assigned To fields to the query.
In this example, you would configure an expression on the Next Date field using the NOW function. Additionally, you would configure a prompt to prompt the user for the name of the user whose Task records you want to view.
The expression syntax is:
(>= Now() AND <= (Now() + 30))
The syntax indicates that you want to view the tasks that are due today and within the next thirty days. For example, if a task is due thirty-one days after today's date, it will not appear in the query results.
The following table lists more examples of how you can use the NOW function.
Example Expression | Description | Current Date | Result |
---|---|---|---|
NOW(0) or NOW() | Displays the current date. | 11/01/2009 | 11/01/2009 |
NOW() - 3 | Displays the date that is three days prior to the current date. | 11/01/2009 | 10/29/2009 |
NOW() + 3 | Displays the date that is three days later than the current date. | 11/01/2009 | 11/04/2009 |
Example: LastDate
Suppose that you want to see all the air cooled heat exchanger failures in your facility that occurred in a given month. If each Air Cooled Heat Exchanger record is linked to a Failure record, and each Failure record contains the Failure Date/Time field that stores that date and time on which a failure occurred, you could do so using the LAST DATE function.
You might configure a query on the Air Cooled Heat Exchanger and Failure families, joined via the Asset Has Failure relationship, and add the Asset ID, Failure ID, Failure Date/Time, and Last Day fields to the query.
In this example, you would configure an expression using the LAST DATE function. Additionally, you would create a prompt that prompts you to select the last day of the month whose failures you want to view. You would configure the alias to indicate that the column displays the last day of the month.
The expression syntax is:
LastDate([Failure].[Failure Date/Time])
The prompt syntax is:
((? :d :caption='Last Day' :id=Last Day))
When you run the query, a prompt appears, where you can select 11/30/2009 12:00:00 A.M. to indicate that you want to view failures that occurred during the month of November.
Example: ISNULL
Suppose that you want to see the installation date of the shell and tube heat exchangers in your facility even if the Asset Installation Date field in the Shell and Tube Heat Exchanger records is empty, and if the Asset Installation Date field is empty, you want to show the value Not Installed.
In this case, you might configure a query on the Shell and Tube Heat Exchanger family, and add the Asset ID, Asset Description, and Installation Dates (ALL) fields to the query.
In this example, you would configure an expression using the ISNULL function. You would also configure the alias to indicate that the column returns the installation dates.
In this case, the expression syntax is:
IsNull([Shell and Tube Heat Exchanger].[Asset Installation Date], 'Not Installed')
...where Not Installed is the value that will appear where a null value is found on the Asset Installation Date field in the Shell and Tube Heat Exchanger records.
Example: ROUND
Suppose that you want to see the values on the As Left fields for the analyzer instruments in your facility rounded to two decimal places. If all Analyzer Calibration records contain the As Left field, you can do so using the ROUND function.
You might configure a query on the Analyzer Calibration family, and add the Analyzer ID, Calibration Date, and As Left (rounded) fields to the query.
In this example, you would configure an expression using the ROUND function. You would also configure the alias to indicate that the column displays the rounded as left values.
The expression syntax is:
ROUND([Analyzer Calibration].[As Left], '2')
...where 2 is the number of decimal places to which the values will be rounded in the results.
Example: DATENAME
Suppose that you want to see the name of the month in which the shell and tube heat exchangers were installed. Instead of 11, you want to see November, and you do not want to return the year or day in the query results. If all Shell and Tube Heat Exchanger records in your database contain an Asset Installation Date field, and the values are stored in the format mm/dd/yyyy (e.g., 11/01/2009), you could do so using the DATENAME function.
You might configure a query on the Shell and Tube Heat Exchanger family, and add the Asset ID, Asset Description, and Installed by Month fields to the query.
In this example, you would configure an expression using the DATENAME function. You would also configure the alias to indicate that the results display the month.
The expression syntax is:
DATENAME('mm', [Shell and Tube Heat Exchanger].[Asset Installation Date])
...where mm
indicates the part of the date (i.e., month) that you want to convert to its character format.
The following table lists more examples of how you can use the DATENAME function.
Parameter | Description | Example | Stored Value | Result |
---|---|---|---|---|
yy year | Displays a number representing the year from a stored date value. | DATENAME('year', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | 11/01/2009 | 2009 |
quarter | Displays a number representing the quarter of the year based on a stored date value. | DATENAME('qq', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | 11/01/2009 | 4 |
mm month | Displays the month from a stored date value. | DATENAME('mm', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | 11/01/2009 | November |
ww | Displays a number representing the week of the month based on a stored date value. | DATENAME('ww', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | 11/01/2009 | 1 |
dd day | Displays a number representing the day from a stored date value. | DATENAME('day', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | 11/01/2009 | 01 |
dw | Displays the day of the week based on a stored date value. | DATENAME('dw', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | 11/01/2009 | Sunday |
dy dayofyear | Displays a number representing the day of the year based on a stored date value. | DATENAME('dayofyear', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | 11/01/2009 | 305 |
Example: DATEPART
Suppose that you want to see the year in which the shell and tube heat exchangers were installed in your facility. If all Shell and Tube Heat Exchanger records in your database contain an Asset Installation Date field, and the values are stored in the format mm/dd/yyyy (e.g., 11/01/2009), you could do so using the DATEPART function.
You might configure a query on the Shell and Tube Heat Exchanger family, and add the Asset ID, Asset Description, and Installation Year fields to the query.
In this example, you would configure an expression using the DATEPART function. You would also configure the alias to indicate that the column displays the installation year.
The expression syntax is:
DATEPART('year', [Shell and Tube Heat Exchanger].[Asset Installation Date])
...where year
is the portion of the date value that you want to view.
Parameter | Example | Description | Stored Value | Result |
---|---|---|---|---|
yy | DATEPART('yy', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | Displays a number representing the year from a stored date value. | 11/01/2009 | 2009 |
yyyy | DATEPART('yy', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | |||
year | DATEPART('year', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | |||
q | DATEPART('q', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | Displays a number representing the quarter of the year based on a stored date value. | 11/01/2009 | 4 |
DATEPART('qq', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | ||||
quarter | DATEPART('quarter', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | |||
m | DATEPART('m', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | Displays a number representing the month from a stored date value. | 11/01/2009 | 11 |
mm | DATEPART('mm', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | |||
month | DATEPART('month', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | |||
wk | DATEPART('wk', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | Displays a number representing the week of the month based on a stored date value. | 11/01/2009 | 1 |
ww | DATEPART('ww', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | |||
week | DATEPART('week', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | |||
d | DATEPART('d', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | Displays a number representing the day from a stored date value. | 11/01/2009 | 1 |
dd | DATEPART('dd', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | |||
day | DATEPART('day', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | |||
dw | DATEPART('dw', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | Displays a number representing the day of the week based on a stored date value. | 11/01/2009 | 1 (i.e., Sunday) |
weekday | DATEPART('weekday', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | |||
y | DATEPART('y', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | Displays a number representing the day of the year based on a stored date value. | 11/01/2009 | 305 |
dy | DATEPART('dy', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | |||
dayofyear | DATEPART('dayofyear', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | |||
hh | DATEPART ('hh', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | Displays only the hour from a stored date value. | 11/01/2009 4:00:00 | 4 |
hour | DATEPART ('hour', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | |||
n | DATEPART ('n', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | Displays only the minutes from a stored date value. | 11/01/2009 4:00:00 | 00 |
mi | DATEPART ('mi', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | |||
minute | DATEPART ('minute', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | |||
s | DATEPART ('s', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | Displays only the seconds from a stored date value. | 11/01/2009 4:00:00 | 00 |
ss | DATEPART ('ss', [Shell and Tube Heat Exchanger].[Asset Installation Date]) | |||
second | DATEPART ('second', [Shell and Tube Heat Exchanger].[Asset Installation Date]) |
About Number/Mathematical Functions
About the DECODE Function
A DECODE function is used to evaluate a value in the query results and, based on that evaluation, trigger an action or return a different value.
Example: DECODE Function
Suppose that, in your organization, you have open and closed work history events. Each Work History record contains an Order System Status field, which is used to record the status of that work history event. You want to see how many open work history events you have and how many closed work history events you have. Instead of the stored values of CLSD TECO or OPEN, however, you want to see the values Closed or Open in your query results.
In addition, you are concerned that not all Work History records contain a value in the Order System Status field. You also want to see in your query results which records do not have a value in this field so that you can update those records.
In this case, you might configure a query on the Work History family, and then add the Expr and Order System Status fields to the query.
In this example, to return the status of each work history event as Closed, Open, or No Status (meaning that the record does not contain a value in the Order System Status field), you can configure an expression using the DECODE function.
In this case, the expression syntax is:
Decode([Work History].[Order System Status], 'CLSD TECO', 'Closed', 'OPEN', 'Open', 'No Status')
This syntax indicates that for Work History records that contain the value CLSD TECO in the Order System Status field, you want to return the value Closed. For those records with the value OPEN in the Order System Status field, you want to return the value Open. For records where the Order System Status field is empty, you want to return the value No Status.
You would also add a COUNT function on the Order System Status field so that you can see the number of work history events that fall into each category.
Other possible uses include:
- You want to review the types of maintenance activities that are being performed in your plant and the total number of failures that resulted in each type of activity. Users can enter any value they choose into a field that tracks maintenance activities, so you know that your users are using different terminology to mean the same thing. For example, to indicate that they replaced broken components, different users might enter replace, replacing, or replacement. You can write a DECODE statement to indicate that the values replace, replacing, and replacement should return the value Replace in the query results.
- Members of management want to investigate failures that resulted in a failure cost of $50,000 or more. You can write a DECODE statement to indicate that failures with a failure cost greater than or equal to $50,000 should return the value Please Investigate in the query results. Other failures should return the value OK in the query results.
MetaSQL Functions
Aggregate Functions
- AVG
- COUNT
- MAX
- MIN
- SUM
Meridium Functions
Meridium functions are supported regardless of what database management system you use. The MetaSQL compiler will automatically convert the expression to a native SQL expression.
<meridium_function> ::=
{
function_id ( [ { <expression> [,...n] } | * ] )
}
...where function_id is the name of the function you are executing. - UserKey
- Gets the key of the current logged-in user.
SELECT UserKey() FROM <source>
- Str
- Converts the designated field to a VARCHAR value.
-- Syntax SELECT Str(<expression> [, <size>]) "Expr" FROM <source> -- Simple Example SELECT [MI_ACTION].ENTY_KEY "ENTY_KEY" , Str([MI_ACTION].ENTY_KEY) "Str Enty Key" FROM [MI_ACTION] -- Specify the size SELECT [MI_ACTION].ENTY_KEY "ENTY_KEY" , Str([MI_ACTION].ENTY_KEY, 20) "Str Enty Key" FROM [MI_ACTION]
- IsNull
- Evaluates an expression. If the value is null, evaluates the expression in the second argument and returns its result.Note: Both arguments must return the same data type.
-- Syntax SELECT IsNull(<expression>, <expression>) "Expr" FROM <source> -- Example (Note the conversion of number to string ensuring consistent data types) SELECT [MI_ACTION].[MI_ACTION_ID_C] "Action ID" , [MI_ACTION].[MI_ACTION_SHORT_DESC_C] "Name" , IsNull(Str([MI_ACTION].[MI_ACTION_RESOURCE_COST_N]), 'No Cost Data') "Cost" FROM [MI_ACTION]
- Now
- Returns the DBMS system date.
-- Syntax SELECT Now() FROM <source>
- LocalizedCaption
- Returns a localized Family Caption for a given Family Key and User Key.
-- Syntax SELECT LocalizedCaption(<family_key>, <user_key>) FROM <source> -- Example SELECT mi_families.FMLY_CAPTION_TX "Caption" , LocalizedCaption(mi_families.FMLY_KEY, 64251708261) "Localized Caption" FROM mi_families
- Decode
- Returns a given output based on one or more possible inputs.
-- Syntax SELECT DECODE(<field_id>, <input_value>, <output_value> [ , <input_value>, <output_value> ], <default_value> ) FROM <source> -- Example SELECT [MI_ACTION].[MI_ACTION_ID_C] "Action ID" , [MI_ACTION].[MI_ACTION_SHORT_DESC_C] "Name" , [MI_ACTION].[MI_ACTION_RESOURCE_COST_N] "Cost" , Decode([MI_ACTION].[MI_ACTION_RESOURCE_COST_N], 100, 'Cheap', 10000, 'Moderately Expensive', 100000, 'Expensive', 'Misc') "Cost Category" FROM [MI_ACTION] ORDER BY "Cost" Desc
- DatePart
- Returns the specified part of a date/time value. DatePart and MI_DatePart are equivalent. The return is a number.
The date_part can contain any of the following values:--Syntax SELECT DatePart( <date_part>, <expression> ) FROM <source> -- Example SELECT [MI_ACTION].[MI_ACTION_ID_C] "Action ID" , [MI_ACTION].[MI_ACTION_SHORT_DESC_C] "Name" , [MI_ACTION].[MI_ACTION_TARGE_COMPL_DATE_CHR] "Target Completion Date" , DatePart('yy', [MI_ACTION].[MI_ACTION_TARGE_COMPL_DATE_CHR]) "Year" , DatePart('mm', [MI_ACTION].[MI_ACTION_TARGE_COMPL_DATE_CHR]) "Month" , DatePart('dd', [MI_ACTION].[MI_ACTION_TARGE_COMPL_DATE_CHR]) "Day" , DatePart('hh', [MI_ACTION].[MI_ACTION_TARGE_COMPL_DATE_CHR]) "Hour" , DatePart('mi', [MI_ACTION].[MI_ACTION_TARGE_COMPL_DATE_CHR]) "Minute" , DatePart('ss', [MI_ACTION].[MI_ACTION_TARGE_COMPL_DATE_CHR]) "Second" , DatePart('dw', [MI_ACTION].[MI_ACTION_TARGE_COMPL_DATE_CHR]) "Day of the week" , DatePart('qq', [MI_ACTION].[MI_ACTION_TARGE_COMPL_DATE_CHR]) "Quarter" , DatePart('dy', [MI_ACTION].[MI_ACTION_TARGE_COMPL_DATE_CHR]) "Day of the year" , DatePart('ww', [MI_ACTION].[MI_ACTION_TARGE_COMPL_DATE_CHR]) "Week" FROM [MI_ACTION] WHERE [MI_ACTION].[MI_ACTION_TARGE_COMPL_DATE_CHR] IS NOT NULL
- ‘quarter’, ‘qq’, ‘q’ - Quarter of the year, 1 - 4
- ‘year’, ‘yyyy’, ‘yy’ - Year, 4 digits (always)
- ‘month’, ‘mm’, ‘m’ - Month of the year, 1 - 12
- ‘day’, ‘dd’, ‘d’ - Day of the month, 1 - 31
- ‘hour’, ‘hh’, ‘h’ - Hour of the day, 0 - 23
- ‘minute’,’mi’, ‘n’ - Minute of the hour, 0 - 59
- ‘second’, ‘ss’, ‘s’ - Second of the minute, 0 - 59
- ‘dayofyear’, ‘dy’, ‘y’ - Day of the year
- ‘dayofweek’, ‘weekday’, ‘dw’ - Day of the week, 1 - 7, Sunday is 1
- ‘weekofyear’, ‘week’, ‘ww’ - Week of the year
- ‘weekofmonth’, ‘wk’ - Week of month
- DateAdd
- Adds the specified number of units to a given date/time and returns a new date/time value. DateAdd and MI_DateAdd are equivalent. On Oracle databases, adding years and months is not supported.
The date_part can contain one of the following values:-- Syntax SELECT DateAdd( <date_part>, <num_const>, <expression> ) FROM <source> -- Example SELECT [MI_ACTION].[MI_ACTION_ID_C] "Action ID" , [MI_ACTION].[MI_ACTION_SHORT_DESC_C] "Name" , [MI_ACTION].[MI_ACTION_TARGE_COMPL_DATE_CHR] "Target Completion Date" , DateAdd('yy', 10, [MI_ACTION].[MI_ACTION_TARGE_COMPL_DATE_CHR]) "Add 10 Years" , DateAdd('mm', 10, [MI_ACTION].[MI_ACTION_TARGE_COMPL_DATE_CHR]) "Add 10 Months" , DateAdd('dd', 10, [MI_ACTION].[MI_ACTION_TARGE_COMPL_DATE_CHR]) "Add 10 Days" , DateAdd('hh', 10, [MI_ACTION].[MI_ACTION_TARGE_COMPL_DATE_CHR]) "Add 10 Hours" , DateAdd('mi', 10, [MI_ACTION].[MI_ACTION_TARGE_COMPL_DATE_CHR]) "Add 10 Minutes" , DateAdd('ss', 10, [MI_ACTION].[MI_ACTION_TARGE_COMPL_DATE_CHR]) "Add 10 Seconds" FROM [MI_ACTION] WHERE [MI_ACTION].[MI_ACTION_TARGE_COMPL_DATE_CHR] IS NOT NULL
- ‘year’, ‘yyyy’, ‘yy’ - Year
- ‘month’, ‘mm’, ‘m’ - Month
- ‘day’, ‘dd’, ‘d’ - Day
- ‘hh’, ‘h’ - Hour
- ‘minute’, ‘mi’, ‘n’ - Minute
- ‘second’, ‘ss’, ‘s’ - Second
- DateFormat
- Returns a date/time value formatted as a string.
The date_format can contain any reasonable combination of the following values:--Syntax SELECT DateFormat( <date_format>, <expression> ) FROM <source> -- Example SELECT [MI_ACTION].[MI_ACTION_ID_C] "Action ID" , [MI_ACTION].[MI_ACTION_SHORT_DESC_C] "Name" , [MI_ACTION].[MI_ACTION_TARGE_COMPL_DATE_CHR] "Target Completion Date" , DateFormat('yyyy-mm-dd', [MI_ACTION].[MI_ACTION_TARGE_COMPL_DATE_CHR]) "Date" FROM [MI_ACTION] WHERE [MI_ACTION].[MI_ACTION_TARGE_COMPL_DATE_CHR] IS NOT NULL
- ‘yyyy’ - four digit year
- ‘yyy’ - last 3 digits of the year
- ‘yy’ - last 2 digits of the year
- ‘y’ - last digit of the year
- ‘mm’ - month of the year, 01 - 12
- ‘mon’ - abbrreviated month name
- ‘dd’ - Day of the month, 01 - 31
- ‘ddd’ - Day of the year, 001 - 366
- ‘d’ - Day of the week, 1 - 7, Sunday is 1
- ‘dy’ - abbrreviated day name
- ‘hh’ - Hour of the day, 01 - 12
- ‘hh12’ - Hour of the day, 01 - 12
- ‘hh24’ - Hour of the day, 00 - 23
- ‘mi’ - Minute of the hour, 00 - 59
- ‘ss’ - Second of the minute, 00 - 59
- ‘ms’ - Millisecond, 000 - 999
- ‘am’ - (or pm) meridiem indicator
Note:- Oracle does not support fractional seconds.
- Microsoft does not support day of the year.
- DateName
- Returns the month or day name for date/time value. Note that this value will not be localized.
The date_format can contain any of the following values:--Syntax SELECT DateName( <date_format>, <expression> ) FROM <source> -- Example SELECT [MI_ACTION].[MI_ACTION_ID_C] "Action ID" , [MI_ACTION].[MI_ACTION_SHORT_DESC_C] "Name" , [MI_ACTION].[MI_ACTION_TARGE_COMPL_DATE_CHR] "Target Completion Date" , DateFormat('day', [MI_ACTION].[MI_ACTION_TARGE_COMPL_DATE_CHR]) "Day" FROM [MI_ACTION] WHERE [MI_ACTION].[MI_ACTION_TARGE_COMPL_DATE_CHR] IS NOT NULL
- ‘month’, ‘mm’, ‘m’ - Month of the year
- ‘day’, ‘dd’, ‘weekday’, ‘dw’ - Day of the week
- UTC
- Returns the formatted string equivalent of the argument date/time value. The return will be formatted ‘yyyy-mm-dd hh:mi:ss’.
--Syntax SELECT UTC(<expression> ) FROM <source> -- Example SELECT [MI_ACTION].[MI_ACTION_ID_C] "Action ID" , [MI_ACTION].[MI_ACTION_TARGE_COMPL_DATE_CHR] "Target Completion Date" , UTC([MI_ACTION].[MI_ACTION_TARGE_COMPL_DATE_CHR]) "UTC Date" FROM [MI_ACTION] WHERE [MI_ACTION].[MI_ACTION_TARGE_COMPL_DATE_CHR] IS NOT NULL
- DateDiff
- Returns the difference between to date/time values as number. The argument determines the unit of measure returned. The expression1 argument is subtracted from expression2.
The date_PART can contain any of the following values:--Syntax SELECT DateDiff( <date_part>, <expression1>, <expression2>) FROM <source> -- Example SELECT [MI_ACTION].[MI_ACTION_ID_C] "Action ID" , [MI_ACTION].[MI_ACTION_SHORT_DESC_C] "Name" , [MI_ACTION].[MI_ACTION_TARGE_COMPL_DATE_CHR] "Target Completion Date" , DateDiff('day', [MI_ACTION].[MI_ACTION_TARGE_COMPL_DATE_CHR], [MI_ACTION].LAST_UPDT_DT) "Days" FROM [MI_ACTION] WHERE [MI_ACTION].[MI_ACTION_TARGE_COMPL_DATE_CHR] IS NOT NULL
- ‘day’, ‘dd’, ‘d’ - Days
- ‘hour’, ‘hh’, ‘h’ - Hours
- ‘minute’, ‘mi’, ‘n’ - Minutes
- ‘second’, ‘ss’, ‘s’ - Seconds
- Length
- Returns the length of the specified expression.
-- Syntax SELECT Length( <expression> ) FROM <source> -- Example , [MI_ACTION].[MI_ACTION_SHORT_DESC_C] "Name" , Length([MI_ACTION].[MI_ACTION_SHORT_DESC_C]) "Name Length" , [MI_ACTION].[MI_ACTION_TARGE_COMPL_DATE_CHR] "Target Completion Date" , Str([MI_ACTION].[MI_ACTION_TARGE_COMPL_DATE_CHR]) "Target Completion Date String" , Length(Str([MI_ACTION].[MI_ACTION_TARGE_COMPL_DATE_CHR])) "Target Completion Date Length" , (1000000 + 2689432) "Test" , Length((1000000 + 2689432)) "Test Length" FROM [MI_ACTION]
Note: When determining string length of a Date/Time value, the results may not be as expected. To ensure predictable results, cast the Date/Time to a string with a known format prior to passing it into the Length() function. - CastChar, CastNu,, CastDate
- Takes an expression and attempts to return a value cast to the desired type.
-- Syntax SELECT CastChar(<expression>, <size>) FROM <source> SELECT CastNum(<expression>) FROM <source> SELECT CastDate(<expression>, <date_format_string>) FROM <source> -- Example SELECT TOP 1 CastChar(Now()) "Now string" , CastChar(1234567, 7) "Number string" , CastNum('1234567') "Number from string" , CastDate('2009-01-01', 'YYYY-MM-DD') "Date from string" FROM [MI_ACTION]
The size accepts a <num_const> representing the size of the VARCHAR.
The date_format_string is a format string for the date/time value (i.e. YYYY-MM-DD). This string format needs to be compatible with the underlying DBMS.
- IndexOf
- Returns the index (1-based) of a given character expression within another character expression.Note: This function is case-sensitive for Oracle and PostgreSQL, but case-insensitive for SQL.
-- Syntax SELECT IndexOf( <char_const_to_search>, <char_const_to_find> [, <start_position>] ) FROM <source> -- Example SELECT [MI_ACTION].[MI_ACTION_ID_C] "Action ID" , [MI_ACTION].[MI_ACTION_SHORT_DESC_C] "Name" , INDEXOF([MI_ACTION].[MI_ACTION_SHORT_DESC_C], 'c') "Index of C" FROM [MI_ACTION]
- Modulus
- Returns the modulus (remainder) of exp1 divided by exp2.
-- Syntax SELECT Modulus( <exp1>, <exp2>) FROM <source>
- Substring
-
-- Syntax SELECT Substring( <expression>, <start_pos> [, <end_pos>] ) FROM <source> -- Example SELECT [MI_ACTION].[MI_ACTION_ID_C] "Action ID" , [MI_ACTION].[MI_ACTION_SHORT_DESC_C] "Name" , Substring([MI_ACTION].[MI_ACTION_SHORT_DESC_C], 2) "Name substring from pos 2" , Substring([MI_ACTION].[MI_ACTION_SHORT_DESC_C], 2, 6) "Name substring from pos 2-6" FROM [MI_ACTION]
- Upper, Lower
- Return the argument string expression in upper or lower case.
-- Syntax SELECT Upper(<expression>) FROM <source> SELECT Lower(<expression>) FROM <source> -- Example SELECT [MI_ACTION].[MI_ACTION_ID_C] "Action ID" , [MI_ACTION].[MI_ACTION_SHORT_DESC_C] "Name" , Upper([MI_ACTION].[MI_ACTION_SHORT_DESC_C]) "Upper" , Lower([MI_ACTION].[MI_ACTION_SHORT_DESC_C]) "Lower" FROM [MI_ACTION]
- LTrim, RTrim, Trim
- Return a character expression after removing the leading or trailing white space (or both, for Trim).
-- Syntax SELECT LTrim(<expression>) FROM <source> SELECT RTrim(<expression>) FROM <source> -- Example SELECT [MI_ACTION].[MI_ACTION_ID_C] "Action ID" , [MI_ACTION].[MI_ACTION_SHORT_DESC_C] "Name" , ('----|' & ' ' & [MI_ACTION].[MI_ACTION_SHORT_DESC_C] & ' ' & '|----') "Untrimmed Name" , ('----|' & LTRIM((' ' & [MI_ACTION].[MI_ACTION_SHORT_DESC_C] & ' ')) & '|----') "LTrimmed Name" , ('----|' & RTRIM((' ' & [MI_ACTION].[MI_ACTION_SHORT_DESC_C] & ' ')) & '|----') "RTrimmed Name" FROM [MI_ACTION]
- LPad, RPad
- Return a character expression of a specified length after padding with a specified character. A space is the default padchar value.
-- Syntax SELECT LPad(<expression>, <length> [, <padchar>]) FROM <source> SELECT RPad(<expression>, <length> [, <padchar>]) FROM <source> -- Example SELECT [MI_ACTION].[MI_ACTION_ID_C] "Action ID" , LPAD(CASTCHAR(DatePart('d', [MI_ACTION].[MI_ACTION_TARGE_COMPL_DATE_CHR])), 2, ' ') "Day" FROM [MI_ACTION]
- Concat
- Concatenates the arguments returning a string. The argument list is a params argument (multiple arguments are supported). At least two arguments are required.
-- Syntax SELECT Concat(<exp1>, <exp2> [,<expn>]) FROM <source> SELECT Concat(<exp1>, <exp2>) FROM <source> -- Example SELECT Concat('foo-', [MI_ACTION].[MI_ACTION_ID_C], '-bar') "Action ID" FROM [MI_ACTION]
- Year, Month, Day
- Return a part of the specified date expression. For more control or granularity when retrieving date parts, see the DatePart function.
-- Syntax SELECT Year(<date_expression>) FROM <source> SELECT Month(<date_expression>) FROM <source> SELECT Day(<date_expression>) FROM <source> -- Example SELECT [MI_ACTION].[MI_ACTION_ID_C] "Action ID" , [MI_ACTION].[MI_ACTION_TARGE_COMPL_DATE_CHR] "Target Completion Date" , YEAR([MI_ACTION].[MI_ACTION_TARGE_COMPL_DATE_CHR]) "Target Completion Year" , MONTH([MI_ACTION].[MI_ACTION_TARGE_COMPL_DATE_CHR]) "Target Completion Month" , DAY([MI_ACTION].[MI_ACTION_TARGE_COMPL_DATE_CHR]) "Target Completion Day" FROM [MI_ACTION]
- SysDate
- Retrieves the system date.
-- Syntax SELECT SysDate() FROM <source> -- Example SELECT [MI_ACTION].[MI_ACTION_ID_C] "Action ID" , SYSDATE() "System Date" FROM [MI_ACTION]
- LastDate
- Returns a date representing the last day of the month in which a given date occurs.
cost_char must be formatted as YYYY-MM-DD.-- Syntax SELECT LastDate(<const_char>) FROM <source> -- Example SELECT [MI_ACTION].[MI_ACTION_ID_C] "Action ID" , LASTDATE('2016-02-01') "Last Day of Feb, 2016" , LASTDATE('2017-02-01') "Last Day of Feb, 2017" , LASTDATE('2018-02-01') "Last Day of Feb, 2018" , LASTDATE('2019-02-01') "Last Day of Feb, 2019" , LASTDATE('2020-02-01') "Last Day of Feb, 2020" FROM [MI_ACTION]
- Case
- Performs a series of evaluations and returns the first result that evaluates to True. The simple syntax works well for an EQUALS comparison. However, if more complexity is required, you can use the general CASE expression to perform various types of comparisons.
-- Syntax (simple CASE expression) SELECT CASE <field_id> WHEN <expression> THEN <expression> [ ELSE <expression> ] END FROM <source> -- Example SELECT [MI_ACTION].[MI_ACTION_ID_C] "Action ID" , [MI_ACTION].[MI_ACTION_DESCRIPTION_T] "Description" , CASE [MI_ACTION].[MI_ACTION_DESCRIPTION_T] WHEN 'Perform check of lubricant, add or change oil when needed' THEN 'Check' WHEN 'Perform changeout of lubricant' THEN 'Changeout' ELSE 'Other' END "Lubricant Action" FROM [MI_ACTION] WHERE [MI_ACTION].[MI_ACTION_DESCRIPTION_T] LIKE '%Lubricant%' -- Syntax (general CASE expression) SELECT CASE WHEN <boolean_expression> THEN <expression> [ ELSE <expression> ] END FROM <source> -- Example SELECT [MI_ACTION].[MI_ACTION_ID_C] "Action ID" , [MI_ACTION].[MI_ACTION_DESCRIPTION_T] "Description" , CASE WHEN [MI_ACTION].[MI_ACTION_DESCRIPTION_T] LIKE 'Perform check of lubricant%' THEN 'Check' WHEN [MI_ACTION].[MI_ACTION_DESCRIPTION_T] LIKE 'Perform changeout%' THEN 'Changeout' ELSE 'Other' END "Lubricant Action" FROM [MI_ACTION] WHERE [MI_ACTION].[MI_ACTION_DESCRIPTION_T] LIKE '%Lubricant%'
- Sign
- Returns the sign of the numeric argument (-1, 0, +1).
-- Syntax SELECT Sign(<exp1>) FROM <source>
- Abs
- Returns the absolute value of the numeric the argument.
-- Syntax SELECT abs(<exp1>) FROM <source>
- Reverse
- Returns the reverse order of a string value.
-- Syntax SELECT Reverse(<exp1>) FROM <source>
- Floor
- Returns the largest integer less than or equal to the argument numeric expression.
-- Syntax SELECT Floor(<exp1>) FROM <source>
- Round
- Returns the nearest integer for the argument numeric expression. Rounds to the precision, if specified.
-- Syntax SELECT Round(<exp1> [, <precision>]) FROM <source>
Analytic Functions
Analytic functions are used for aggregating data on a row-by-row basis. They work similar to aggregate functions, except they can return multiple rows of results for each group. They are useful for calculating running totals, moving percentages, and so on.
Analytic functions work the same way, regardless of the database management system. For more information on analytic functions, refer to https://learn.microsoft.com/en-us/sql/t-sql/functions/analytic-functions-transact-sql?view=sql-server-2017.
<analytic_function> ::= function_id() [OVER ( [PARTITION BY field_id] ORDER BY <order_by_expression> )]
...where function_id is the name of the function you are executing, field_id is the field used to group results, and <order_by_expression> specifies which fields must be used to sort the results in the current partition. - SUM
-
SELECT SUM([FIELD]) OVER(PARTITION BY [FIELD], [FIELD]... ORDER BY [FIELD] ASC, [FIELD] DESC... ROWS BETWEEN CURRENT ROW AND 1 FOLLOWING) "Cost" FROM [FAMILY]
- MAX
-
SELECT MAX([FIELD]) OVER(PARTITION BY [FIELD], [FIELD]... ORDER BY [FIELD] ASC, [FIELD] DESC... ROWS BETWEEN CURRENT ROW AND 1 FOLLOWING) "Cost" FROM [FAMILY]
- AVG
-
SELECT AVG([FIELD]) OVER(PARTITION BY [FIELD], [FIELD]... ORDER BY [FIELD] ASC, [FIELD] DESC... ROWS BETWEEN CURRENT ROW AND 1 FOLLOWING) "Expr" FROM [FAMILY]
- COUNT
-
SELECT COUNT([FIELD]) OVER(PARTITION BY [FIELD], [FIELD]... ORDER BY [FIELD] ASC, [FIELD] DESC... ROWS BETWEEN CURRENT ROW AND 1 FOLLOWING) "Expr" FROM [FAMILY]
- ROW_NUMBER
-
SELECT ROW_NUMBER() OVER(PARTITION BY [FIELD], [FIELD]... ORDER BY [FIELD] ASC, [FIELD] DESC...) "Row #" FROM [FAMILY]
- CUME_DIST
-
SELECT CUME_DIST() OVER ([PARTITION BY [FIELD], [FIELD]...] ORDER BY [FIELD] ASC, [FIELD] DESC...) "Expr" FROM [FAMILY]
- PERCENT_RANK
-
SELECT PERCENT_RANK([FIELD]) OVER(PARTITION BY [FIELD], [FIELD]... ORDER BY [FIELD] ASC, [FIELD] DESC... ROWS BETWEEN CURRENT ROW AND 1 FOLLOWING) "Expr" FROM [FAMILY]
- PERCENTILE_DISC
-
SELECT PERCENTILE_DISC([FIELD]) OVER(PARTITION BY [FIELD], [FIELD]... ORDER BY [FIELD] ASC, [FIELD] DESC... ROWS BETWEEN CURRENT ROW AND 1 FOLLOWING) "Expr" FROM [FAMILY]
- PERCENTILE_CONT
-
SELECT PERCENTILE_CONT([FIELD]) OVER(PARTITION BY [FIELD], [FIELD]... ORDER BY [FIELD] ASC, [FIELD] DESC... ROWS BETWEEN CURRENT ROW AND 1 FOLLOWING) "Expr" FROM [FAMILY]
- NTILE
num_const is a positive integer representing the number of groups that will be created in the resultSELECT NTILE(num_const) OVER(PARTITION BY [FIELD], [FIELD]... ORDER BY [FIELD] DESC) "Expr" FROM [FAMILY]
Using Max, Min, Avg, Count, and Sum
SELECT DISTINCT [MI_MRBIANAL].[MI_CRITANAL_RSK_CAT_C] "Risk Category"
, Min([MI_MRBIANAL].[MI_CRITANAL_PROB_OF_FAIL_UP_C])OVER ( PARTITION BY [MI_MRBIANAL].[MI_CRITANAL_RSK_CAT_C] ) "Min Prob of Fail"
, Max([MI_MRBIANAL].[MI_CRITANAL_PROB_OF_FAIL_UP_C])OVER ( PARTITION BY [MI_MRBIANAL].[MI_CRITANAL_RSK_CAT_C] ) "Max Prob of Fail"
, Avg([MI_MRBIANAL].[MI_CRITANAL_INSPE_PRIOR_UP_N])OVER ( PARTITION BY [MI_MRBIANAL].[MI_CRITANAL_RSK_CAT_C] ) "Avg Insp Priority"
, Count([MI_EQUIP000].ENTY_ID)OVER ( PARTITION BY [MI_MRBIANAL].[MI_CRITANAL_RSK_CAT_C] ) "# Assets"
, Sum([MI_MRBIANAL].[MI_CRITANAL_LEAK_QUANTITY_N])OVER ( PARTITION BY [MI_MRBIANAL].[MI_CRITANAL_RSK_CAT_C] ) "Total Leak Quantity"
FROM {MIR_HSRBICMP}
JOIN [MI_CCRBICOM] ON {MIR_HSRBICMP}.SUCC_ENTY_KEY = [MI_CCRBICOM].ENTY_KEY
JOIN {MIR_HSRBICMP} Has_RBI_Components1 ON [MI_CCRBICOM].ENTY_KEY = Has_RBI_Components1.SUCC_ENTY_KEY
JOIN {MIR_RBICRAN} ON [MI_CCRBICOM].ENTY_KEY = {MIR_RBICRAN}.PRED_ENTY_KEY
JOIN [MI_EQUIP000] ON Has_RBI_Components1.PRED_ENTY_KEY = [MI_EQUIP000].ENTY_KEY
JOIN [MI_MRBIANAL] ON {MIR_RBICRAN}.SUCC_ENTY_KEY = [MI_MRBIANAL].ENTY_KEY
ORDER BY [MI_MRBIANAL].[MI_CRITANAL_RSK_CAT_C] Asc
Results:Risk Category | Min Prob of Fail | Max Prob of Fail | Avg Insp Priority | # Assets | Total Leak Quantity |
---|---|---|---|---|---|
1 | 2 | 0 | 615 | 4 | |
HIGH | 1 | 2 | 2.425675675675676 | 148 | 1,216,204.004371306 |
LOW | 3 | 5 | 22.43975903614458 | 166 | 590,251.1253449451 |
MEDIUM | 2 | 5 | 16.331818181818182 | 220 | 813,327.89638713 |
MEDIUM HIGH | 1 | 4 | 8.489247311827956 | 186 | 1,305,554.6602732195 |
Additional Meta-SQL Functions
Meta-SQL constructs are used in functions that pass SQL strings.
The following table provides a list of Meta-SQL functions that you can use in query expressions in GE Digital APM.
Description | Meta-SQL Function | Construction |
---|---|---|
Return the local time of the database server. | SysDate | SysDate |
Evaluate one or more When expressions and return the appropriate Then expression. The Else condition is optional. The End statement is required. This function returns the datatype thenexpression. Note: This function is not a selectable option in the Design workspace, but you can enter the function directly in the SQL workspace. | Case |
Case evalexpression When whenexpression Then thenexpression [When whenexpression Then thenexpression] [Else thenexpression] End Evalexpression: Any column or literal value. Whenexpression: Must be same datatype of evalexpression. Thenexpression: All must be the same datatype. Does not have to be the same datatype as evalexpression or whenexpression. |
Modulus Function
SELECT Modulus(ROUND([AQA REG All Fld Types].[ARAQA_REG_ALL_FLD_TY_NUMER_NBR]), 2) "Modulus2"
, Modulus(ROUND([AQA REG All Fld Types].[ARAQA_REG_ALL_FLD_TY_NUMER_NBR]), 3) "Modulus3"
FROM [AQA REG All Fld Types]
About Adding Hyperlinks to a Query
For each column in a query, you can configure one or more URLs to display as hyperlinks in the query results. When a user runs the query, the GE Digital APM system will build the URLs as needed, passing data from the query results into the URL parameters if necessary, and will display in the query results hyperlinks that the user can select to access the associated feature or perform the associated function.
For example, you might define a URL on a field to an external website. When a user runs the query, the GE Digital APM system will build a hyperlink from that URL and display the link to the user in the query results. The user will be able to select the hyperlink to open the website in a new browser tab.
If you configure only one URL for a field, when you run the query, that URL will be used to build a single hyperlink in that cell of the query results. If you have not modified the Field cell, whatever values are found in the database for that column will serve as the text for each hyperlink. For example, if an Asset ID column contains a URL to open a record in the Record Manager, when you run the query, the actual Asset IDs retrieved by the GE Digital APM system will appear as hyperlinks in the results.