You can exclude TMLs so that they will not be included in the TM Analysis calculations. The TML is excluded at the asset level, not the TML level.
Steps
Access the Analysis Overview workspace for the asset or TML Group that contains the TMLs that you want to exclude.
In the workspace, select the TMLs tab.
A list of TMLs contained in the analysis appears in the workspace.
In the upper-right corner of the workspace, select , and then select Exclude TMLs.
The Exclude TMLs window appears, providing a list of TMLs in the analysis. If a TML has already been excluded, the corresponding check box is selected.
In the list, select the check boxes corresponding to the TMLs that you want to exclude.
Note: If you do not see the TMLs that you expect, or want to limit the list, in the upper-left corner of the window, confirm the setting in the Analysis Type box, and whether the Active TMLs Only check box is selected.
Select Done.
The selected TMLs are excluded from the analysis.
Tip: At this time, you can calculate the Analysis with the newly excluded TMLs by selecting .
Copyright © 2018 General Electric Company. All rights reserved.