Create Corrosion Analysis Settings

Before an asset can be accessed via the Thickness Monitoring Overview page, you must create Corrosion Analysis Settings for that asset.

Steps

  1. On the top navigation bar, select .

    The Asset Hierarchy page appears.

  2. On the Asset Hierarchy page, select the asset for which you want to create corrosion analysis settings.
  3. In the workspace, select the Integrity tab, and then, in the Thickness Monitoring row, select TML Groups.

    Note: TML Groups will only appear if you have selected an asset. If you have selected a functional location, Assets replaces TML Groups.

    The TM page appears, displaying the Corrosion Analysis Settings workspace.

    By default, values in the following boxes are populated automatically as follows:

    Tip: If needed, you can modify values in the available fields.

  4. Select Create Settings.

    The Corrosion Analysis Settings record is created.

Results

What's Next?

Copyright © 2018 General Electric Company. All rights reserved.