Process Data Integration (PDI) System Requirements

License Requirements

The OPC Interfaces license is required to take advantage of Process Data Integration functionality.

Additional Components Required

In addition to the basic GE Digital APM system architecture, the following additional components are required:

Refer to the supported software and devices documentation for information about the OPC Servers and process historians are supported for the PDI feature. Other OPC Servers and process historians have not been tested and connections to them are not supported by GE Digital.

System Architecture

The following image shows how these machines should be incorporated into the basic GE Digital APM system architecture if you implement the standard configuration where the OPC Server software and the Meridium APM Process Data Integration Service are installed on the same machine.

The following image shows the alternate configuration of these machines when the OPC Server software is installed on a separate machine from the Meridium APM Process Data Integration Service.

Deploying Process Data Integration

After you have installed and configured the basic GE Digital APM system architecture, you will need to perform some configuration steps specifically for Process Data Integration.

If you want to use Process Data Integration with Asset Health Manager and Policy Designer, you must also configure the services associated with these modules. For additional information on how services used by these three modules interact, select this link.

Supported Features in APM Now

This GE Digital APM module is not available in the APM Now environment.

Copyright © 2018 General Electric Company. All rights reserved.