License Requirements
The Asset Health license and the licenses for the modules that you want to use with AHM are required to take advantage of AHM functionality.
Additional Components Required
When you install the GE Digital APM Server, the Asset Health Indicator Service is installed automatically. In order for the Asset Health Indicator Service to function as described within this documentation, you must start the Asset Health Indicator Service. After you do so, the Asset Health Indicator Service will allow the health indicator status values to be updated automatically.
Your system must also meet the system requirements for any of these additional modules that you plan to use with Asset Health Manager.
System Architecture
The following image shows the architecture components that are required to support this module.
Deploying Asset Health Manager
After you have installed and configured the basic GE Digital APM system architecture, you will need to perform some configuration steps specifically for Asset Health Manager.
If you want to use Asset Health Manager with
Supported Features in
In the
Copyright © 2018 General Electric Company. All rights reserved.