You can create an Instrumented Function by copying the details from another Instrumented Function linked to a SIL Analysis.
When you copy an Instrumented Function, the SIL Assessment that is associated with the Instrumented Function is also copied.
However, the values of the following fields are not copied:
You can also create an Instrumented Function using a blank datasheet.
Steps
In the left pane, select
The Search window appears.
In the upper-right corner of the window, select
A list of Instrumented Functions appears.
Select the check box that corresponds to the Instrumented Function that you want to copy, and then in the lower-right corner of the window, select OK.
A copy of the Instrumented Function is created, and listed in the left pane.
In the upper-right corner of the datasheet, select
The changes made to the Instrumented Function are saved.
Copyright © 2018 General Electric Company. All rights reserved.